package ti.sysbios.gates |
|
Contains modules that inherit from IGatePovider
The
xdc.runtime.Gate module is provided by XDCtools, and
is documented in the XDCtools help, but SYS/BIOS provides
additional implementations in the
ti.sysbios.gates package.
[
more ... ]
package ti.sysbios.gates [2, 0, 0, 0] {
// Hwi, Swi & Task Gate
// Hardware Interrupt Gate
// Mutex Gate
// Mutex Gate with priority inheritance
// Software Interrupt Gate
// Task Gate
}
DETAILS
The
xdc.runtime.Gate module is provided by XDCtools, and
is documented in the XDCtools help, but SYS/BIOS provides
additional implementations in the
ti.sysbios.gates package.
A "Gate" is a module that implements the IGateProvider interface.
Gates are devices for preventing concurrent accesses to critical
regions of code. The various Gate implementations differ in how they
attempt to lock the critical regions.
Threads can be preempted by other threads of higher priority, and
some sections of code need to be completed by one thread before they
can be executed by another thread. Code that modifies a linked list
is a common example of a critical region that may need to be protected
by a Gate.
Gates generally work by either disabling some level of preemption such
as disabling task switching or even hardware interrupts, or by using a
binary semaphore.
All Gate implementations support nesting through the use of a "key".
For Gates that function by disabling preemption, it is possible that
multiple threads would call Gate_enter(), but preemption should not be
restored until all of the threads have called Gate_leave().
This functionality is provided through the use of a key. A call to
Gate_enter() returns a key that must then be passed back to Gate_leave().
Only the outermost call to Gate_enter() returns the correct key for
restoring preemption. (The actual module name for the implementation
is used instead of "Gate" in the function name.)
RUNTIME EXAMPLE
The following C code protects a critical region with
a Gate. This example uses a GateHwi, which disables and enables
interrupts as the locking mechanism.
UInt gateKey;
GateHwi_Handle gateHwi;
GateHwi_Params prms;
GateHwi_Params_init(&prms);
gateHwi = GateHwi_create(&prms, NULL);
// Simultaneous operations on a List by multiple threads could
// corrupt the List structure, so modifications to the List
// are protected with a Gate.
gateKey = GateHwi_enter(gateHwi);
List_get(myList);
GateHwi_leave(gateHwi, gateKey);
generated on Thu, 23 May 2019 00:22:19 GMT