This implementation provides a fully functional implementation of
all methods specified by
ISystemSupport. As with all
ISystemSupport modules, this module is the back-end for the
xdc.runtime.System module.
This implementation relies on the target's runtime support libraries
(i.e. fflush() and putchar()). Therefore the functions are re-entrant
(thread-safe) if the underlying rts library is re-entrant.
enum SysUart_Uart |
|
UART peripheral base address
typedef enum SysUart_Uart {
SysUart_Uart0,
// UART0 Base Address
SysUart_Uart1,
// UART1 Base Address
SysUart_Uart2,
// UART2 Base Address
SysUart_Uart3,
// UART3 Base Address
SysUart_Uart4
// UART4 Base Address
} SysUart_Uart;
DETAILS
These enumerations are the base addresses of the different
UART peripherals.
config SysUart_uartBaseAddr // module-wide |
|
extern const Ptr SysUart_uartBaseAddr;
SysUart_abort() // module-wide |
|
Backend for xdc.runtime.System.abort()
Void SysUart_abort(CString str);
ARGUMENTS
str
message to output just prior to aborting
If non-NULL, this string should be output just prior to
terminating.
DETAILS
This function is called by
System.abort() prior to calling
the ANSI C Standard library function
abort(). So, to ensure the
abort processing of the system's ANSI C Standard library completes,
this function should return to its caller.
This abort function writes the string via putchar()
and flushes via fflush() to stdout.
SEE
SysUart_exit() // module-wide |
|
Backend for xdc.runtime.System.exit()
Void SysUart_exit(Int stat);
ARGUMENTS
stat
status value passed to all "atexit" handlers
This value is passed to all "atexit" handles bound via
System.atexit().
DETAILS
This function is called as part the normal "atexit" processing
performed by the ANSI C Standard Library's
exit() function;
System.exit() directly calls ANSI
exit().
This function is called after all "atexit" handlers bound via
System.atexit() are run and it
is always called while "inside" the the
System gate.
To ensure that all exit processing of the system's ANSI C
Standard Library completes, this function should return to its caller.
Exit handlers bound using the ANSI C Standard Library atexit()
function may run before or after this function.
This exit function flushes via fflush() to stdout.
SEE
SysUart_flush() // module-wide |
|
Backend for xdc.runtime.System.flush()
DETAILS
This function is simply called by
System_flush
to output any characters buffered by the underlying
SystemSupport
module to an output device.
This flush function flushes via fflush() to stdout.
SEE
SysUart_putch() // module-wide |
|
Backend for xdc.runtime.System.printf() and xdc.runtime.System.putch()
Void SysUart_putch(Char ch);
ARGUMENTS
ch
character to output
DETAILS
Output a single character. This function is called by
System_printf() to write each character
of formated output specified by its arguments.
This function outputs the character via putchar().
SEE
SysUart_ready() // module-wide |
|
Test if character output can proceed
DETAILS
This function is called by
System prior to performing
any character output. If this function returns
FALSE, the
System
functions that would normally call
putch() simply return
(with an appropriate error status) without ever calling
putch.
This always returns TRUE.
SEE
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool SysUart_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool SysUart_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 SysUart_Module_getMask();
// Returns the diagnostics mask for this module
Void SysUart_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module