1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     *
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     *
    11     * */
    12    /*!
    13     *  ======== gnu.targets.ITarget ========
    14     *  Interface to GCC compatible compilers
    15     */
    16    @TargetHeader("xdc/bld/stddefs.xdt")
    17    metaonly interface ITarget inherits xdc.bld.ITarget3 {
    18    
    19        override readonly config string stdInclude = "gnu/targets/std.h";
    20        override config string dllExt = ".so";
    21    
    22        /*!
    23         *  ======== GCCVERS ========
    24         *  Version number of the GCC compiler; e.g., "3.2".
    25         *
    26         *  This string can be supplied by the user, otherwise it is obtained
    27         *  by running "gcc -dumpversion".
    28         */
    29        config string GCCVERS = null;
    30    
    31        /*!
    32         *  ======== BINVERS ========
    33         *  Version number of binutils used with the compiler; e.g., "2.19".
    34         *
    35         *  This string can be supplied by the user, otherwise it is obtained
    36         *  by running "ld -v".
    37         */
    38        config string BINVERS = null;
    39    
    40        /*!
    41         *  ======== version ========
    42         *  The Compatibility Key associated with this target.
    43         *
    44         *  The first two components of this target's Compatibility Key are '1,0'.
    45         *  The rest of the Key represents the compiler version. The third
    46         *  component combines the major and the minor version number in the format
    47         *  Major.Minor. The fourth component is the patch number.
    48         *
    49         *  @a(Example)
    50         *  If this target's `rootDir` points to the compiler version 3.4.6, the 
    51         *  Compatibility Key is [1,0,3.4,6].
    52         *
    53         */
    54        override metaonly config String version;
    55    
    56        /*!
    57         *  ======== GCCTARG ========
    58         *  The name of the platform executing programs produced by this target
    59         *
    60         *  This string can be supplied by the user, otherwise is is obtained
    61         *  from the compiler and follows the GNU standard format
    62         *  (<cpu>-<manufacturer>-<os> or <cpu>-<manufacturer>-<kernel>-<os>);
    63         *  e.g., "arm-none-eabi" or "x86_64-unknown-linux-gnu".
    64         *
    65         *  When building a GCC compiler, there are three different execution
    66         *  platforms to consider: the platform used to "build" the compiler, the
    67         *  "host" platform that runs the compiler, and the "target" platform
    68         *  that runs the executables produced by the compiler. All three
    69         *  platforms are identified using a
    70         *  {@link http://sources.redhat.com/autobook/autobook/autobook_17.html configuration name}
    71         *  defined by GNU Autotools.  `GCCTARG` is the name of the "target"
    72         *  platform.
    73         */
    74        config string GCCTARG = null;
    75    
    76        /*!
    77         *  ======== LONGNAME ========
    78         *  @_nodoc
    79         *  The "long name" of the gcc compiler
    80         *
    81         *  This name is used (in conjunction with rootDir) to find the compiler
    82         *  and linker for this target. The format of `LONGNAME` is always
    83         *  "/bin/<machine>-gcc". For majority of the targets, the default value
    84         *  for `LONGNAME` does not ever need to be changed. But, there are
    85         *  targets where the different but compatible compilers may have
    86         *  different `LONGNAME` parameters. For such targets and compilers,
    87         *  `LONGNAME` can be set in `config.bld`.
    88         *
    89         *  @a(Example)
    90         *  If a version 2010q1 of the CodeSourcery GNU toolchain for Arm is
    91         *  installed in C:/CodeSourcery/arm-2010q1, the following settings in
    92         *  `config.bld` configure `gnu.targets.arm.GCArmv6` target to use that
    93         *  toolchain:
    94         *  @p(code)
    95         *  var GCArmv6 = xdc.module("gnu.targets.arm.GCArmv6");
    96         *  GCArmv6.rootDir = "C:/CodeSourcery/arm-2010q1"; 
    97         *  GCArmv6.LONGNAME = "bin/arm-none-linux-gnueabi-gcc";
    98         *  @p
    99         *
   100         */
   101        config string LONGNAME = null;
   102    
   103        /*!
   104         *  ======== CYGWIN ========
   105         *  Is the target's compiler a cygwin executable
   106         *
   107         *  Since file names produced by cygwin-based tools differ from the
   108         *  names understood by other Windows executables, it is important
   109         *  to avoid using the names output by cygwin tools as input to
   110         *  non-cygwin programs.  This property tells the target whether
   111         *  or not it's possible to use the output from `gcc -MD -MF`, for
   112         *  example.
   113         */
   114        readonly config Bool CYGWIN = false;
   115    
   116        /*!
   117         *  ======== noStdLinkScript ========
   118         *  Don't use the standard linker script
   119         *
   120         *  If `true`, add a `-T` flag before the generated `package/cfg/*.xdl`
   121         *  file passed to the linker.  This flag suppresses use of the
   122         *  standard linker script implicit in the GCC flow, which effectively
   123         *  says the generated `.xdl` file assumes total control for all
   124         *  `MEMORY` and `SECTION` directives.
   125         *
   126         */
   127        config Bool noStdLinkScript = false;
   128    
   129        /*
   130         *  ======== profiles ========
   131         */
   132        override config xdc.bld.ITarget.OptionSet profiles[string] = [
   133            ["debug", {
   134                compileOpts: {
   135                    copts: "-g",
   136                    defs:  "-D_DEBUG_=1",
   137                },
   138                linkOpts: "-g",
   139            }],
   140    
   141            ["release", {
   142                compileOpts: {
   143                    copts: "-O2 -ffunction-sections -fdata-sections",
   144                },
   145                linkOpts: "-Wl,--gc-sections",
   146            }],
   147    
   148            ["profile", {
   149                compileOpts: {
   150                    copts: "-g -pg",
   151                },
   152                linkOpts: "-pg"     /* can't use -static here */
   153            }],
   154    
   155            ["coverage", {
   156                compileOpts: {
   157                    copts: "-fprofile-arcs -ftest-coverage",
   158                },
   159                linkOpts: "-fprofile-arcs -ftest-coverage",
   160            }],
   161        ];
   162    
   163        /*!
   164         *  ======== versionMap ========
   165         *  Map of GCC compiler version numbers to compatibility keys.
   166         *
   167         *  This map translates version string information from the compiler
   168         *  into a compatibility key.  The compatibilty key is used to
   169         *  validate consistency among a collection of packages used in
   170         *  a configuration.
   171         *
   172         *  The compiler version string is "gcc<ver>", where <ver> is
   173         *  GCCVERS.
   174         *
   175         *  If a compiler version is not found in this map the default is
   176         *  "1,0,<ver>", where <ver> is the compiler version number.  Thus,
   177         *  the user only needs to extend this table when a significant
   178         *  incompatibility occurs or when two versions of the compiler should
   179         *  be treated as 100% compatible.
   180         */
   181        override config string versionMap[string] = [
   182            ["gcc3.2", "1,0,3.2,0"],
   183        ];
   184    
   185        /*!
   186         *  ======== remoteHost ========
   187         *  Remote host used to run compiler, linker, and archiver tools
   188         *
   189         *  If `remoteHost` is `null` (or `undefined`), the configured compiler
   190         *  is run locally; otherwise, `remoteHost` is taken to be the host name
   191         *  of the machine that that should be used to run the specified compiler.
   192         *
   193         *  All target commands are prefixed with a command that uses `rsh` to run
   194         *  the commands on the specified host.  Thus, in order to use this
   195         *  setting, the remote machine must be support `rsh` and the user must
   196         *  have permission to run commands from the local machine on the remote
   197         *  host named `remoteHost`.  This usually involves adding a line to the
   198         *  user's `~/.rhosts` file on the remote machine of the form:
   199         *  @p(code)
   200         *      local-machine-name user-name
   201         *  @p
   202         *  where `local-machine-name` is the name of the local machine and
   203         * `user-name` is the user's login name on the local machine.
   204         */
   205        config string remoteHost;
   206    
   207        /*!
   208         *  ======== ar ========
   209         *  The command used to create an archive
   210         */
   211        override readonly config xdc.bld.ITarget2.Command ar = {
   212            cmd: "$(rootDir)/bin/ar",
   213            opts: "cr"
   214        };
   215    
   216        /*!
   217         *  ======== lnk ========
   218         *  The command used to link executables.
   219         */
   220        override readonly config xdc.bld.ITarget2.Command lnk = {
   221            cmd: "$(rootDir)/bin/gcc",
   222            opts: ""
   223        };
   224    
   225        override config xdc.bld.ITarget2.Options lnkOpts = {
   226            prefix: "",
   227            suffix: "-Wl,-Map=$(XDCCFGDIR)/$@.map -lstdc++ -L$(rootDir)/lib"
   228        };
   229    
   230        /*!
   231         *  ======== cc ========
   232         *  The command used to compile C/C++ source files into object files
   233         */
   234        override readonly config xdc.bld.ITarget2.Command cc = {
   235            cmd: "$(rootDir)/bin/gcc -c -MD -MF $@.dep",
   236            opts: ""
   237        };
   238    
   239        /*!
   240         *  ======== asm ========
   241         *  The command used to assembles assembly source files into object files
   242         */
   243        override readonly config xdc.bld.ITarget2.Command asm = {
   244            cmd: "$(rootDir)/bin/gcc -c -x assembler",
   245            opts: ""
   246        };
   247    
   248        /*!
   249         *  ======== includeOpts ========
   250         *  Additional user configurable target-specific include path options
   251         */
   252        override config string includeOpts = "";
   253    
   254        override config String binaryParser = "ti.targets.omf.elf.Elf32";
   255    
   256        /*
   257         *  ======== initVers ========
   258         *  The function that detects the version of the Gnu compiler.
   259         */
   260        String initVers();
   261    
   262        /*!
   263         *  ======== asmName ========
   264         *  The function that converts a C name into an assembly name
   265         */
   266        String asmName(String CName);
   267    
   268        /*!
   269         *  ======== bspLib ========
   270         *  bspLib is assigned the name of the BSP library. The specified library
   271         *  is included on the link line.
   272         */
   273        config string bspLib = null;
   274    }
   275    /*
   276     *  @(#) gnu.targets; 1, 0, 1,0; 4-18-2019 17:32:43; /db/ztree/library/trees/xdctargets/xdctargets-t04/src/ xlibrary
   277    
   278     */
   279