SYS/BIOS Static Analysis Report
This report summarizes the results from the Klocwork static analysis checker.
Klocwork v12.2.0 was used to analyze the complete set of SYS/BIOS source files across all source directories. Source files were built for all supported toolchains. Klocwork analysis was performed across all of these builds.
Raw Data from Klocworks static analysis using default configuration.
Explanation of Issues:
ti/sysbios/family/arm/v7r/Keystone3/Hwi.c – 2 issues. The issues were reviewed. Klowork cannot see an external constant define for the NUMINT constant. These issues are false positives.
ti/sysbios/family/arm/lm4/Seconds.c – 2 issues. The function cannot be coded differently. The issues were reviewed. These issues are false positives.
ti/sysbios/family/arp32/Hwi.c – 12 issues. This code is for a mature device that is very stable and no longer under development. The issues were reviewed and deemed to be false positives.