This release note is divided into the following sections:
Introduction,
Documentation,
What's New,
Upgrading And
Compatibility Information,
Host Support,
Dependencies,
Device Support,
Validation Information,
Known Issues,
Benchmarks,
Versioning,
Technical Support
And Product Updates,
SYS/BIOS 6.40.03.39 is a GA release of SYS/BIOS
6.40.00. CCS users must use CCSv6.0.0 or higher. This
release also has support for GCC (for Cortex-M) and IAR (for Cortex-M
and MSP430).
Please read the SYS/BIOS User's Guide for help installing and setting
up your environment to use SYS/BIOS 6.40.03.39.
back to top
The following documentation is provided with this release. These
documents are also available via the CCS Eclipse help table of
contents.
License and manifest.
Additional online sources of documentation.
Release
notes from previous releases are also available in the
release notes archive
directory.
back to top
SYS/BIOS
6.40.03.39 GA
Release (this release).
- Maintenance release. See bug list.
Defects Fixed in
SYS/BIOS
6.40.03.39 GA (Fixes since SYS/BIOS 6.40.02):
ID
Headline
SDOCM00112256 F2837x Boot module needs clock configuration for CPU2
SDOCM00112220
MSP430: remove the one-tick-late limit for triggering an interrupt when
timer threshold is set too late
SDOCM00112070 Add Cortex-M4 Timer API to notify BIOS a timer is being used.
SDOCM00108595 Hwi stack size is not configured correctly using IAR tools.
SDOCM00108501 _c_int00 (Entry Point) should be put in its own section for all Cortex-A and Cortex-M GNU targets
SDOCM00108411
Hwi_dispatcher can restore incorrect IER register if Hwi_create()
called after init time (ARP32/EVE specific issue)
SDOCM00108287 Number of IRQ Xbar inputs in IntXbar module is incorrect (Affects DRA7XX, TDA2XX & TDA3XX devices)
SDOCM00108254 Re-order the placement of linker contributions in GNU linker template for Cortex-A targets
SDOCM00108230 c2800/initF2837x's initFlash() function needs to flush the pipeline before returning
SDOCM00108193
Update C28 Hwi documentation to include info about the extended PIE
vector (128-223) support for F2837x
SDOCM00108148 Update gnu/targets/std.h to use C99 types to define XDC types
SDOCM00108039 Add support for MMU0 present in DSP Sub-systems found on ADAS Low and J6 devices
SDOCM00107973 lm3 and lm4 Timestamp_get64() function do not handle the 32-bit rollover correctly
back to top
SYS/BIOS
software downloads
SYS/BIOS 6.35 and 6.37
- Binary compatible for all targets except MSP430 and C2000.
- MSP430
and C2000 users must recompile all source files that use the Semaphore,
Mailbox, or Event modules. The timeout parameter was changed from
UInt to UInt32 which are different sizes.
- All other users can use libraries built with 6.35.0x and 6.37.0x with 6.40.00.
SYS/BIOS 6.34 and older
- Source compatible. All APIs are supported but all source files must be recompiled.
back to top
- Supported
Operating Systems
- Windows 8, Windows
7
- Ubuntu [10.04, 12.04, 12.10, 13.04]
back to top
- Minimum Required Software Versions
- Code Composer Studio v6.0.x or later
- TI Code Generation Tools
- C28X
version 6.2.5 or later
- C6X version 7.4.7 or later
- ARM version 5.1.5 or later
- MSP430 version 4.3.1 or later
- XDCTools 3.30.00.21 or later
- GNU Code Generation Tools (for ARM only)
- ARM gcc-arm-none-eabi-4_7-2013q3 or later
- XDCtools 3.30.00.21 or later
- IAR Code Generation Tools (for Arm Cortex-M and MSP430 only)
- ARM version 6.70.1
- MSP430 version 5.60.1
- XDCtools 3.30.00.21 or later
- Required Hardware
- See Device Support Section below.
back to top
Click here
for the list of supported devices.
back to top
Click
here
for the list of compilers used to build and validate this release
(scroll down to Supported Targets section).
back to top
The
following issues are known to affect this release:
back to top
For a full description of Benchmarks please see the
appendices in the SYS/BIOS
6 User's
Guide.
back to top
All releases
have 4 digits (M.mm.pp.bb).
This includes GA and pre-releases (engineering, alpha/EA, beta, etc.).
Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or
6.30.00.10-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit
Major number, mm
is 2 digit minor number, pp
is a 2 digit patch number, and b
is an unrestricted set of digits used as an incrementing build counter.
To
support multiple side-by-side installations of the product, the product
version is encoded in the top level directory (e.g. bios_6_30_00_00).
Subsequent
releases of patch upgrades will be identified by the patch number, ex.
SYS/BIOS 6.30.01.15 with directory bios_6_30_01_15. Typically, these
patches only include critical bug fixes.
Please note that
version numbers and compatibility keys are NOT the same. For an
explanation of compatibility keys, please refer to the 'Upgrade and
Compatibility Information' section.
back to top
Technical
Support and Product Updates
back to top
Last
updated: July 29, 2014 Build Ver: 6.40.03.39 Rev: o39