1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32 33 34
35
36 package ti.sysbios.family.arm.msp432;
37
38 import xdc.rov.ViewInfo;
39
40 /*!
41 * ======== ClockFreqs ========
42 * ClockFreqs Module.
43 *
44 * This module is used to define the ACLK, SMCLK, and HSMCLK frequencies in
45 * effect when BIOS_start() is called at the end of main(). It also provides
46 * runtime functions that can be used to query or set individual clock
47 * frequencies.
48 *
49 * If the application defines values for these three clocks, the application
50 * is responsible for setting up the clocks to the corresponding frequencies.
51 * This module will simply hold the values specified, for reference by other
52 * SYS/BIOS modules, or for query by the application at runtime.
53 *
54 * If the application configuration specifies (in its .cfg file) a value for
55 * one of these three clock frequencies, it must specify values for all three
56 * clocks; if it does not, a build error will be thrown.
57 *
58 * If the application does not define values for these clocks, the values will
59 * default either to the device reset values, or the boost values setup by
60 * the Boot module (ti.sysbios.family.arm.msp432.init.Boot). For example, if
61 * the application does not configure values for ClockFreq, and does not turn
62 * off the Boot module's default frequency boost, then the Boot module boost
63 * frequencies are used.
64 *
65 * If the application does not configure values for ClockFreq, and *does* turn
66 * off the Boot module's frequency boost (see snippet below), then the default
67 * reset frequency values will be used.
68 *
69 * @p(code)
70 * var Boot = xdc.module('ti.sysbios.family.arm.msp432.init.Boot');
71 * Boot.configureClocks = false;
72 * @p
73 *
74 * Currently the reset and Boot module boost values are fixed, as shown below.
75 *
76 * The default reset values are:
77 *
78 * @p(code)
79 * ACLK = 32768 Hz
80 * SMCLK = 3 MHz
81 * HSMCLK = 3 MHz
82 * @p
83 *
84 * The default Boot module boost values are:
85 *
86 * @p(code)
87 * ACLK = 32768 Hz
88 * SMCLK = 12 MHz
89 * HSMCLK = 24 MHz
90 * @p
91 *
92 * Note: This module only tracks the ACLK, SMCLK, and HSMCLK values. It does
93 * not track the CPU clock (MCLK) frequency. MCLK can be configured and
94 * queried with the BIOS module. For example, to configure the CPU
95 * frequency:
96 *
97 * var BIOS = xdc.useModule('ti.sysbios.BIOS');
98 * BIOS.cpuFreq.lo = 48000000;
99 * BIOS.cpuFreq.hi = 0;
100 * @p
101 *
102 * @p(html)
103 * <h3> Calling Context </h3>
104 * <table border="1" cellpadding="3">
105 * <colgroup span="1"></colgroup> <colgroup span="5" align="center"></colgroup>
106 *
107 * <tr><th> Function </th><th> Hwi </th><th> Swi </th><th> Task </th><th> Main </th><th> Startup </th></tr>
108 * <!-- -->
109 * <tr><td> {@link #getFrequency} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
110 * <tr><td> {@link #setFrequency} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
111 * <tr><td colspan="6"> Definitions: <br />
112 * <ul>
113 * <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
114 * <li> <b>Swi</b>: API is callable from a Swi thread. </li>
115 * <li> <b>Task</b>: API is callable from a Task thread. </li>
116 * <li> <b>Main</b>: API is callable from main(). </li>
117 * <li> <b>Startup</b>: API is callable during any module startup. </li>
118 * </ul>
119 * </td></tr>
120 *
121 * </table>
122 * @p
123 */
124
125
126 @Template("./ClockFreqs.xdt")
127
128
129 @DirectCall
130 module ClockFreqs
131 {
132 metaonly struct ModuleView {
133 UInt ACLK;
134 UInt SMCLK;
135 UInt HSMCLK;
136 }
137
138 @Facet
139 metaonly config ViewInfo.Instance rovViewInfo =
140 ViewInfo.create({
141 viewMap: [
142 [
143 'Module',
144 {
145 type: ViewInfo.MODULE,
146 viewInitFxn: 'viewInitModule',
147 structName: 'ModuleView'
148 }
149 ],
150 ]
151 });
152
153 /*! Clocks */
154 enum Clock {
155 Clock_ACLK,
156 Clock_SMCLK,
157 Clock_HSMCLK
158 };
159
160 /*! ACLK frequency (Hz) */
161 config UInt32 ACLK;
162
163 /*! SMCLK frequency (Hz) */
164 config UInt32 SMCLK;
165
166 /*! HSMCLK frequency (Hz) */
167 config UInt32 HSMCLK;
168
169 /*!
170 * ======== getFrequency ========
171 * Get the frequency for a clock.
172 *
173 */
174 UInt32 getFrequency(Clock clock);
175
176 /*!
177 * ======== setFrequency ========
178 * Set the frequency for a clock.
179 *
180 */
181 Void setFrequency(Clock clock, UInt32 frequency);
182
183 internal:
184
185 struct Module_State {
186 UInt32 ACLK;
187 UInt32 SMCLK;
188 UInt32 HSMCLK;
189 }
190 }