When the
idle configuration parameter is set, this function
will be added to the list of Idle loop functions. When called from the
Idle loop, it will transition the CPU into the idle mode specified
by the
idleMode configuration parameter. The CPU will stay
in the corresponding low power mode until the next interrupt occurs.
// Get this module's unique id
Bool Power_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Power_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Power_Module_getMask();
// Returns the diagnostics mask for this module
Void Power_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module