module ti.catalog.c2800.initF2837x.Boot

Soprano Boot Support

The Boot module supports boot initialization for the C28 Soprano cores. A special boot init function is created based on the configuration settings for this module. This function is hooked into the xdc.runtime.Reset.fxns[] array and called very early at boot time (prior to cinit processing). [ more ... ]
C synopsis target-domain sourced in ti/catalog/c2800/initF2837x/Boot.xdc
#include <ti/catalog/c2800/initF2837x/Boot.h>
Constants
extern const Bool 
 
DETAILS
The Boot module supports boot initialization for the C28 Soprano cores. A special boot init function is created based on the configuration settings for this module. This function is hooked into the xdc.runtime.Reset.fxns[] array and called very early at boot time (prior to cinit processing).
The code to support the boot module is placed in a separate section named ".text:.bootCodeSection" to allow placement of this section in the linker .cmd file if necessary. This section is a subsection of the ".text" section so this code will be placed into the .text section unless explicitly placed, either through Program.sectMap or through a linker command file.
 
config Boot_configureClocks  // module-wide

Clock configuration flag, default is false

C synopsis target-domain
extern const Bool Boot_configureClocks;
 
DETAILS
Set to true to configure the PLL and system subsystem clock dividers.
 
Configuration settings sourced in ti/catalog/c2800/initF2837x/Boot.xdc
var Boot = xdc.useModule('ti.catalog.c2800.initF2837x.Boot');
module-wide constants & types
 
 
    var obj = new Boot.ModuleView// ;
        obj.configureClocks = Bool  ...
        obj.OSCCLK = UInt  ...
        obj.SPLLIMULT = UInt  ...
        obj.SPLLFMULT = String  ...
        obj.SYSCLKDIVSEL = String  ...
        obj.bootCPU2 = Bool  ...
module-wide config parameters
 
 
 
metaonly enum Boot.FractMult

System PLL Fractional Multiplier (SPLLFMULT) value

Configuration settings
values of type Boot.FractMult
    const Boot.Fract_0;
    // Fractional multiplier is 0
    const Boot.Fract_25;
    // Fractional multiplier is 0.25
    const Boot.Fract_50;
    // Fractional multiplier is 0.5
    const Boot.Fract_75;
    // Fractional multiplier is 0.75
 
 
metaonly enum Boot.OscClk

Oscillator Clock Source Select Bit for OSCCLK

Configuration settings
values of type Boot.OscClk
    const Boot.OscClk_INTOSC2;
    // internal oscillator 2 (default on reset)
    const Boot.OscClk_XTAL;
    // external oscillator
    const Boot.OscClk_INTOSC1;
    // internal oscillator 1
    const Boot.OscClk_RESERVED;
    // reserved (default to INTOSC1)
 
 
metaonly struct Boot.ModuleView
Configuration settings
var obj = new Boot.ModuleView;
 
    obj.configureClocks = Bool  ...
    obj.OSCCLK = UInt  ...
    obj.SPLLIMULT = UInt  ...
    obj.SPLLFMULT = String  ...
    obj.SYSCLKDIVSEL = String  ...
    obj.bootCPU2 = Bool  ...
 
 
config Boot.configureClocks  // module-wide

Clock configuration flag, default is false

Configuration settings
Boot.configureClocks = Bool false;
 
DETAILS
Set to true to configure the PLL and system subsystem clock dividers.
C SYNOPSIS
 
metaonly config Boot.OSCCLK  // module-wide

OSCCLK input frequency to PLL, in MHz

Configuration settings
Boot.OSCCLK = UInt 10;
 
DETAILS
This is the frequency of the oscillator clock (OSCCLK) input to the PLL. The default internal oscillator is 10 Mhz.
 
metaonly config Boot.OSCCLKSRCSEL  // module-wide

Oscillator Clock source select bit for OSCCLK

Configuration settings
Boot.OSCCLKSRCSEL = Boot.OscClk Boot.OscClk_INTOSC2;
 
DETAILS
The default on reset is INTOSC2
 
metaonly config Boot.SPLLFMULT  // module-wide

System PLL Fractional Multiplier (SPLLFMULT) value

Configuration settings
Boot.SPLLFMULT = Boot.FractMult Boot.Fract_0;
 
 
metaonly config Boot.SPLLIMULT  // module-wide

System PLL Integer Multiplier (SPLLIMULT) value

Configuration settings
Boot.SPLLIMULT = UInt 1;
 
 
metaonly config Boot.SYSCLKDIVSEL  // module-wide

System Clock Divider Select (SYSCLKDIVSEL) value

Configuration settings
Boot.SYSCLKDIVSEL = UInt 2;
 
 
metaonly config Boot.bootCPU2  // module-wide

Initiate booting of the CPU2 processor. Default is false

Configuration settings
Boot.bootCPU2 = Bool false;
 
DETAILS
Set to true to enable CPU1 to initiate boot of CPU2.
If enabled, this will occur after the optional clock configuration step, enabled by configureClocks.
 
metaonly config Boot.bootFromFlash  // module-wide

Boot from Flash flag. Default is true

Configuration settings
Boot.bootFromFlash = Bool true;
 
DETAILS
Set to true to enable booting CPU1 from Flash.
 
metaonly config Boot.configSharedRAMs  // module-wide

Configure Shared RAM regions before booting the C28 processor. Default is true

Configuration settings
Boot.configSharedRAMs = Bool true;
 
DETAILS
Set to true to enable Shared RAM regions S0-S7, to set the owner of each region and the write access permissions for the onwer.
 
metaonly config Boot.configureFlashController  // module-wide

Flash controller configuration flag, default is true

Configuration settings
Boot.configureFlashController = Bool true;
 
DETAILS
Set to true to enable the configuration of the Flash controller wait states, program and data cache.
 
metaonly config Boot.configureFlashWaitStates  // module-wide

Flash controller wait states configuration flag, default is true

Configuration settings
Boot.configureFlashWaitStates = Bool true;
 
DETAILS
Set to true to configure the Flash controller wait states. The number of wait states is computed based upon the CPU frequency.
 
metaonly config Boot.disableWatchdog  // module-wide

Watchdog disable flag, default is false

Configuration settings
Boot.disableWatchdog = Bool false;
 
DETAILS
Set to true to disable the watchdog timer.
 
metaonly config Boot.enableFlashDataCache  // module-wide

Flash controller data cache enable flag, default is true

Configuration settings
Boot.enableFlashDataCache = Bool true;
 
DETAILS
Set to true to enable the Flash controller's data cache.
 
metaonly config Boot.enableFlashProgramCache  // module-wide

Flash controller program cache enable flag, default is true

Configuration settings
Boot.enableFlashProgramCache = Bool true;
 
DETAILS
Set to true to enable the Flash controller's program cache.
 
metaonly config Boot.limpAbortFunction  // module-wide

Function to be called when Limp mode is detected

Configuration settings
Boot.limpAbortFunction = Fxn undefined;
 
DETAILS
This function is called when the Boot module is about to configure the PLL, but finds the device operating in Limp mode (i.e., the mode when a missing OSCCLK input has been detected).
If this function is not specified by the application, a default function will be used, which spins in an infinite loop.
 
metaonly config Boot.loadSegment  // module-wide

Specifies where to load the flash function (include the 'PAGE' number)

Configuration settings
Boot.loadSegment = String undefined;
 
DETAILS
If 'configureFlashWaitStates' is true, then this parameter determines where the ".ti_catalog_c2800_initF2837x_flashfuncs" section gets loaded.
 
metaonly config Boot.rovViewInfo  // module-wide
Configuration settings
Boot.rovViewInfo = ViewInfo.Instance ViewInfo.create;
 
 
metaonly config Boot.runSegment  // module-wide

Specifies where to run the flash function (include the 'PAGE' number)

Configuration settings
Boot.runSegment = String undefined;
 
DETAILS
If 'configureFlashWaitStates' is true then this parameter determines where the ".ti_catalog_c2800_initF2837x_flashfuncs" section gets executed at runtime.
 
metaonly config Boot.sharedMemoryOwnerMask  // module-wide

Shared RAM owner select mask

Configuration settings
Boot.sharedMemoryOwnerMask = Bits32 0;
 
DETAILS
This parameter is used for writing the GSxMSEL register. By default, each value of each shared RAM select bit is '0'. This means the CPU1 is the owner and has write access. Setting a '1' in any bit position makes CPU2 the owner of that shared RAM segment.
generated on Thu, 25 May 2017 22:11:10 GMT