1 /* 2 * Copyright (c) 2014 Texas Instruments. All rights reserved. 3 * This program and the accompanying materials are made available under the 4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License 5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is 6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse 7 * Distribution License is available at 8 * http://www.eclipse.org/org/documents/edl-v10.php. 9 * 10 * Contributors: 11 * Texas Instruments - initial implementation 12 * */ 13 14 /* 15 * ======== Settings.xdc ======== 16 */ 17 18 package gnu.targets.arm.rtsv7M; 19 20 /*! 21 * ======== Settings ======== 22 * Collection of parameters relevant for this package as a whole 23 * 24 */ 25 26 module Settings { 27 28 /*! 29 * ======== bootOnly ======== 30 * Allow supplying only the boot code library 31 * 32 * This package can supply the boot code and the library with the 33 * implementation of xdc.runtime modules. If this parameter is set to 34 * `true`, only the boot code is supplied. Otherwise, both the boot code 35 * and the xdc.runtime implementation are supplied. 36 */ 37 metaonly config Bool bootOnly = false; 38 } 39 /* 40 * @(#) gnu.targets.arm.rtsv7M; 1, 0, 0,0; 5-12-2017 11:08:13; /db/ztree/library/trees/xdctargets/xdctargets-n04/src/ xlibrary 41 42 */ 43