module ti.sysbios.rts.iar.MultithreadSupport |
|
This Multithread support module uses Hook Functions, Hook Context
and an overloaded implementation of the library's lock and thread
local storage access functions to make C runtime library calls re-entrant
Multithread support will be enabled when IAR linker option "--threaded_lib"
is passed as the target's linker options prefix. This can be done in one
of the following ways:
- When building an application in IAR Embedded Workbench, under
Project -> Options -> General Options -> Library Configuration,
check the "Enable thread support in Library" box.
- When building an application through makefile using configuro, pass
the linker options on configuro command line using "--linkOptions"
option.
- When building an application through XDC build system using config.bld,
pass the linker options through the XDC target linkOpts.prefix in
config.bld.
[
more ... ]
#include <ti/sysbios/rts/iar/MultithreadSupport.h>
Functions common to all target modules |
|
|
DETAILS
Multithread support will be enabled when IAR linker option "--threaded_lib"
is passed as the target's linker options prefix. This can be done in one
of the following ways:
- When building an application in IAR Embedded Workbench, under
Project -> Options -> General Options -> Library Configuration,
check the "Enable thread support in Library" box.
- When building an application through makefile using configuro, pass
the linker options on configuro command line using "--linkOptions"
option.
- When building an application through XDC build system using config.bld,
pass the linker options through the XDC target linkOpts.prefix in
config.bld.
Note: Calling C runtime functions from SWI and HWI threads
is not supported and will generate an exception if
multithread support is enabled.
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool MultithreadSupport_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool MultithreadSupport_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 MultithreadSupport_Module_getMask();
// Returns the diagnostics mask for this module
Void MultithreadSupport_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var MultithreadSupport = xdc.useModule('ti.sysbios.rts.iar.MultithreadSupport');
module-wide config parameters
generated on Tue, 14 Feb 2017 19:59:46 GMT