1    /*
     2     * Copyright (c) 2015, Texas Instruments Incorporated
     3     * All rights reserved.
     4     *
     5     * Redistribution and use in source and binary forms, with or without
     6     * modification, are permitted provided that the following conditions
     7     * are met:
     8     *
     9     * *  Redistributions of source code must retain the above copyright
    10     *    notice, this list of conditions and the following disclaimer.
    11     *
    12     * *  Redistributions in binary form must reproduce the above copyright
    13     *    notice, this list of conditions and the following disclaimer in the
    14     *    documentation and/or other materials provided with the distribution.
    15     *
    16     * *  Neither the name of Texas Instruments Incorporated nor the names of
    17     *    its contributors may be used to endorse or promote products derived
    18     *    from this software without specific prior written permission.
    19     *
    20     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    21     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    22     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    23     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    24     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    25     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    26     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    27     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    28     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    29     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    30     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    31     */
    32    /*
    33     *  ======== IHwi.xdc ========
    34     *
    35     */
    36    
    37    import xdc.runtime.Error;
    38    
    39    
    40    /*!
    41     *  ======== Hwi ========
    42     *  Hardware Interrupt Support Module.
    43     *
    44     *  The IHwi interface specifies APIs for globally enabling, disabling, and
    45     *  restoring interrupts.
    46     *
    47     *  Additionally, management of individual, device-specific hardware 
    48     *  interrupts is provided.
    49     *
    50     *  The user can statically or dynamically assign routines that run when 
    51     *  specific hardware interrupts occur. 
    52     *
    53     *  Dynamic assignment of Hwi routines to interrupts at run-time is done 
    54     *  using the Hwi_create function.
    55     *
    56     *  Interrupt routines can be written completely in C, completely in 
    57     *  assembly, or in a mix of C and assembly. In order to support interrupt
    58     *  routines
    59     *  written completely in C, an interrupt dispatcher is provided that performs
    60     *  the requisite prolog and epilog for an interrupt routine.
    61     *
    62     *  Some routines are assigned to interrupts by the other SYS/BIOS
    63     *  modules. For example, the Clock module configures its own timer interrupt
    64     *  handler. See the Clock Module for more details.
    65     *
    66     *  @a(Runtime Hwi Creation)
    67     *
    68     *  Below is an example of configuring an interrupt at runtime. 
    69     *  Usually this code would be placed in main().
    70     *
    71     *  @p(code)
    72     *  #include <xdc/runtime/Error.h>
    73     *  #include <ti/sysbios/hal/Hwi.h>
    74     *  
    75     *  Hwi_Handle myHwi;
    76     *  
    77     *  Int main(Int argc, char* argv[])
    78     *  {
    79     *      Hwi_Params hwiParams;
    80     *      Error_Block eb;
    81     *   
    82     *      Hwi_Params_init(&hwiParams);
    83     *      Error_init(&eb);
    84     *  
    85     *      // set the argument you want passed to your ISR function
    86     *      hwiParams.arg = 1;        
    87     *   
    88     *      // set the event id of the peripheral assigned to this interrupt
    89     *      hwiParams.eventId = 10;   
    90     *   
    91     *      // don't allow this interrupt to nest itself
    92     *      hwiParams.maskSetting = Hwi_MaskingOption_SELF;
    93     *   
    94     *      // 
    95     *      // Configure interrupt 5 to invoke "myIsr".
    96     *      // Automatically enables interrupt 5 by default
    97     *      // set params.enableInt = FALSE if you want to control
    98     *      // when the interrupt is enabled using Hwi_enableInterrupt()
    99     *      //
   100     *   
   101     *      myHwi = Hwi_create(5, myIsr, &hwiParams, &eb);
   102     *   
   103     *      if (Error_check(&eb)) {
   104     *          // handle the error
   105     *      }
   106     *  }
   107     *   
   108     *  Void myIsr(UArg arg)
   109     *  {
   110     *      // here when interrupt #5 goes off
   111     *  }
   112     *  @p
   113     *
   114     *  @a(Hook Functions)
   115     *
   116     *  Sets of hook functions can be specified for the Hwi module
   117     *  using the configuration tool.  Each set contains these hook
   118     *  functions:
   119     *  @p(blist)
   120     *  -Register:  A function called before any statically-created Hwis
   121     *      are initialized at runtime.  The register hook is called at boot time
   122     *      before main() and before interrupts are enabled.
   123     *  -Create:    A function that is called when a Hwi is created.
   124     *      This includes hwis that are created statically and those
   125     *      created dynamically using {@link #create Hwi_create}.
   126     *  -Begin:     A function that is called just prior to running a Hwi.
   127     *  -End:       A function that is called just after a Hwi finishes.
   128     *  -Delete:    A function that is called when a Hwi is deleted at
   129     *      run-time with {@link #delete Hwi_delete}.
   130     *  @p
   131     *
   132     *  Register Function
   133     *
   134     *  The Register function is provided to allow a hook set to store its
   135     *  hookset ID.  This id can be passed to 
   136     *  {@link #setHookContext Hwi_setHookContext} and
   137     *  {@link #getHookContext Hwi_getHookContext} to set or get 
   138     *  hookset-specific context.  The
   139     *  Register function must be specified if the hook implementation
   140     *  needs to use {@link #setHookContext  Hwi_setHookContext} or 
   141     *  {@link #getHookContext  Hwi_getHookContext}.
   142     *  The registerFxn hook function is called during system initialization
   143     *  before interrupts have been enabled.
   144     *
   145     *  @p(code)
   146     *  Void myRegisterFxn(Int id);
   147     *  @p
   148     *
   149     *  Create and Delete Functions
   150     * 
   151     *  The create and delete functions are called whenever a Hwi is created
   152     *  or deleted.  They are called with interrupts enabled (unless called 
   153     *  at boot time or from main()).
   154     *
   155     *  @p(code)
   156     *  Void myCreateFxn(Hwi_Handle hwi, Error_Block *eb);
   157     *  @p
   158     *
   159     *  @p(code)
   160     *  Void myDeleteFxn(Hwi_Handle hwi);
   161     *  @p
   162     *
   163     *  Begin and End Functions
   164     *
   165     *  The beginFxn and endFxn function hooks are called with interrupts
   166     *  globally disabled, therefore any hook processing function will contribute
   167     *  to the overall system interrupt response latency.  In order to minimize
   168     *  this impact, carefully consider the processing time spent in an Hwi
   169     *  beginFxn or endFxn function hook.
   170     *
   171     *  @p(code)
   172     *  Void myBeginFxn(Hwi_Handle hwi);
   173     *  @p
   174     *
   175     *  @p(code)
   176     *  Void myEndFxn(Hwi_Handle hwi);
   177     *  @p
   178     *
   179     *  Hook functions can only be configured statically.
   180     */
   181    
   182    @DirectCall
   183    @InstanceFinalize
   184    @InstanceInitError
   185    
   186    interface IHwi {
   187    
   188        // -------- Module Types --------
   189    
   190        /*! Hwi create function type definition. */
   191        typedef Void (*FuncPtr)(UArg);
   192        
   193        /*! 
   194         * Interrupt Return Pointer.
   195         *
   196         * This is the address of the interrupted instruction.
   197         */
   198        typedef UArg Irp;
   199       
   200        /*! 
   201         *  Hwi hook set type definition. 
   202         *
   203         *  The functions that make up a hookSet have certain restrictions. They
   204         *  cannot call any Hwi instance functions other than Hwi_getHookContext()
   205         *  and Hwi_setHookContext(). For all practical purposes, they should treat
   206         *  the Hwi_Handle passed to these functions as an opaque handle.
   207         */
   208        struct HookSet {
   209            Void (*registerFxn)(Int);
   210            Void (*createFxn)(Handle, Error.Block *);
   211            Void (*beginFxn)(Handle);
   212            Void (*endFxn)(Handle);
   213            Void (*deleteFxn)(Handle);
   214        };
   215        
   216        /*!
   217         *  ======== MaskingOption ========
   218         *  Shorthand interrupt masking options
   219         *
   220         *  @value(MaskingOption_NONE)      No interrupts are disabled
   221         *
   222         *  @value(MaskingOption_ALL)       All interrupts are disabled
   223         *
   224         *  @value(MaskingOption_SELF)      Only this interrupt is disabled
   225         *
   226         *  @value(MaskingOption_BITMASK)   User supplies interrupt enable masks
   227         *
   228         *  @value(MaskingOption_LOWER)     All current and lower priority
   229         *                                  interrupts are disabled.
   230         *
   231         *                                  Only a few targets/devices truly
   232         *                                  support this masking option. For those
   233         *                                  that don't, this setting is treated
   234         *                                  the same as MaskingOption_SELF.
   235         */
   236        enum MaskingOption {
   237            MaskingOption_NONE,
   238            MaskingOption_ALL, 
   239            MaskingOption_SELF,
   240            MaskingOption_BITMASK,
   241            MaskingOption_LOWER
   242        };
   243    
   244        /*!
   245         *  ======== StackInfo ========
   246         *  Structure contains Hwi stack usage info 
   247         *
   248         *  Used by getStackInfo() and viewGetStackInfo() functions
   249         */
   250        struct StackInfo {
   251            SizeT hwiStackPeak;
   252            SizeT hwiStackSize;
   253            Ptr hwiStackBase;
   254        };
   255    
   256        // -------- Module Parameters --------
   257    
   258        /*!
   259         *  Include interrupt nesting logic in interrupt dispatcher?
   260         *
   261         *  Default is true.
   262         *
   263         *  This option provides the user with the ability to optimize
   264         *  interrupt dispatcher performance when support for interrupt
   265         *  nesting is not required.
   266         *
   267         *  Setting this parameter to false will disable the logic in
   268         *  the interrupt dispatcher that manipulates interrupt mask
   269         *  registers and enables and disables interrupts before and
   270         *  after invoking the user's Hwi function. 
   271         *
   272         *  Set this parameter to false if you don't need interrupts 
   273         *  enabled during the execution of your Hwi functions.
   274         */
   275        config Bool dispatcherAutoNestingSupport = true;
   276    
   277        /*!
   278         *  Include Swi scheduling logic in interrupt dispatcher?
   279         *
   280         *  Default is inherited from {@link ti.sysbios.BIOS#swiEnabled 
   281         *  BIOS.swiEnabled}, which is true by default.
   282         *
   283         *  This option provides the user with the ability to optimize
   284         *  interrupt dispatcher performance when it is known that Swis
   285         *  will not be posted from any of their Hwi threads.
   286         *
   287         *  @a(Warning)
   288         *  Setting this parameter to false will disable the logic in
   289         *  the interrupt dispatcher that invokes the Swi scheduler
   290         *  prior to returning from an interrupt.
   291         *  With this setting, Swis MUST NOT be posted from Hwi functions!
   292         */
   293        config Bool dispatcherSwiSupport;
   294    
   295        /*!
   296         *  Include Task scheduling logic in interrupt dispatcher?
   297         *
   298         *  Default is inherited from {@link ti.sysbios.BIOS#taskEnabled 
   299         *  BIOS.taskEnabled}, which is true by default.
   300         *
   301         *  This option provides the user with the ability to optimize
   302         *  interrupt dispatcher performance when it is known that no
   303         *  Task scheduling APIs (ie {@link ti.sysbios.knl.Semaphore#post 
   304         *  Semaphore_post()}) will be executed from any of their Hwi threads.
   305         *
   306         *  Setting this parameter to false will disable the logic in
   307         *  the interrupt dispatcher that invokes the Task scheduler
   308         *  prior to returning from an interrupt.
   309         */
   310        config Bool dispatcherTaskSupport;
   311    
   312        /*!
   313         *  Controls whether the
   314         *  dispatcher retains the interrupted thread's return address.
   315         *
   316         *  This option is enabled by default.
   317         *
   318         *  Setting this parameter to false will disable the logic in
   319         *  the interrupt dispatcher that keeps track of the interrupt's
   320         *  return address and provide a small savings in interrupt latency.
   321         *
   322         *  The application can get an interrupt's most recent return
   323         *  address using the {@link #getIrp} API.
   324         */
   325        config Bool dispatcherIrpTrackingSupport = true;
   326    
   327        // -------- Module Functions --------
   328    
   329        /*!
   330         *  ======== addHookSet ========
   331         *  addHookSet is used in a config file to add a hook set (defined
   332         *  by struct HookSet).
   333         *
   334         *  HookSet structure elements may be omitted, in which case those
   335         *  elements will not exist.
   336         *
   337         *  @param(hook)    structure of type HookSet
   338         */
   339        metaonly Void addHookSet(HookSet hook);
   340    
   341        /*!
   342         *  ======== viewGetStackInfo ========
   343         *  @_nodoc
   344         *  Returns the Hwi stack usage info. Used at ROV time.
   345         *
   346         *  @b(returns)     Hwi stack base, size, peak
   347         */
   348        metaonly StackInfo viewGetStackInfo();
   349    
   350        /*!
   351         *  ======== getStackInfo ========
   352         *  Get Hwi stack usage Info.
   353         *
   354         *  getStackInfo returns the Hwi stack usage info to its calling 
   355         *  function by filling stack base address, stack size and stack
   356         *  peak fields in the {@link #StackInfo} structure.
   357         *
   358         *  getStackInfo accepts two arguments, a pointer to a structure
   359         *  of type {@link #StackInfo} and a boolean. If the boolean is set
   360         *  to true, the function computes the stack depth and fills the 
   361         *  stack peak field in the StackInfo structure. If a stack overflow
   362         *  is detected, the stack depth is not computed. If the boolean is 
   363         *  set to false, the function only checks for a stack overflow.
   364         *
   365         *  The isr stack is always checked for an overflow and a boolean
   366         *  is returned to indicate whether an overflow occured.
   367         *
   368         *  Below is an example of calling getStackInfo() API:
   369         *
   370         *  @p(code)
   371         *  #include <ti/sysbios/BIOS.h>
   372         *  #include <ti/sysbios/hal/Hwi.h>
   373         *  #include <ti/sysbios/knl/Swi.h>
   374         *  #include <ti/sysbios/knl/Task.h>
   375         *
   376         *  Swi_Handle swi0;
   377         *  volatile Bool swiStackOverflow = FALSE;
   378         *
   379         *  Void swi0Fxn(UArg arg1, UArg arg2)
   380         *  {
   381         *      Hwi_StackInfo stkInfo;
   382         *
   383         *      // Request stack depth
   384         *      swiStackOverflow = Hwi_getStackInfo(&stkInfo, TRUE);
   385         * 
   386         *      // Alternately, we can omit the request for stack depth and 
   387         *      // request only the stack base and stack size (the check for
   388         *      // stack overflow is always performed):
   389         *      //
   390         *      // swiStackOverflow = Hwi_getStackInfo(&stkInfo, FALSE);
   391         *
   392         *      if (swiStackOverflow) {
   393         *          // isr Stack Overflow detected
   394         *      }
   395         *  }
   396         *
   397         *  Void idleTask()
   398         *  {
   399         *      Swi_post(swi0);
   400         *  }
   401         *
   402         *  Int main(Int argc, char* argv[])
   403         *  {
   404         *      swi0 = Swi_create(swi0Fxn, NULL, NULL);
   405         *
   406         *      BIOS_start();
   407         *      return (0);
   408         *  }
   409         *  @p
   410         *
   411         *  @param(stkInfo) pointer to structure of type {@link #StackInfo}
   412         *  @param(computeStackDepth)       decides whether to compute stack depth
   413         *
   414         *  @b(returns)     boolean to indicate a stack overflow
   415         */
   416        Bool getStackInfo(StackInfo *stkInfo, Bool computeStackDepth);
   417    
   418        /*!
   419         *  ======== getCoreStackInfo ========
   420         *  Get Hwi stack usage Info for the specified coreId.
   421         *
   422         *  getCoreStackInfo returns the Hwi stack usage info for the specified
   423         *  coreId to its calling function by filling stack base address,
   424         *  stack size and stack peak fields in the {@link #StackInfo} structure.
   425         *
   426         *  This function should be used only in applications built with
   427         *  {@link ti.sysbios.BIOS#smpEnabled} set to true.
   428         *
   429         *  getCoreStackInfo accepts three arguments, a pointer to a structure
   430         *  of type {@link #StackInfo}, a boolean and a coreId. If the boolean
   431         *  is set to true, the function computes the stack depth and fills the
   432         *  stack peak field in the StackInfo structure. If a stack overflow
   433         *  is detected, the stack depth is not computed. If the boolean is
   434         *  set to false, the function only checks for a stack overflow.
   435         *
   436         *  The isr stack is always checked for an overflow and a boolean
   437         *  is returned to indicate whether an overflow occured.
   438         *
   439         *  Below is an example of calling getCoreStackInfo() API:
   440         *
   441         *  @p(code)
   442         *  #include <ti/sysbios/BIOS.h>
   443         *  #include <ti/sysbios/hal/Hwi.h>
   444         *  #include <ti/sysbios/hal/Core.h>
   445         *  #include <ti/sysbios/knl/Task.h>
   446         *
   447         *  ...
   448         *
   449         *  Void idleTask()
   450         *  {
   451         *      UInt idx;
   452         *      Hwi_StackInfo stkInfo;
   453         *      Bool stackOverflow = FALSE;
   454         *
   455         *      // Request stack depth for each core's Hwi stack and check for
   456         *      // overflow
   457         *      for (idx = 0; idx < Core_numCores; idx++) {
   458         *          stackOverflow = Hwi_getCoreStackInfo(&stkInfo, TRUE, idx);
   459         *
   460         *          // Alternately, we can omit the request for stack depth and
   461         *          // request only the stack base and stack size (the check for
   462         *          // stack overflow is always performed):
   463         *          //
   464         *          // stackOverflow = Hwi_getCoreStackInfo(&stkInfo, FALSE, idx);
   465         *
   466         *          if (stackOverflow) {
   467         *              // isr Stack Overflow detected
   468         *          }
   469         *      }
   470         *  }
   471         *
   472         *  Int main(Int argc, char* argv[])
   473         *  {
   474         *      ...
   475         *      BIOS_start();
   476         *      return (0);
   477         *  }
   478         *  @p
   479         *
   480         *  @param(stkInfo)     pointer to structure of type {@link #StackInfo}
   481         *  @param(computeStackDepth)       decides whether to compute stack depth
   482         *  @param(coreId)      core whose stack info needs to be retrieved
   483         *
   484         *  @b(returns)         boolean to indicate a stack overflow
   485         */
   486        Bool getCoreStackInfo(StackInfo *stkInfo, Bool computeStackDepth,
   487            UInt coreId);
   488    
   489        /*!
   490         *  ======== startup ========
   491         *  Initially enable interrupts
   492         *
   493         *  Called within BIOS_start
   494         */
   495        Void startup();
   496    
   497        /*!
   498         *  ======== disable ========
   499         */
   500        UInt disable();
   501    
   502        /*!
   503         *  ======== enable ========
   504         *  Globally enable interrupts.
   505         *
   506         *  Hwi_enable globally enables hardware interrupts and returns an
   507         *  opaque key indicating whether interrupts were globally enabled or
   508         *  disabled on entry to Hwi_enable(). 
   509         *  The actual value of the key is target/device specific and is meant 
   510         *  to be passed to Hwi_restore(). 
   511         *
   512         *
   513         *  This function is 
   514         *  called as part of SYS/BIOS Startup_POST_APP_MAIN phase.
   515         *
   516         *  Hardware interrupts are enabled unless a call to Hwi_disable disables
   517         *  them. 
   518         *
   519         *  Servicing of interrupts that occur while interrupts are disabled is
   520         *  postponed until interrupts are reenabled. However, if the same type 
   521         *  of interrupt occurs several times while interrupts are disabled, 
   522         *  the interrupt's function is executed only once when interrupts are 
   523         *  reenabled.
   524         *
   525         *  A context switch can occur when calling Hwi_enable or Hwi_restore if
   526         *  an enabled interrupt occurred while interrupts are disabled.
   527         *
   528         *  Any call to Hwi_enable enables interrupts, even if Hwi_disable has 
   529         *  been called several times.
   530         *
   531         *  Hwi_enable must not be called from main().
   532         *
   533         *  @b(returns)     opaque key for use by Hwi_restore()
   534         */
   535        UInt enable();
   536    
   537        /*!
   538         *  ======== restore ========
   539         *  Globally restore interrupts.
   540         *
   541         *  Hwi_restore globally restores interrupts to the state determined 
   542         *  by the key argument provided by a previous invocation of Hwi_disable.
   543         *
   544         *  A context switch may occur when calling Hwi_restore if Hwi_restore
   545         *  reenables interrupts and another Hwi occurred while interrupts were 
   546         *  disabled.
   547         *
   548         *  Hwi_restore may be called from main(). However, since Hwi_enable
   549         *  cannot be called from main(), interrupts are always disabled in 
   550         *  main(), and a call to Hwi_restore has no effect.
   551         *
   552         *  @param(key)     enable/disable state to restore
   553         */
   554        Void restore(UInt key);
   555    
   556        /*!
   557         *  @_nodoc
   558         *  ======== switchFromBootStack ========
   559         *  Indicate that we are leaving the boot stack and
   560         *  are about to switch to a task stack.
   561         *  Used by Task_startup()
   562         */
   563        Void switchFromBootStack();
   564    
   565        /*!
   566         *  ======== post ========
   567         *  Generate an interrupt for test purposes.
   568         *
   569         *  @param(intNum)      ID of interrupt to generate
   570         */
   571        Void post(UInt intNum);
   572    
   573        /*!
   574         *  @_nodoc
   575         *  ======== getTaskSP ========
   576         *  retrieve interrupted task's SP
   577         *
   578         *  Used for benchmarking the SYS/BIOS Hwi dispatcher's task 
   579         *  stack utilization.
   580         *
   581         *  @b(returns)     interrupted task's SP
   582         */
   583        Char *getTaskSP();
   584    
   585        /*
   586         *  @_nodoc
   587         *  The following two target-unique Hwi APIs must be called
   588         *  directly in order to work properly. Thus they are not
   589         *  published here in order to bypass the multi-layered indirect function
   590         *  calls (__E, __F) that would arise if they appeared in this spec file.
   591         *
   592         *  These APIs must be implemented by the target Hwi modules and must be
   593         *  given these EXACT names.
   594         *
   595         *  The two functions, switchToIsrStack() and switchToTaskStack() must
   596         *  work in tandem to insure that only the first order (ie non nested) 
   597         *  invocation of these APIs result in the switch to the ISR stack and 
   598         *  the switch back to the task stack. The opaque char * token returned 
   599         *  by switchToIsrStack() and passed to switchToTaskStack() is provided
   600         *  purely for implementation efficiency and thus can have implementation
   601         *  dependent definitions.
   602         */
   603    
   604        /*
   605         *  @_nodoc
   606         *  ======== switchAndRunFunc ========
   607         *  If not on ISR stack already, switch to it, then call
   608         *  the function whose address is passed as an argument
   609         *  and then switch back to Task stack.
   610         *
   611         *  Used by the Swi scheduler.
   612         *
   613         *  This function must be implemented by all Hwi modules
   614         *  name) because it can't be _E and _F'd due to its
   615         *  inherent stack switching behavior.
   616         *
   617         *  @a(param)       Function pointer
   618         */
   619        /*  Char *ti_bios_family_xxx_Hwi_switchAndRunFunc(); */
   620    
   621        /*
   622         *  @_nodoc
   623         *  ======== switchToIsrStack ========
   624         *  If not on ISR stack already, switch to it.
   625         *  Used by the Swi scheduler and interrupt dispatcher.
   626         *
   627         *  This function must be implemented by all Hwi modules
   628         *  name) because it can't be _E and _F'd due to its
   629         *  inherent stack switching behavior.
   630         *  
   631         *  @b(returns)     token to use with 
   632         *                  switchToTaskStack()
   633         */
   634        /*  Char *ti_bios_family_xxx_Hwi_switchToIsrStack(); */
   635    
   636        /*
   637         *  @_nodoc
   638         *  ======== switchToTaskStack ========
   639         *  If at bottom of ISR stack, switch to Task stack.
   640         *  Used by the Swi scheduler and interrupt dispatcher.
   641         *  
   642         *  This function must be implemented by all Hwi modules
   643         *  and be given this exact name (without a target-specific
   644         *  name) because it can't be _E and _F'd due to its
   645         *  inherent stack switching behavior.
   646         *  
   647         *  @param(key)     token returned by
   648         *                  switchToIsrStack()
   649         */
   650        /*  Void ti_bios_family_xxx_Hwi_switchToTaskStack(Char *key); */
   651    
   652        /*!
   653         *  ======== disableInterrupt ========
   654         *  Disable a specific interrupt.
   655         *
   656         *  Disable a specific interrupt identified by an interrupt number.
   657         *
   658         *  @param(intNum)  interrupt number to disable
   659         *  @b(returns)     key to restore previous enable/disable state
   660         */
   661        UInt disableInterrupt(UInt intNum);
   662    
   663        /*!
   664         *  ======== enableInterrupt ========
   665         *  Enable a specific interrupt.
   666         *
   667         *  Enables a specific interrupt identified by an interrupt number.
   668         *
   669         *  @param(intNum)  interrupt number to enable
   670         *  @b(returns)     key to restore previous enable/disable state
   671         */
   672        UInt enableInterrupt(UInt intNum);
   673    
   674        /*!
   675         *  ======== restoreInterrupt ========
   676         *  Restore a specific interrupt's enabled/disabled state.
   677         *
   678         *  Restores a specific interrupt identified by an interrupt number.
   679         *  restoreInterrupt is generally used to restore an interrupt to its state
   680         *  before {@link #disableInterrupt} or {@link #enableInterrupt} was
   681         *  invoked
   682         *
   683         *  @param(intNum)  interrupt number to restore
   684         *  @param(key)     key returned from enableInt or disableInt
   685         */
   686        Void restoreInterrupt(UInt intNum, UInt key);
   687    
   688        /*!
   689         *  ======== clearInterrupt ========
   690         *  Clear a specific interrupt.
   691         *
   692         *  Clears a specific interrupt's pending status.
   693         *  The implementation is family-specific.
   694         *
   695         *  @param(intNum)  interrupt number to clear
   696         */
   697        Void clearInterrupt(UInt intNum);
   698    
   699    instance:
   700    
   701        /*!
   702         *  Create a dispatched interrupt.
   703         *
   704         *  A Hwi dispatcher table entry is created and filled with the 
   705         *  function specified by the fxn parameter and the attributes 
   706         *  specified by the params parameter.
   707         *
   708         *  If params is NULL, the Hwi's dispatcher properties are assigned a 
   709         *  default set of values. Otherwise, the following properties
   710         *  are specified by a structure of type Hwi_Params.
   711         *
   712         *  @p(blist)
   713         *  - The arg element is a generic argument that is passed to the plugged
   714         *  function as its only parameter. The default value is 0.
   715         *  - The enableInt element determines whether the interrupt should be
   716         *  enabled in the IER by create.
   717         *  - The maskSetting element defines the dispatcherAutoNestingSupport 
   718         *  behavior of the interrupt.
   719         *  @p
   720         *  
   721         *  Hwi_create returns a pointer to the created Hwi object.
   722         *
   723         *  @param(intNum)  interrupt number
   724         *  @param(hwiFxn)  pointer to ISR function
   725         *
   726         */
   727        create(Int intNum, FuncPtr hwiFxn);
   728    
   729        /*! maskSetting. Default is {@link #MaskingOption Hwi_MaskingOption_SELF} */
   730        config MaskingOption maskSetting = MaskingOption_SELF;
   731    
   732        /*! ISR function argument. Default is 0. */
   733        config UArg arg = 0;
   734    
   735        /*! Enable this interrupt when object is created? Default is true. */
   736        config Bool enableInt = true;
   737        
   738        /*! 
   739         *  Interrupt event ID (Interrupt Selection Number)
   740         *
   741         *  Default is -1. 
   742         *  Not all targets/devices support this instance parameter. 
   743         *  On those that don't, this parameter is ignored.
   744         */
   745        config Int eventId = -1;
   746    
   747        /*! 
   748         *  Interrupt priority.
   749         *
   750         *  The default value of -1 is used as a flag to indicate 
   751         *  the lowest (logical) device-specific priority value.
   752         *
   753         *  Not all targets/devices support this instance parameter. 
   754         *  On those that don't, this parameter is ignored.
   755         */
   756        config Int priority = -1;
   757    
   758        /*!
   759         *  ======== getFunc ========
   760         *  Get Hwi function and arg
   761         *
   762         *  @param(arg)     pointer for returning hwi's ISR function argument
   763         *  @b(returns)     hwi's ISR function
   764         */
   765        FuncPtr getFunc(UArg *arg);
   766    
   767        /*!
   768         *  ======== setFunc ========
   769         *  Overwrite Hwi function and arg
   770         *
   771         *  Replaces a Hwi object's hwiFxn function originally
   772         *  provided in {@link #create}.
   773         *
   774         *  @param(fxn)     pointer to ISR function
   775         *  @param(arg)     argument to ISR function
   776         */
   777        Void setFunc(FuncPtr fxn, UArg arg);
   778    
   779        /*!
   780         *  ======== getHookContext ========
   781         *  Get hook instance's context for a Hwi.
   782         *
   783         *  @b(returns)     hook instance's context for hwi
   784         */
   785        Ptr getHookContext(Int id);
   786    
   787        /*!
   788         *  ======== setHookContext ========
   789         *  Set hook instance's context for a Hwi.
   790         *
   791         *  @param(id)            hook instance's ID
   792         *  @param(hookContext)   value to write to context
   793         */
   794        Void setHookContext(Int id, Ptr hookContext);
   795    
   796        /*!
   797         *  ======== getIrp ========
   798         *  Get address of interrupted instruction.
   799         *
   800         *  @b(returns)     most current IRP of a Hwi
   801         */
   802        Irp getIrp();
   803    }