1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32
33 34 35
36 package ti.platforms.tms320x28;
37
38 /*!
39 * ======== Platform ========
40 * A generic platform that supports any TMS320x28 device
41 *
42 * The device to be used by this platform is passed as the platform instance
43 * name. On the `xdc.tools.configuro` command line, it is done in the
44 * following way:
45 * @p(code)
46 * xs xdc.tools.configuro ... -p "ti.platforms.tms320x28:TMS320C2812"
47 * @p
48 *
49 * In package.bld, the platform instance is selected as in:
50 * @p(code)
51 * Pkg.addExecutable("test", target, "ti.platforms.tms320x28:TMS320C2812");
52 * @p
53 */
54 metaonly module Platform inherits xdc.platform.IPlatform
55 {
56 config xdc.platform.IPlatform.Board BOARD = {
57 id: "0",
58 boardName: "tms320x28",
59 boardFamily: null,
60 boardRevision: null
61 };
62
63 /*!
64 * ======== nameFormat ========
65 * Encoding of instance creation parameters in the instance's name
66 *
67 * For this platform, the parameters `deviceName`, `includeLinkCmdFile`
68 * and `clockRate` can be encoded in the instance name supplied on
69 * `xdc.tools.configuro` command line, for example:
70 * @p(code)
71 * xs xdc.tools.configuro ... -p ti.platforms.tms320x28:TMS320F28035:1:60
72 * @p
73 * Optional parameters can be omitted:
74 * @p(code)
75 * xs xdc.tools.configuro ... -p ti.platforms.tms320x28:TMS320F28035
76 * @p
77 */
78 readonly config string nameFormat
79 = "$(deviceName):$(includeLinkCmdFile):$(clockRate)";
80
81 /*!
82 * ======== genAliases ========
83 * Generate symbol mapping for TI Tools 6.0 or newer
84 */
85 config Bool genAliases = true;
86
87 instance:
88
89 config xdc.platform.IExeContext.Cpu CPU = {
90 id: "0",
91 clockRate: 0,
92 catalogName: "ti.catalog.c2800",
93 deviceName: "TMS320F28069",
94 revision: null,
95 };
96
97 /*!
98 * ======== deviceName ========
99 * The name of an `ICpuDataSheet` module for the device
100 *
101 * This parameter is required, but it does not have to be set explicitly;
102 * it can be encoded in the instance's name.
103 */
104 config string deviceName;
105
106 /*!
107 * ======== clockRate ========
108 * The clock rate for this device.
109 */
110 config Double clockRate = 0;
111
112 override config string codeMemory = null;
113
114 override config string dataMemory = null;
115
116 override config string stackMemory = null;
117
118 /*!
119 * ======== includeLinkCmdFile ========
120 * The flag that specifies if the platform should include a linker command
121 * file.
122 *
123 * By default, a user is responsible for adding a linker command file to
124 * the project, or to the linker command line. However, if this flag is
125 * set, this platform will include a default linker command file for the
126 * selected device.
127 */
128 config Bool includeLinkCmdFile = false;
129 };