1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32
33 34 35
36 package ti.platforms.concertoC28;
37
38 /*!
39 * ======== Platform ========
40 * A generic platform that supports any Stellaris device
41 *
42 * The device to be used by this platform is passed as the platform instance
43 * name. On the `xdc.tools.configuro` command line, it is done in the
44 * following way:
45 * @p(code)
46 * xs xdc.tools.configuro ... -p "ti.platforms.concertoC28:F28M35H52C1"
47 * @p
48 *
49 * In package.bld, the platform instance is selected as in:
50 * @p(code)
51 * Pkg.addExecutable("test", target, "ti.platforms.concertoC28:F28M35H52C1");
52 * @p
53 */
54 metaonly module Platform inherits xdc.platform.IPlatform
55 {
56 config xdc.platform.IPlatform.Board BOARD = {
57 id: "0",
58 boardName: "concertoC28",
59 boardFamily: null,
60 boardRevision: null
61 };
62
63 /*!
64 * ======== nameFormat ========
65 * Encoding of instance creation parameters in the instance's name
66 *
67 * For this platform, the parameters `deviceName`, `includeLinkCmdFile`
68 * and `clockRate` can be encoded in the instance name supplied on
69 * `xdc.tools.configuro` command line, for example:
70 * @p(code)
71 * xs xdc.tools.configuro ... -p ti.platforms.concertoC28:F28M35H52C1:1:150
72 * @p
73 * Optional parameters can be omitted:
74 * @p(code)
75 * xs xdc.tools.configuro ... -p ti.platforms.concertoC28:F28M35H52C1
76 * @p
77 */
78 readonly config string nameFormat =
79 "$(deviceName):$(includeLinkCmdFile):$(clockRate)";
80
81 instance:
82
83 config xdc.platform.IExeContext.Cpu CPU = {
84 id: "0",
85 clockRate: 1.0,
86 catalogName: "ti.catalog.c2800",
87 deviceName: "F28M35x",
88 revision: "",
89 };
90
91 /*!
92 * ======== deviceName ========
93 * The name of an `ICpuDataSheet` module for the device
94 *
95 * This parameter is required, but it does not have to be set explicitly;
96 * it can be encoded in the instance's name.
97 */
98 config string deviceName;
99
100 /*!
101 * ======== clockRate ========
102 * The clock rate for this device.
103 */
104 config Double clockRate = 60.0;
105
106 override config string codeMemory = null;
107
108 override config string dataMemory = null;
109
110 override config string stackMemory = null;
111
112 /*!
113 * ======== includeLinkCmdFile ========
114 * The flag that specifies if the platform should include a linker command
115 * file.
116 *
117 * By default, a user is responsible for adding a linker command file to
118 * the project, or to the linker command line. However, if this flag is
119 * set, this platform will include a default linker command file for the
120 * selected device.
121 */
122 config Bool includeLinkCmdFile = false;
123 };