SYS/BIOS 6.41.01.36 GA Release Notes

This release note is divided into the following sections:

Introduction, Documentation, What's New, Upgrading And Compatibility Information, Host Support, Dependencies, Device Support, Validation Information, Known Issues, Benchmarks, Versioning, Technical Support And Product Updates,


Introduction

SYS/BIOS 6.41.01.36 is a GA release of SYS/BIOS 6.40.00.  CCS users must use CCSv6.0.0 or higher.  This release also has support for GCC (for Cortex-M) and IAR (for Cortex-M and MSP430).

Please read the SYS/BIOS User's Guide for help installing and setting up your environment to use SYS/BIOS 6.41.01.36.

back to top

Documentation

The following documentation is provided with this release. These documents are also available via the CCS Eclipse help table of contents.

License and manifest.
Additional online sources of documentation.

Release notes from previous releases are also available in the release notes archive directory.

back to top

What's New

SYS/BIOS 6.41.01.36 GA Release (this release).

Defects Fixed in SYS/BIOS 6.41.01.36 GA (Fixes since SYS/BIOS 6.41.00):
ID                             Headline
SDOCM00114363    Deleting a pre-empted task that was executing Event_pend() can result in application crash.
SDOCM00114079    A8 TimestampProvider 64 bit timestamps jump backwards sometimes
SDOCM00113999    avalabench is generating the export file before the benchmark documents
SDOCM00113957    ti/sysbios/smp/LoggerBuf Timestamp proxy is set to early resulting in TimestampNull (no timestamps in the logs)
SDOCM00113943    Fix MSP430 warnings that occur when building with Codegen tools version 4.4.0B1
SDOCM00113914    ARP32/EVE Hwi_interruptClear() should not clear the IFR register (problem in Timer/IPC intitialization)
SDOCM00113851    CCS on Linux is unable to find linker cmd files in the installed SYS/BIOS or TI-RTOS product
SDOCM00113827    Need 2 new Cache APIs for global L1D operations on c64+/c66
SDOCM00113716    ROM application link should fail or give good error if user has incorrect IAR linker command file
SDOCM00113606    ti.sysbios.family Delegates page needs to be updated to show the relatively new Clock.timerDelegate
SDOCM00113566    Clock module cdoc needs to mention function execution context
SDOCM00113541    Hwi_initStack() routine may generate code that corrupts the stack during boot time (gcc v4.8 Arm issue)
SDOCM00113119    BIOS needs to support creating a secure context
SDOCM00113005    Add ASID tagging support for Cortex-A8 and Cortex-A15 and new API to invalidate TLB
SDOCM00112319    F2837x initFlash() code incorrectly programs the flash wait states
SDOCM00108394    Document that C6x Cache_xxxAll() does not wait for whole memory system to complete before return

back to top

Upgrading and Compatibility Information

SYS/BIOS software downloads

SYS/BIOS 6.35 and 6.37

SYS/BIOS 6.34 and older
back to top

Host Support

back to top

Dependencies

back to top

Device Support

Click here  for the list of supported devices.
 
back to top

Validation Information

Click here for the list of compilers used to build and validate this release (scroll down to Supported Targets section).

back to top

Known Issues

The following issues are known to affect this release:

back to top

Benchmarks

    For a full description of Benchmarks please see the appendices in the SYS/BIOS 6 User's Guide. back to top

Versioning

All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or 6.30.00.10-beta).

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory (e.g. bios_6_30_00_00).

Subsequent releases of patch upgrades will be identified by the patch number, ex. SYS/BIOS 6.30.01.15 with directory bios_6_30_01_15. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top

Technical Support and Product Updates

back to top

Last updated: January 07, 2015 Build Ver: 6.41.01.36 Rev: p36