This release note is divided into the following sections:
Introduction,
Documentation,
What's New,
Upgrading And
Compatibility Information,
Host Support,
Dependencies,
Device Support,
Validation Information,
Known Issues,
Benchmarks,
Versioning,
Technical Support
And Product Updates,
SYS/BIOS 6.35.02.45 is a GA release of SYS/BIOS
6.35.00.
SYS/BIOS is a real-time operating system that provides
pre-emptive deterministic multithreading.
The SYS/BIOS releases introduce a completely new SYS/BIOS kernel
and toolset. The SYS/BIOS releases include numerous major
enhancements, including completely new kernel APIs. They also include
compatibility layers and tooling to facilitate easy porting of
applications
developed on DSP/BIOS 5.x releases.
A number of
tools and libraries that were provided as an
integrated part of DSP/BIOS 5.x releases must now be downloaded
separately to
obtain a functional solution. It is essential for even experienced
DSP/BIOS
users to refer to the Getting Started
Guide and to the Upgrading and Compatibility Information
section for
further details.
Please read the Getting Started Guide for help installing and setting
up your environment to use SYS/BIOS 6.35.02.45.
back to top
The following documentation is provided with this release. These
documents are also available via teh CCS Eclipse help table of
contents.
License and manifest.
Additional online sources of documentation.
Release
notes from previous releases are also available in the
release notes archive
directory.
back to top
SYS/BIOS
6.35.02.45 GA
Release (this release).
- A timing benchmark application has been
included in the examples so that customers can collect and compare
benchmarks on their hardware platforms.
- A
new per-task CallStack ROV view has been added to the Task module ROV
view set. Additionally, the ARM and C6x Exception module ROV views have
been enhanced to provide a CallStack reflecting the thread that caused
the exception. These ROV view enhancements are only available in CCS
5.5 or newer.
- Misc bug fixes. See below.
Defects Fixed in
SYS/BIOS
6.35.02.45 GA (Fixes since SYS/BIOS 6.35.00.20):
ID
Headline
SDOCM00101950 Vector Table is missing from MSP430 Applications built with LibType_Debug
SDOCM00101927 rename/move ti.sysbios.hal.vayu package to ti.sysbios.family.shared.vayu
SDOCM00101875 cachePlatformMemory config param in A15 MMU does not work when set to false
SDOCM00101837
Hwi_plugMeta() .cfg API for c64p incorrectly limits Hwi creation to
have eventId less than 32, instead of less than 128
SDOCM00101813 Implement TimestampProvider.getFreqMeta() for MSP430
SDOCM00101676 Add new metaonly functions to BIOS to return timestamp and CPU frequency in Types.FreqHz
SDOCM00101562 Default value assigned to A15's MAIR AttrIndx 0 & 1 cannot be changed using *.cfg script
SDOCM00101519 A15 MMU cdoc needs to provide more details about 1st Level Descriptor Table setup
SDOCM00101429 Remove M3 and M4F GNU examples in TRex until fully supported
SDOCM00101380 Changing Swi numPriorities with LibType_Instrumented/NonInstrumented is not supported
SDOCM00101372 Filter MSP430 by supported device list for TRex
SDOCM00101355 Make MMR_BASE_ADDR a configurable parameter in hal/vayu/IntXbar module
SDOCM00101332 C66 Cache module ROV should not display reserved MAR bits for C66x CorePac devices
SDOCM00101284 Issues with TREX-generated “separate config” examples
SDOCM00101158 nodoc BIOS.useSK, or clarify its limited applicability within XGCONF displays
SDOCM00101108
Need to allow all J6 (Vayu) cores (A15, DSP and M4) access to all 16
DMTimers using a Availability Mask
SDOCM00101097 c28 Timer module checks incorrecct bit in hwiParams bitmask for 'self'
SDOCM00101029 SMP/BIOS Ducati Timer module needs to use BIOS.cpuFreq to determine the CTM frequency
SDOCM00100932 update example "main()" functions to be "int" and return "0" to avoid compiler warning
SDOCM00100800 ti.bios.support package is not exporting libraries for SYS/BIOS 6.35.00/01. 6.34.0x is OK.
SDOCM00100755
document BIOS.smpEnabled config parameter -- include link to an SMP
wiki page with lots of details
SDOCM00100716 XDCARGS in bios.mak incorrectly labels A15 for gnu.targets.arm.A15F
SDOCM00100704
update Examples.xs to remove most examples from the new project wizard
(use TI Resource Explorer instead)
SDOCM00100701 SMP optimizations (allow interrupt on either core, interrupt-to-task optimizations)
SDOCM00100700
add deprecation message to warn people that ti.bios (legacy API)
support will be removed in the future
SDOCM00100665 cannot set event object handles for Mailbox or Semaphore with xgconf
SDOCM00100661
Review and update GSG and User Guide for any references of the Project
Wizard examples that will be removed
SDOCM00100595
ti/sysbios/family/c28/Hwi.h cannot be used from C++ code -- change
extern to __extern in Hwi__epilogue.h
SDOCM00100579 New C2000 Codegen Tools causes SYSBIOS Failure when compiled with o3
SDOCM00100517 dmTimerSources are missing from M4 pre-built libraries
SDOCM00100496 In SMP mode, allow interrupts to be assigned to a specific core
SDOCM00100468 Add device view for DM Timer and GP Timer
SDOCM00100277 Main heading for BIOS in resource explorer goes to top level wiki instead of sysbios category
SDOCM00100242 Cleanup and publish the new "Quick Start Guide" for SYS/BIOS for MSP430
SDOCM00100000
update ti/bios/include/tsk.h to use a different field name than
'errno'. errno conflicts with <errno.h> with C6x/ELF/7.4.2
SDOCM00099833
update regresstest/src/xdc/runtime/systests/assert golden files
should use line numbers (not %d)
SDOCM00099828 Why is the Mmu_disable() API nodoc'ed for A8/A15 ?
SDOCM00099340 Make all A15 family specific modules (MMU, Cache, Timer and Hwi) configurable using XGCONF
SDOCM00098065 Remove examples from the new-project-wizard in favor of using TRex for all examples
SDOCM00090117 BIOS 6: Add task stack back trace ROV view for each task.
SDOCM00086193
provide benchmarks app with SYS/BIOS product so customers can easily
run a subset of our benchmarks themselves
back to top
SYS/BIOS
releases have many significant changes from
DSP/BIOS 5.x. It is important to understand the information
below in order to
successfully use SYS/BIOS and to migrate applications from DSP/BIOS
5.x.
SYS/BIOS
software downloads
SYS/BIOS 6.34
- Binary
Compatibility. A few fields have been added to several data
structures which means that SYS/BIOS 6.34 is not binary compatible
SYS/BIOS 6.33. The safest thing to do is to rebuild all source
code against the .h files provided with SYS/BIOS 6.34. Note that only
the following externally visible structures have changed:
Task_Params, Task_Struct, HeapMem_Params. If your source
code does not use these structures directly, then you may not need to
recompile. Be careful when using other libraries from other
sources (like the NDK stack or other libraries provided with an
SDK or otherwise). These libraries should also be recompiled
against SYS/BIOS 6.34.
- MSP430
Clock. The Clock module for the MSP430 now uses the periodic
timer mode (TickMode_PERIODIC) by default. SYS/BIOS 6.33
used TickMode_DYNAMIC. You can change this default using
the ‘Clock.tickMode’ configuration parameter in your .cfg file.
TickMode_DYNAMIC minimizes the need for periodic interrupts, but adds
some constraints on the application. See
https://processors.wiki.ti.com/index.php/SYS/BIOS_for_the_MSP430#Clock_Tick_Suppression
for more information about MSP430 clock modes.
- This release requires XDC 3.24.01 or later.
- This
release requires Arm codegen 5.0.1 or later. 5.0.1 will be
provided with CCSv5.3 and is available separately for use in CCSv5.2.
SYS/BIOS 6.33
- The
default directory for SYS/BIOS is changing to match CCSv5.1.0, "C:\ti"
is the new default directory (SDOCM00086138 -- BIOS installer needs to
change its default directory to match CCSv5.1.0)
- RTDX
has been removed and is no longer supported.
Only stop mode is supported for Realtime Analysis (RTA).
SYS/BIOS 6.32
- For
TI816X devices (ie Netra), GPTimers 3 and 7 have been removed from the
list of usable timers due to anomalous behavior when clocked at 32KHz
resulting in two interrupts for every period when run in continuous
mode.
- We
are planning to remove support for the whole_program and
whole_program_debug profiles because of build time problems and
compatibility problems when using different compiler
versions. SYS/BIOS 6.32 will output a warning
message when
the whole_program or whole_program_debug profiles are
used.
We are now providing pre-built libraries which can be selected via the
BIOS.libType configuration parameter (see section 7.6.1 of the BIOS
User's Guide for details). The instrumented
library contains Assert() and Log statements. The
non-instrumented library does not. The custom
library can
be used to build a custom BIOS library which will be built using
#define constants reflecting some of the key configuration parameters
from your application .cfg file. The
non-instrumented
library and custom library should give you similar or better
performance
to SYS/BIOS 6.31 using the whole_program profile.
- .taskStackSection
has been renamed – The .taskStackSection linker section has been
renamed to be a subsection of .far, .bss, or .ebss as appropriate for
the given target. This allows BIOS to be used with
CCS-supplied
linker .cmd files for the MSP430, Stellaris and 28x devices.
This
section is used to place the stacks for tasks created at configuration
time. The new name is provided in the
Task.defaultStackSection field in your configuration. If you
reference ‘.taskStackSection’ in your .cfg file, you should change the
code to use Task.defaultStackSection.
SYS/BIOS 6.31
- Added
an assert to GateMutex. GateMutex_enter() calls
BIOS_getThreadType() to validate the calling context.
GateMutex_enter() will raise an assert if called from Hwi or Swi
context. GateMutex internally calls
Semaphore_pend/post to
provide the mutex. Semaphore_pend() cannot be called from Swi
or
Hwi context if the semaphore is not available. Note that a
GateMutex gate is registered with the TI compiler’s RTS library to make
the RTS library reentrant. Calling printf() and a
few other
RTS functions from Swi or Hwi context will yield this
assert.
- This
assert check will catch bad code
that could cause a rare crash. While not recommended, this
assert
can be disabled by adding ‘GateMutex.common$.diags_ASSERT =
Diags.ALWAYS_OFF;’ to your .cfg file.
- Text
footprint on the C6x
increased by 2K due to Exception.enablePrint default now being set to
‘true’ by default. This enables better diagnostic output when
an
exception occurs. You can set this config parameter to
‘false’ to
save memory and get a shorter, less informative diagnostic string.
- MMU
and Cache are now enabled by default for Arm9.
- Arm9
applications will have larger data/text footprint
due to the 16kbyte MMU table and MMU initialization code.
- Moved
ti.sysbios.arm.Cache module to ti.sysbios.arm.arm9.Cache since this
module is Arm9-specific. .cfg scripts will have to be updated
to
use new name (‘ti.sysbios.family.arm.arm9.Cache’) and .c files will
have to change to use ‘#include
<ti/sysbios/arm/arm9/Cache.h>’.
- Use
BIOS_exit() rather than System_exit() if called from ISR or Swi context
to avoid Assert() in GateMutex module. BIOS_exit()
and
System_exit() both flush the SysMin trace buffer using CIO.
The
CIO library is protected by GateMutex.
DA830
ROM
- BIOS
6.30 and 6.31 cannot be used with the
DA830 ROM. BIOS 6.21 is the preferred version for DA830 ROM.
The
'ti.sdo.io' and 'ti.sdo.utils' packages are no longer provided with
SYS/BIOS
- These
packages are now provided in a
separate
"IPC" product. Users of these packages simply need to add
this
other product directory to their package path (XDCPATH) to build their
applications.
The
ti.sysbios.ipc package and its modules have been deprecated
- The
Semaphore, Event, and Mailbox modules were moved from the
ti.sysbios.ipc package into the ti.sysbios.knl package. Please update
your applications to use the ti.sysbios.knl package versions of the
Semaphore, Event, and Mailbox modules. Using the ipc package versions
of these modules will result in build warnings. In a subsequent release
of BIOS, using any module within the ipc package will result in a build
error.
The
ti.sysbios.family.arm.m3.Exception module has been deprecated
- The
ti.sysbios.family.arm.m3.Exception module functionality has been
enhanced and merged into the ti.sysbios.family.arm.m3.Hwi module.
Please update your applications to use the ti.sysbios.family.arm.m3.Hwi
module to configure exception handling. By default, exceptions will be
reported to CIO with an Error message. Details of the exception can be
seen using Hwi module's "Exception" ROV view. At the expense of
additonal code size, some of this detailed information can ALSO be
routed to the CIO console by setting the Hwi.enableException
configuration flag to true.
Placing of sections using
MEM configs is no longer supported (ie MEM.TEXTSEG is unsupported)
- All
of the legacy MEM memory segment placment functionality has been
removed. Legacy BIOS users must use Program.sectMap to place memory
sections.
The
ti.sysbios.family.c64p.Cache.initSize configuration item is no longer
supported
- The
ti.sysbios.family.c64p.Cache module no longer supports setting the
Cache sizes. These settings are now managed within a platform and can
be configured using the platform wizard.
SYS/BIOS no
longer
contains all the tools and objects you will need
- The
XDC tools now provide the
SYS/BIOS configuration tools and Platform support.
XDC also includes a minimal run-time environment that provides the LOG,
System,
Asserts, Error handling, Timestamp, and Memory Allocation APIs that
will be
used by SYS/BIOS applications. Please refer to the Getting Started Guide on where to
download the XDC tools and
run-time.
Migrating DSP/BIOS
5.x applications to SYS/BIOS
- SYS/BIOS has different APIs
compared to those in
DSP/BIOS 5.x. Configuration scripts are also incompatible between the
two
releases. To provide easy migration of DSP/BIOS 5.x
applications, an API
compatibility layer is provided along with a conversion tool that
converts
configuration scripts to work with XDC and SYS/BIOS. The
API compatibility
layer provides 100% C source code compatibility with the exception of a
few
APIs that are no longer supported. For more complete details
of migrating
DSP/BIOS 5.x applications and configuration scripts, please refer
to Migrating
a DSP/BIOS 5 Application to SYS/BIOS.
- As mentioned
above, some APIs previously supported in
DSP/BIOS 5.x releases will no longer be supported in this release or
the
compatibility layer. Complete details are provided in the
Migration document referenced
above.
back to top
- Supported
Operating Systems
- Windows
7, Windows XP, Windows Vista
- Linux
[RH4], Ubuntu [10.04]
back to top
- Required Software
- Code Composer Studio v5.3.x or later
- Code Generation Tools
- C28X
version 6.1.0 or later
- C6X version 7.3.1 or later
- ARM version 4.9.1 or later, M3/M4 version 5.0.1 or later
- MSP430 version 4.1.0 or later
- XDCtools 3.24.06.63 or later
- Required Hardware
- See Device Support Section below.
back to top
Click here
for the list of supported devices.
back to top
Click
here
for the list of compilers used to build and validate this release
(scroll down to Supported Targets section).
back to top
The
following issues are known to affect this release:
- If
this version of SYS/BIOS is installed on the same system
as SYS/BIOS 6.31.00.xx or older, and use the same
version of
CCS, the user may see two "SYS/BIOS" folders in the examples when
creating a new project. The Eclipse plugins were
updated to
fix this in SYS/BIOS 6.31.01.19 and later. To work around
this
issue remove all versions of SYS/BIOS older than 6.31.01.19.
- Workaround for SDOCM00102016. Add the below line before the useModule for the Timer module.
var Clock = xdc.useModule(‘ti.sysbios.knl.Clock’); - Workaround for SDOCM00102021 see the FAQ here https://processors.wiki.ti.com/index.php/SYS/BIOS_FAQs
ID
Headline
SDOCM00102023 ARM9 benchmarks are broken in avalabench-c series
SDOCM00102021 Update SYS/BIOS FAQ to show how to get IO working for GNU Cortex-A CCS example projects
SDOCM00102016 Clock module's module$use references Timer.TimerProxy before it is initialized
SDOCM00082528 Linker command file
inserted regardless of platform selected for C28 examples
SDOCM00074130 ROV should reference kernel
object names versus object addresses
SDOCM00068360 No data displayed in RTA
Exec Graph when attaching to running target
back to top
For a full description of Benchmarks please see the
appendices in the SYS/BIOS
6 User's
Guide.
back to top
All releases
have 4 digits (M.mm.pp.bb).
This includes GA and pre-releases (engineering, alpha/EA, beta, etc.).
Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or
6.30.00.10-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit
Major number, mm
is 2 digit minor number, pp
is a 2 digit patch number, and b
is an unrestricted set of digits used as an incrementing build counter.
To
support multiple side-by-side installations of the product, the product
version is encoded in the top level directory (e.g. bios_6_30_00_00).
Subsequent
releases of patch upgrades will be identified by the patch number, ex.
SYS/BIOS 6.30.01.15 with directory bios_6_30_01_15. Typically, these
patches only include critical bug fixes.
Please note that
version numbers and compatibility keys are NOT the same. For an
explanation of compatibility keys, please refer to the 'Upgrade and
Compatibility Information' section.
back to top
Technical
Support and Product Updates
back to top
Last
updated: June 14, 2013 Build Ver: 6.35.02.45 Rev: k45