This release note is divided into the following sections:
Introduction,
Documentation,
What's New,
Upgrading And
Compatibility Information,
Host Support,
Dependencies,
Device Support,
Validation Information,
Known Issues,
Benchmarks,
Versioning,
Technical Support
And Product Updates,
SYS/BIOS 6.30.01.33 is a Patch release of SYS/BIOS
6.30.
SYS/ BIOS is a real-time operating system that provides
pre-emptive deterministic multithreading.
The SYS/BIOS 6.x releases introduce a completely new SYS/BIOS kernel
and toolset. The SYS/BIOS 6.x releases include numerous major
enhancements, including completely new kernel APIs. They also include
compatibility layers and tooling to facilitate easy porting of
applications
developed on DSP/BIOS 5.x releases.
A number of
tools and libraries that were provided as an
integrated part of DSP/BIOS 5.x releases must now be downloaded
separately to
obtain a functional solution. It is essential for even experienced
DSP/BIOS
users to refer to the Getting Started
Guide and to the Upgrading and Compatibility Information
section for
further details.
Please read the Getting Started Guide for help installing and setting
up your environment to use SYS/BIOS 6.30.01.33.
back to top
The following documentation is provided with this release:
Release notes from previous releases are also available in the
release notes archive
directory.
back to top
SYS/BIOS 6.30.01.33 Patch
Release (this release).
This
release is based on DSP/BIOS 6.30.00.
Notes on this release:
- The product name has
been changed to SYS/BIOS to reflect the support for a wider set of embedded
processors (i.e., MSP430, Cortex-M3, Arm9).
- Source code in the
product is now licensed using the Open-Source BSD license.
- This release
contains support for MSP430.
- Size and timing
benchmarks are provided (see benchmark link in this document for more
information).
- The DSP/BIOS Getting Started Guide describes
how to build the examples.
- Numerous minor bug
fixes, new device support, and enhancements as listed in the Defects list
below
Defects Fixed:
ID
Headline
SDOCM00071405 Need ROV for EventCombiner
SDOCM00071248 Minor updates needed to "Rebuilding SYS/BIOS" chapter in User Guide
SDOCM00071160 ti.sysbios.benchmarks is missing from
cdoc table of contents (+ minor change to latency benchmark)
SDOCM00071154 Add filters to example templates based on supported targets and platforms.
SDOCM00071108 The @a(HeapMem) in HeapMem.restore() etc. is redundant in new cdoc
SDOCM00071095 xgconf product view is not working for BIOS 6.30 (typo in Product.xdc)
SDOCM00071065 (Child) BCACHE_wait() contains a hole
which can cause an exception if MPC is enabled
SDOCM00070979 Update CDOC for 2nd level MMU descriptor for ARM9 devices
SDOCM00070974 release notes don't show compiler
version correctly (uses M,S,R,P instead of 7.0.1)
SDOCM00070677 .cinit sectMap code generated by conversion tool is incorrect
SDOCM00070513 c66 Cache needs mfence instruction
SDOCM00070410 update BIOS examples to include
"disable Assert()" and other common options (commented out for easy
access and use)
SDOCM00070364 mask math in timer64/Timer.xs doesn't work if ntimers >= 16 (Shannon)
SDOCM00064359 (MSP430) Resolve a common platform/catalog approach, and implement
SDOCM00046568 Examples with unique module / config
requirements should have their own cfg files
back to top
SYS/BIOS 6.x releases have many significant changes from
DSP/BIOS 5.x. It is important to understand the information
below in order to
successfully use SYS/BIOS 6.x and to migrate applications from DSP/BIOS
5.x.
DA830
ROM
BIOS 6.30 cannot be used with the
DA830 ROM. BIOS 6.21 is the preferred version for DA830 ROM.
The
'ti.sdo.io' and 'ti.sdo.utils' packages are no longer provided with
SYS/BIOS
These packages are now provided in a
separate
"IPC" product. Users of these packages simply need to add
this
other product directory to their package path (XDCPATH) to build their
applications.
The ti.sysbios.ipc package and its modules have been deprecated
The
Semaphore, Event, and Mailbox modules were moved from the
ti.sysbios.ipc package into the ti.sysbios.knl package. Please update
your applications to use the ti.sysbios.knl package versions of the
Semaphore, Event, and Mailbox modules. Using the ipc package versions
of these modules will result in build warnings. In a subsequent release
of BIOS, using any module within the ipc package will result in a build
error.
The ti.sysbios.family.arm.m3.Exception module has been deprecated
The
ti.sysbios.family.arm.m3.Exception module functionality has been
enhanced and merged into the ti.sysbios.family.arm.m3.Hwi module.
Please update your applications to use the ti.sysbios.family.arm.m3.Hwi
module to configure exception handling. By default, exceptions will be
reported to CIO with an Error message. Details of the exception can be
seen using Hwi module's "Exception" ROV view. At the expense of
additonal code size, some of this detailed information can ALSO be
routed to the CIO console by setting the Hwi.enableException
configuration flag to true.
Placing of sections using MEM configs is no longer supported (ie MEM.TEXTSEG is unsupported)
All
of the legacy MEM memory segment placment functionality has been
removed. Legacy BIOS users must use Program.sectMap to place memory
sections.
The ti.sysbios.family.c64p.Cache.initSize configuration item is no longer supported
The
ti.sysbios.family.c64p.Cache module no longer supports setting the
Cache sizes. These settings are now managed within a platform and can
be configured using the platform wizard.
SYS/BIOS no
longer
contains all the tools and objects you will need
The XDC tools now provide the
SYS/BIOS configuration tools and Platform support.
XDC also includes a minimal run-time environment that provides the LOG,
System,
Asserts, Error handling, Timestamp, and Memory Allocation APIs that
will be
used by SYS/BIOS applications. Please refer to the Getting Started Guide on where to
download the XDC tools and
run-time.
Migrating DSP/BIOS
5.x applications to SYS/BIOS 6.x
SYS/BIOS 6.x has different APIs
compared to those in
DSP/BIOS 5.x. Configuration scripts are also incompatible between the
two
releases. To provide easy migration of DSP/BIOS 5.x
applications, an API
compatibility layer is provided along with a conversion tool that
converts
configuration scripts to work with XDC and SYS/BIOS 6.x. The
API compatibility
layer provides 100% C source code compatibility with the exception of a
few
APIs that are no longer supported. For more complete details
of migrating
DSP/BIOS 5.x applications and configuration scripts, please refer
to Migrating
a DSP/BIOS 5 Application to SYS/BIOS 6.
As mentioned
above, some APIs previously supported in
DSP/BIOS 5.x releases will no longer be supported in this release or
the
compatibility layer. Complete details are provided in the
Migration document referenced
above.
back to top
- Supported Operating Systems
- Windows 7, Windows XP, Windows Vista
- Linux [RH4], Ubuntu [10.1]
back to top
- Required
Software
- Code Composer Studio
v4.2 Beta or higher
- Code Generation
Tools
- C28X version 5.2.3
- C6X
version 7.0.2
- ARM version
4.6.3
- MSP430 version
3.3.0B2 or higher
- XDCtools
3.20.00.40 or higher
- IPC 1.21.00.14
or higher
- Required
Hardware
- See Device Support
Section below.
back to top
Click here
for the list of supported devices.
back to top
This release was built and validated using the following
components:
- Click here
for validation information.
back to top
The following issues are known to affect this release:
ID
Headline
SDOCM00071397
Review supported device list in release notes - msp430 device list is
missing
SDOCM00071153 Need examples for 28x
SDOCM00069680 BIOS legacy app note updates for 6.30
SDOCM00070088 BIOS dispatcher should set TSR.XEN so
that exceptions that happen during ISR context will be caught
immediately
SDOCM00068360 No data displayed in RTA Exec Graph when attaching to running target
SDOCM00064397 RTA crashes CCS 4.1 after a few reset/reload with USB emulator
SDOCM00046756 BIOS6 doesn't have MPC module
back to top
For a full description of Benchmarks please see the
appendices in the SYS/BIOS
6 User's
Guide.
- Timing and Size
Benchmarks
- The Timing Benchmarks for the MSP430 target have not been
determined.
The published numbers for MSP430 were inadvertantly duplicated from the
M3 timing benchmarks.
back to top
All releases have 4 digits (M.mm.pp.bb).
This includes GA and pre-releases (engineering, alpha/EA, beta, etc.).
Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or
6.30.00.10-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit
Major number, mm
is 2 digit minor number, pp
is a 2 digit patch number, and b
is an unrestricted set of digits used as an incrementing build counter.
To
support multiple side-by-side installations of the product, the product
version is encoded in the top level directory (e.g. bios_6_30_00_00).
Subsequent
releases of patch upgrades will be identified by the patch number, ex.
SYS/BIOS 6.30.01.15 with directory bios_6_30_01_15. Typically, these
patches only include critical bug fixes.
Please note that
version numbers and compatibility keys are NOT the same. For an
explanation of compatibility keys, please refer to the 'Upgrade and
Compatibility Information' section.
back to top
Technical
Support and Product Updates
back to top
Last updated: June 28, 2010 Build Ver: 6.30.01.33 Rev: f33