1    /*
     2     *  ======== Rta.xdc ========
     3     */
     4    
     5    package xdc.runtime;
     6    
     7    /*!
     8     *  ======== Rta ========
     9     *  The Rta module contains target and configuration code for providing RTA
    10     *  support.
    11     *
    12     *  The 'Command' enum defines the available control commands, and the
    13     *  'CommandPacket' structure defines the format of commands received from
    14     *  the host.
    15     *
    16     *  All commands should send back a response, even if only to acknowledge
    17     *  receipt and completion of the command. The format of the response
    18     *  is defined by the 'ResponsePacket' structure.
    19     *
    20     *  The Rta_processCommand can be used to process commands received from a
    21     *  host to call the appropriate API. Alternatively, the individual APIs can
    22     *  be called if not all of the defined commands are used.
    23     */
    24    @DirectCall
    25    module Rta {
    26    
    27        /*! Logged when the Agent receives a command */
    28        config Log.Event LD_cmdRcvd = {
    29            mask: Diags.USER2,
    30            msg: "LD_cmdRcvd: Received command: %d, arg0: 0x%x, arg1: 0x%x"
    31        };
    32    
    33        /*! Logged when a diags mask is changed */
    34        config Log.Event LD_writeMask = {
    35            mask: Diags.USER2,
    36            msg: "LD_writeMask: Mask addres: 0x%x, New mask value: 0x%x"
    37        };
    38    
    39        /*! Assert if logger id in control command is invalid. */
    40        config Assert.Id A_invalidLogger = {
    41            msg: "A_invalidLogger: The logger id %d is invalid."
    42        };
    43    
    44        /*! Error raised if Agent receives an invalid command. */
    45        config Error.Id E_badCommand  = {
    46            msg: "E_badCommand: Received invalid command, id: %d."
    47        };
    48    
    49        /*! Command ids */
    50        enum Command : Int {
    51            Command_READ_MASK = 0,  
    52            Command_WRITE_MASK = 1, 
    53            Command_LOGGER_OFF = 2,
    54            Command_LOGGER_ON = 3,
    55            Command_GET_CPU_SPEED = 4,
    56            Command_RESET_LOGGER = 5,
    57            Command_CHANGE_PERIOD = 6,
    58            Command_START_TX = 7,
    59            Command_STOP_TX = 8
    60        };
    61        
    62        /*! 
    63         * Structure of command received from host 
    64         * TODO - Either the types should be changed to 32-bits, or the packet
    65         * size information should be added to the RTA XML file.
    66         */
    67        struct CommandPacket {
    68            Command  cmdId;
    69            UArg     arg0;
    70            UArg     arg1;
    71        }
    72    
    73        /*! Structure of response packet sent back to host */
    74        struct ResponsePacket {
    75            Command  cmdId;
    76            UArg     resp0;
    77            UArg     resp1;
    78        }
    79        
    80        /*! 
    81         *  ======== dataTransportClassName ========= 
    82         *  The name of the xdc.rta.IDataTransport class to use. 
    83         *  
    84         *  The class specified here can be used on the host for reading RTA data
    85         *  from this target application.
    86         */
    87        config String dataTransportClassName = "";
    88    
    89        /*!
    90         *  ======== controlTransportClassName ========
    91         *  The name of the xdc.rta.IControlTransport class to use.
    92         *
    93         *  The class specified here can be used on the host for communicating with
    94         *  this target application to send control commands and receive responses.
    95         */
    96        config String controlTransportClassName = "";
    97         
    98        /*!
    99         *  ======== processCommand ========
   100         *  Executes a command packet and prepares the response packet.
   101         *  
   102         *  This API will execute the command specified by the command packet
   103         *  argument, and will store the response information in the response
   104         *  packet argument.
   105         *
   106         *  @param(cmd)    The CommandPacket to execute.
   107         *  @param(resp)   The ResponsePacket to populate with the response.
   108         */
   109        Void processCommand(CommandPacket *cmd, ResponsePacket *resp);
   110        
   111        /*!
   112         *  ======== acknowledgeCmd ========
   113         */
   114        Void acknowledgeCmd(ResponsePacket *resp);
   115    
   116        /*!
   117         *  ======== readMask ========
   118         */
   119        Void readMask(ResponsePacket *resp, UArg addr);
   120        
   121        /*!
   122         *  ======== writeMask ========
   123         */   
   124        Void writeMask(ResponsePacket *resp, UArg addr, UArg val);
   125        
   126        /*!
   127         *  ======== enableLog ========
   128         */
   129        Void enableLog(ResponsePacket *resp, UArg log);
   130        
   131        /*!
   132         *  ======== disableLog ========
   133         */
   134        Void disableLog(ResponsePacket *resp, UArg log);
   135        
   136        /*!
   137         *  ======== getCpuSpeed ========
   138         */
   139        Void getCpuSpeed(ResponsePacket *resp);
   140        
   141        /*!
   142         *  ======== resetLog ========
   143         */
   144        Void resetLog(ResponsePacket *resp, UArg log);
   145        
   146        /*!
   147         *  ======== changePeriod ========
   148         */
   149        Void changePeriod(ResponsePacket *resp, UArg period);
   150    
   151        /*!
   152         *  @_nodoc
   153         *  ======== genRta ========
   154         *  Generates the Rta XML file.
   155         */
   156        function genRta(outputFileName);
   157    
   158    }
   159    /*
   160     *  @(#) xdc.runtime; 2, 1, 0,0; 12-9-2015 17:36:48; /db/ztree/library/trees/xdc/xdc-B06/src/packages/
   161     */
   162