1    /* 
     2     *  Copyright (c) 2009-2015 Texas Instruments Incorporated
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     *
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     *
    11     * */
    12    /*
    13     *  ======== ITarget.xdc ========
    14     *
    15     */
    16    
    17    /*!
    18     *  ======== ITarget ========
    19     *  A TI specific extension to the base `xdc.bld.ITarget3` interface.
    20     */
    21    @TargetHeader("xdc/bld/stddefs.xdt")
    22    metaonly interface ITarget inherits xdc.bld.ITarget3 {
    23    
    24        override readonly config string stdInclude = "ti/targets/std.h";
    25    
    26        /*!
    27         *  ======== binDir ========
    28         *  This parameter controls the location of the target's commands.
    29         *
    30         *  All build commands returned within a command set
    31         *  (`xdc.bld.ITarget.CommandSet.cmds`) are formed by prefixing `binDir`
    32         *  to this target's Command.cmd specification.  For example, the
    33         *  compile command returned is formed as follows:
    34         *  @p(code)
    35         *      $(binDir)$(cc.cmd)
    36         *  @p
    37         *  where, `$(binDir)` is this target's `binDir` value and `$(cc.cmd)` is
    38         *  the value of this target's `cc.cmd` string.
    39         *
    40         *  If `binDir` is non-empty then it must end with '/'.  If it is empty,
    41         *  the target's commands (compiler, linker, archiver, etc.) will be
    42         *  located along a path constructed from this target's `pathPrefix`.
    43         */
    44        config string binDir = "$(rootDir)/bin/";
    45    
    46        /*!
    47         *  ======== pathPrefix ========
    48         *  A prefix to the PATH environment variable
    49         *
    50         *  Each target command is executed with C_DIR set to "" and PATH
    51         *  set as follows:
    52         *  @p(code)
    53         *      $(pathPrefix);$(binDir);$(PATH)
    54         *  @p
    55         *  where, `$(pathPrefix)` and `$(binDir)` are the values of the
    56         *  configuration parameters and `$(PATH)` is the value of the `PATH`
    57         *  environment variable set by the `xdc` command (type 'xdc -n' to
    58         *  see this).
    59         *
    60         *  Embedded ';' characters within `pathPrefix` separate directory
    61         *  names.  On UNIX hosts these ';' characters are convered to an
    62         *  appropriate separator; i.e., ':'.
    63         */
    64        config string pathPrefix = "";
    65    
    66        override config String binaryParser = "ti.targets.omf.cof.Coff";
    67    
    68        /*!
    69         *  ======== debugGen ========
    70         *  TI Debugger/IDE file generation support.
    71         *
    72         *  @_nodoc
    73         *  These templates below are long outdated and are no longer used.
    74         *  They remain as an example in the event that we want to generate
    75         *  project suport in the future.
    76         *
    77         *  To avoid unnecessary build time overhead, these files are not always
    78         *  generated; by default, they are only generated for "debug" profiles.
    79         *  The generation of these files is controlled by the
    80         *  `{@link xdc.cfg.Program#gen}` configuration parameter.  To force these
    81         *  files to be generated for a particular executable, add the following
    82         *  line to the executable's program configuration script:
    83         *  @p(code)
    84         *      Program.gen.debuggerFiles = true;
    85         *  @p
    86         *  It is also possible to control the generation via build options; see
    87         *  `{@link xdc.bld.ITarget#DebugGen}`.
    88         *
    89         *  @a(See Also) `xdc.bld.ITarget` contains addition information about
    90         *  how to create and use these templates.
    91         */
    92        //    override config xdc.bld.ITarget.DebugGen debugGen = {
    93        //  execTemplate   : "ti/targets/ccs_exec.xdt",
    94        //  execPattern    : "$(cfgDir)$(cfgName).pjt",
    95        //  packageTemplate: "ti/targets/ccs_package.xdt",
    96        //  packagePattern : "package/$(pkgName).pjt"
    97        //    };
    98        override config xdc.bld.ITarget.DebugGen debugGen = {
    99            execTemplate   : null,
   100            execPattern    : null,
   101            packageTemplate: null,
   102            packagePattern : null
   103        };
   104    
   105        /*!
   106         *  ======== extensions ========
   107         *  File extensions recognized by TI targets
   108         *
   109         *  @a(TI Specifics)
   110         *  For TI targets, the `typ` string field of an
   111         *  `xdc.bld.ITarget.Extension` structure may be of the form
   112         *  `"<cmd>:<langOpt>"` where `<cmd>` is one of `"asm"`, `"c"`, `"cpp"`,
   113         *  and `<langOpt>` is the language option used to identify the source
   114         *  language of a source file.  This allows one to explicitly control the
   115         *  language flag passed to the compiler based on a source file's
   116         *  extension; in particular, one can define separate source extensions
   117         *  for "linear" and "scheduled" assembly files, or simply cause `".s62"`
   118         *  files to be treated as "linear" assembly rather than "scheduled"
   119         *  assembly.
   120         *
   121         *  For example,
   122         *  @p(code)
   123         *  tiTargets.C62.extensions[".s62"] = {suf: ".s62", typ: "asm:-fl"};
   124         *  @p
   125         *  causes all `".s62"` files to be treated as linear assembly.
   126         *
   127         *  If no ':' appears in the `typ` string, a default will be used:
   128         *  `"-fa"` for `"asm"` files `"-fc"` for `"c"` files, and `"-fp"` for
   129         *  `"cpp"` files.
   130         */
   131        override config xdc.bld.ITarget.Extension extensions[string] =
   132            xdc.bld.ITarget.extensions;
   133    
   134        readonly config Bool splitMap[string];
   135    
   136        /*!
   137         *  ======== profiles ========
   138         *  Standard options profiles for the TI tool-chain.
   139         */
   140        override config xdc.bld.ITarget.OptionSet profiles[string] = [
   141            ["debug", {
   142                compileOpts: {
   143                    copts: "-g",
   144                    defs:  "-D_DEBUG_=1",
   145                }
   146            }],
   147            ["release", {
   148                compileOpts: {
   149                    copts: "-O2",
   150                },
   151            }],
   152        ];
   153    
   154        /*!
   155         *  ======== versionMap ========
   156         *  Map of TI compiler version numbers to compatibility keys.
   157         *
   158         *  This map translates version string information from the compiler
   159         *  into a compatibility key.  The compatibility key is used to validate
   160         *  consistency among a collection of packages used in a configuration.
   161         *
   162         *  TI compiler strings are formed by parsing the output of the
   163         *  compiler's --compiler_revision option and creating a string of the
   164         *  form:
   165         *  @p(code)
   166         *      <comp>_<ver>
   167         *  @p
   168         *  where `<comp>` is the first word of the output and `<ver>` is the
   169         *  version number that appears on this same line.
   170         *
   171         *  There are two forms of version numbers output by the TI code gen
   172         *  tools; an "old" style that is of the form "<major>.<minor>" and a
   173         *  new style of the form "<major>.<minor>.<update>[.<branch>][<qual>],
   174         *  where <major>, <minor>, <update>, and <branch> are non-negative
   175         *  integers and <qual> is of  the form "[IBAP]<yyddd>", and <yyddd>
   176         *  is the last two digits of the year concatenated with the number of
   177         *  the day.
   178         *
   179         *  If a compiler version is not found in this map the default is
   180         *  "1,0,<major>.<minor>" for old style version numbers, and
   181         *  "1,0,<major>.<minor>,<update>[.<branch>][,<yyddd>]" for new style
   182         *  version numbers.
   183         *
   184         *  The user only needs to extend this table when a significant
   185         *  incompatibility occurs (and this package doesn't know about it) or
   186         *  when two versions of the compiler should be treated as 100%
   187         *  compatible.
   188         *
   189         *  @a(Examples)
   190         *  @p(code)
   191         *      var C62 = xdc.useModule('ti.targets.C62');
   192         *
   193         *      // assert that 4.0 is forward compatible with 4.32
   194         *      C62.versionMap["TMS320C6x_4.32"] =  "1,0,4.0,0";
   195         *
   196         *      // assert that 4.28 is incompatible with all other compilers
   197         *      C62.versionMap["TMS320C6x_4.28"] =  "1,1,4.28,0";
   198         */
   199        override config string versionMap[string] = [
   200            ["TMS320C6x_4.32", "1,0,4.32,0"],
   201            ["TMS320C2000_3.07", "1,0,3.07,0"],
   202        ];
   203    
   204        /*!
   205         *  ======== alignDirectiveSupported ========
   206         *  The compiler supports an align directive.
   207         */
   208        override readonly config Bool alignDirectiveSupported = true;
   209    
   210        /*!
   211         *  ======== ccConfigOpts ========
   212         *  User configurable compiler options for the generated config C file.
   213         */
   214        override config xdc.bld.ITarget2.Options ccConfigOpts = {
   215            prefix: "$(ccOpts.prefix) -mo",
   216            suffix: "$(ccOpts.suffix)"
   217        };
   218    
   219        /*!
   220         *  ======== lnkOpts ========
   221         *  Linker options
   222         *
   223         *  Options:
   224         *  @p(dlist)
   225         *      -`-q`
   226         *          Quite run
   227         *      -`-u`
   228         *          Place unresolved external symbol into symbol table
   229         *      -`-c`
   230         *          ROM autoinitialization model
   231         *      -`-m`
   232         *          create a map file
   233         *      -`-l`
   234         *          archive library file as linker input
   235         */
   236        override config xdc.bld.ITarget2.Options lnkOpts = {
   237            prefix: "-q -u _c_int00",
   238            suffix: "-w -c -m $(XDCCFGDIR)/$@.map -l $(rootDir)/lib/libc.a"
   239        };
   240    
   241        /*!
   242         *  ======== asmName ========
   243         *  The function that converts a C name into an assembly name
   244         */
   245        String asmName(String CName);
   246    
   247        /*!
   248         *  ======== vers ========
   249         *  The command used to get the tool-chain to return a version number.
   250         */
   251        readonly config xdc.bld.ITarget2.Command vers;
   252    
   253        /*!
   254         *  ======== version ========
   255         *  The Compatibility Key associated with this target.
   256         *
   257         *  The first two components of this target Compatibility Key are '1,0'.
   258         *  The rest of the Key represents the compiler version. The third
   259         *  component combines the major and the minor version number in the format
   260         *  Major.Minor. The fourth component is the patch number, and the optional
   261         *  fifth component is the version of an Alpha or Beta release.
   262         *
   263         *  @a(Example)
   264         *  If this target's `rootDir` points to the compiler version 6.0.11, the
   265         *  Compatibility Key is [1,0,6.0,11]. If this target's `rootDir` points to
   266         *  the compiler version 7.0.0B1, the Compatibility Key is [1,0,7.0,0,1].
   267         *
   268         */
   269        override metaonly config String version;
   270    
   271        /*
   272         *  ======== rawVersion ========
   273         *  The raw version string from the compiler
   274         *
   275         */
   276        override metaonly config String rawVersion;
   277    
   278    }
   279    /*
   280     *  @(#) ti.targets; 1, 0, 3,0; 10-21-2016 18:16:53; /db/ztree/library/trees/xdctargets/xdctargets-l07/src/ xlibrary
   281    
   282     */
   283