module ti.sysbios.family.arm.v7r.tms570.Boot |
|
|
TMS570DCxx/RM57Dxx Boot Support
//TODO Document this module
[
more ... ]
#include <ti/sysbios/family/arm/v7r/tms570/Boot.h>
Functions common to all target modules |
|
|
Constants |
extern const Bool | |
DETAILS
//TODO Document this module
This Boot module supports boot initialization for the Cortex-R5F cores.
A special boot init function is created based on the configuration
settings for this module. This function is hooked into the
xdc.runtime.Reset.fxns[] array and called very early at boot time (prior
to cinit processing).
The code to support the boot module is placed in a separate section
named
".text:.bootCodeSection" to allow placement of this section in
the linker .cmd file if necessary. This section is a subsection of the
".text" section so this code will be placed into the .text section unless
explicitly placed, either through
Program.sectMap or through a linker
command file.
CLOCK CONFIGURATION
Using this Boot module will automatically enable clock configuration. As
part of the clock configuration, this module will setup the PLL based
on the multiplier and divider values configured. Once the PLL is setup,
the CPU clock source (GCLK) is changed from OSCIN to PLL1. In addition,
this module also sets up the VCLK to equal GCLK/2 and selects the VCLK
as the source for the RTI timer.
The formula for PLL output frequency is shown below. The multiplier
and the various dividers can be configured to achieve different CPU
frequencies. By default, this module will configure the PLL to run the
CPU at 100MHz and the RTI Timer is clocked at 50MHz.
Formula for PLL output frequency:
Foscin NF
Fpll = -------- X --------
NR OD x R
where, Foscin is frequency of PLL input clock from oscillator
NR is prescale divider for the input clock
NF is multiplier
OD,R is postscale divider
NF = PLLMUL + 1
NR = REFCLKDIV + 1 (max 62)
R = PLLDIV + 1
OD = ODPLL + 1
FLASH CONFIGURATION
If flash configuration is enabled, this module will compute the number
of flash wait states required at the current CPU frequency and will
program the respective flash registers. This module also allows the
user to enable/disable flash prefetching on flash ports A and B.
config Boot_configureClocks // module-wide |
|
Clock configuration flag, default is true
extern const Bool Boot_configureClocks;
DETAILS
Set to false to disable clock configuration.
Clock configuration will setup the CPU (and RTI) clock source,
configure the PLL and system clock dividers.
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool Boot_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Boot_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Boot_Module_getMask();
// Returns the diagnostics mask for this module
Void Boot_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var Boot = xdc.useModule('ti.sysbios.family.arm.v7r.tms570.Boot');
module-wide constants & types
module-wide config parameters
metaonly struct Boot.ModuleView |
|
var obj = new Boot.ModuleView;
obj.configureClocks = Bool ...
obj.frequencyModulationEnable = Bool ...
obj.OSCIN = UInt ...
obj.PLLMUL = UInt ...
obj.PLLDIV = UInt ...
obj.REFCLKDIV = UInt ...
obj.ODPLL = UInt ...
obj.SPREADINGRATE = UInt ...
obj.MULMOD = UInt ...
obj.SPR_AMOUNT = UInt ...
config Boot.configureClocks // module-wide |
|
Clock configuration flag, default is true
Boot.configureClocks = Bool true;
DETAILS
Set to false to disable clock configuration.
Clock configuration will setup the CPU (and RTI) clock source,
configure the PLL and system clock dividers.
C SYNOPSIS
metaonly config Boot.MULMOD // module-wide |
|
Multiplier correction when modulation enabled (valid range
from 0 to 511)
metaonly config Boot.ODPLL // module-wide |
|
Internal PLL Output divider (valid range from 0 to 7)
DETAILS
PLL postscale divider, OD = ODPLL + 1
metaonly config Boot.OSCIN // module-wide |
|
Input frequency to PLL, in MHz. Default is 16 MHz
DETAILS
This is the frequency of the oscillator clock (OSCIN) input to the
PLL.
metaonly config Boot.PLLDIV // module-wide |
|
PLL Output clock divider (valid range from 0 to 31)
DETAILS
PLL postscale divider, R = PLLDIV + 1
metaonly config Boot.PLLMUL // module-wide |
|
PLL Multiplication factor value (valid range from 0 to 255)
DETAILS
PLL Multiplier, NF = PLLMUL + 1
metaonly config Boot.REFCLKDIV // module-wide |
|
PLL Reference clock divider value (valid range from 0 to 62)
Boot.REFCLKDIV = UInt 0x5;
DETAILS
PLL Prescale divider, NR = REFCLKDIV + 1 (max 62)
metaonly config Boot.SPREADINGRATE // module-wide |
|
Spreading rate (valid range from 0 to 511)
Boot.SPREADINGRATE = UInt 0x1FF;
metaonly config Boot.SPR_AMOUNT // module-wide |
|
Spreading amount (valid range from 0 to 511)
Boot.SPR_AMOUNT = UInt 0;
metaonly config Boot.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Boot.configureFlashController // module-wide |
|
Flash controller configuration flag, default is true
Boot.configureFlashController = Bool true;
DETAILS
Set to true to enable the configuration of the Flash controller
wait states and prefetch mode.
metaonly config Boot.configureFlashWaitStates // module-wide |
|
Flash controller wait states configuration flag, default is true
Boot.configureFlashWaitStates = Bool true;
DETAILS
Set to true to configure the Flash controller wait states. The number
of wait states is computed based upon the CPU frequency.
metaonly config Boot.flashPortAPrefetchEnable // module-wide |
|
Flash controller port A prefetch enable flag, default is true
Boot.flashPortAPrefetchEnable = Bool true;
metaonly config Boot.flashPortBPrefetchEnable // module-wide |
|
Flash controller port B prefetch enable flag, default is true
Boot.flashPortBPrefetchEnable = Bool true;
metaonly config Boot.frequencyModulationEnable // module-wide |
|
Enable frequency modulation. Default is false
Boot.frequencyModulationEnable = Bool false;
metaonly config Boot.rovViewInfo // module-wide |
|
generated on Tue, 09 Oct 2018 20:57:52 GMT