Target Platform: ti.platforms.evmTI814X
Tool Chain Version: 7.4.17
BIOS Version: bios_6_46_02_46_eng
XDCTools Version: xdctools_3_32_01_22
Benchmark | Cycles |
---|---|
Interrupt Latency | 227 |
Hwi_restore() | 1 |
Hwi_disable() | 2 |
Hwi dispatcher prolog | 113 |
Hwi dispatcher epilog | 138 |
Hwi dispatcher | 246 |
Hardware Interrupt to Blocked Task | 405 |
Hardware Interrupt to Software Interrupt | 252 |
Swi_enable() | 71 |
Swi_disable() | 12 |
Post Software Interrupt Again | 41 |
Post Software Interrupt without Context Switch | 70 |
Post Software Interrupt with Context Switch | 147 |
Create a New Task without Context Switch | 1450 |
Set a Task Priority without a Context Switch | 139 |
Task_yield() | 196 |
Post Semaphore No Waiting Task | 47 |
Post Semaphore No Task Switch | 160 |
Post Semaphore with Task Switch | 220 |
Pend on Semaphore No Context Switch | 61 |
Pend on Semaphore with Task Switch | 239 |
Clock_getTicks() | 12 |
POSIX Create a New Task without Context Switch | 2679 |
POSIX Set a Task Priority without a Context Switch | 119 |
POSIX Post Semaphore No Waiting Task | 63 |
POSIX Post Semaphore No Task Switch | 177 |
POSIX Post Semaphore with Task Switch | 237 |
POSIX Pend on Semaphore No Context Switch | 77 |
POSIX Pend on Semaphore with Task Switch | 255 |
The benchmark application was built using BIOS.LibType_Custom with the following BIOS.customCCOpts settings: “-mv6740 -mi10 -mo -pdr -pden -pds=238 -pds=880 -pds1110 –program_level_compile -o3”.
As the timer used to run these benchmarks is run at 1/25 the CPU frequency, a deviation of +-25 cycles is to be expected.
See the SYS/BIOS User’s Guide for more information regarding how interrupt latency is calculated.