1 /*
2 * Copyright (c) 2015, Texas Instruments Incorporated
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 *
9 * * Redistributions of source code must retain the above copyright
10 * notice, this list of conditions and the following disclaimer.
11 *
12 * * Redistributions in binary form must reproduce the above copyright
13 * notice, this list of conditions and the following disclaimer in the
14 * documentation and/or other materials provided with the distribution.
15 *
16 * * Neither the name of Texas Instruments Incorporated nor the names of
17 * its contributors may be used to endorse or promote products derived
18 * from this software without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31 */
32 /*
33 * ======== Hwi.xdc ========
34 *
35 */
36
37 package ti.sysbios.family.c64p;
38
39 import xdc.rov.ViewInfo;
40
41 import xdc.runtime.Diags;
42 import xdc.runtime.Error;
43 import xdc.runtime.Log;
44
45 /*!
46 * ======== Hwi ========
47 * C64+ Hardware Interrupt Support Module.
48 *
49 * This Hwi module provides C64+ family-specific implementations of the
50 * APIs defined in {@link ti.sysbios.interfaces.IHwi IHwi}.
51 *
52 * Additional C64+ device-specific APIs are also provided.
53 *
54 * An example of creating a Hwi instance:
55 *
56 * @p(code) 57 *
58 * Int intNum;
59 * Hwi_Params params;
60 * Error_Block eb;
61 *
62 * // Initialize the error block
63 * Error_init(&eb);
64 *
65 * // Initialize the Hwi parameters
66 * Hwi_Params_init(¶ms);
67 *
68 * // Set the GEM event id in the params
69 * params.eventId = 78
70 *
71 * // Specify the interrupt vector number
72 * intNum = 8;
73 *
74 * // create the Hwi for the specified interrupt number and params
75 * Hwi_create(intNum, myIsr, ¶ms, &eb);
76 *
77 * @p 78 *
79 * @a(NOTE) 80 * In this Hwi module implementation, the instance config parameter value
81 * {@link #MaskingOption_LOWER} is equivalent to {@link #MaskingOption_SELF}.
82 * Statically configuring a Hwi object's {@link #Params.maskSetting} to
83 * {@link #MaskingOption_LOWER} will result in the generation of a benign
84 * build warning. Dynamic usages of {@link #MaskingOption_LOWER} will be
85 * silently converted to {@link #MaskingOption_SELF}.
86 *
87 * @p(html) 88 * <h3> Calling Context </h3>
89 * <table border="1" cellpadding="3">
90 * <colgroup span="1"></colgroup> <colgroup span="5" align="center"></colgroup>
91 *
92 * <tr><th> Function </th><th> Hwi </th><th> Swi </th><th> Task </th><th> Main </th><th> Startup </th></tr>
93 * <!-- -->
94 * <tr><td> {@link #clearInterrupt} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
95 * <tr><td> {@link #create} </td><td> N </td><td> N </td><td> Y </td><td> Y </td><td> N </td></tr>
96 * <tr><td> {@link #disable} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
97 * <tr><td> {@link #disableIER} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
98 * <tr><td> {@link #disableInterrupt} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
99 * <tr><td> {@link #enable} </td><td> Y </td><td> Y </td><td> Y </td><td> N </td><td> N </td></tr>
100 * <tr><td> {@link #enableIER} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
101 * <tr><td> {@link #enableInterrupt} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
102 * <tr><td> {@link #eventMap} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
103 * <tr><td> {@link #getEventId} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
104 * <tr><td> {@link #getHandle} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
105 * <tr><td> {@link #Params_init} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
106 * <tr><td> {@link #restore} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
107 * <tr><td> {@link #restoreIER} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
108 * <tr><td> {@link #restoreInterrupt} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
109 * <tr><td> {@link #construct} </td><td> N </td><td> N </td><td> Y </td><td> Y </td><td> N </td></tr>
110 * <tr><td> {@link #delete} </td><td> N </td><td> N </td><td> Y </td><td> Y </td><td> N </td></tr>
111 * <tr><td> {@link #destruct} </td><td> N </td><td> N </td><td> Y </td><td> Y </td><td> N </td></tr>
112 * <tr><td> {@link #getHookContext} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
113 * <tr><td> {@link #reconfig} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
114 * <tr><td> {@link #setFunc} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
115 * <tr><td> {@link #setHookContext} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
116 * <tr><td colspan="6"> Definitions: <br />
117 * <ul>
118 * <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
119 * <li> <b>Swi</b>: API is callable from a Swi thread. </li>
120 * <li> <b>Task</b>: API is callable from a Task thread. </li>
121 * <li> <b>Main</b>: API is callable during any of these phases: </li>
122 * <ul>
123 * <li> In your module startup after this module is started (e.g. Hwi_Module_startupDone() returns TRUE). </li>
124 * <li> During xdc.runtime.Startup.lastFxns. </li>
125 * <li> During main().</li>
126 * <li> During BIOS.startupFxns.</li>
127 * </ul>
128 * <li> <b>Startup</b>: API is callable during any of these phases:</li>
129 * <ul>
130 * <li> During xdc.runtime.Startup.firstFxns.</li>
131 * <li> In your module startup before this module is started (e.g. Hwi_Module_startupDone() returns FALSE).</li>
132 * </ul>
133 * </ul>
134 * </td></tr>
135 *
136 * </table>
137 * @p 138 */
139
140 @Template("./Hwi.xdt") /* generates the vector table and the dispatcher */
141 @ModuleStartup /* generate a call to Hwi_init at startup */
142 @InstanceInitStatic /* allow constructs in static only systems */
143
144 module Hwi inherits ti.sysbios.interfaces.IHwi
145 {
146 // -------- Module Constants --------
147
148 /*! C64+ supports 16 interrupts. */
149 const Int NUM_INTERRUPTS = 16;
150
151 // -------- Module Types --------
152
153 /*! @_nodoc Hwi plug function type definition. */
154 typedef Void (*PlugFuncPtr)(void);
155
156 /*!
157 * ======== BasicView ========
158 * @_nodoc 159 */
160 metaonlystruct BasicView {
161 Ptr halHwiHandle;
162 String label;
163 UInt intNum;
164 String fxn;
165 UArg arg; // Argument to Hwi function.
166 Ptr irp;
167 UInt eventId;
168 String disableMask; // Interrupts to mask during ISR.
169 String restoreMask; // Interrupts to restore after ISR.
170 };
171
172 /*!
173 * ======== ModuleView ========
174 * @_nodoc 175 */
176 metaonlystruct ModuleView {
177 String options[4];
178 String hwiStackPeak;
179 SizeT hwiStackSize;
180 Ptr hwiStackBase;
181 };
182
183 /*!
184 * ======== rovViewInfo ========
185 * @_nodoc 186 */
187 @Facet
188 metaonlyconfig ViewInfo.Instance rovViewInfo =
189 ViewInfo.create({
190 viewMap: [
191 ['Basic', {type: ViewInfo.INSTANCE, viewInitFxn: 'viewInitBasic', structName: 'BasicView'}],
192 ['Module', {type: ViewInfo.MODULE, viewInitFxn: 'viewInitModule', structName: 'ModuleView'}]
193 ]
194 });
195
196 // -------- Module Parameters --------
197
198 /*!
199 * non-dispatched interrupt object.
200 * provided so that XGCONF users can easily plug non-dispatched interrupts
201 */
202 metaonlystruct NonDispatchedInterrupt {
203 Int intNum;
204 PlugFuncPtr fxn; /*! "Hwi_plug'd" ISR function. */
205 Bool enableInt;
206 Int eventId;
207 };
208
209 /*!
210 * non-dispatched interrupt array.
211 * provided so that XGCONF users can easily plug non-dispatched interrupts
212 */
213 metaonlyconfig NonDispatchedInterrupt nonDispatchedInterrupts[string];
214
215 /*!
216 * Alternate reset vector address. Default is undefined.
217 *
218 * if initialized by the user then an additional reset vector
219 * is created and placed in the ".resetVector" section.
220 * To place the .resetVector section into a specific memory section,
221 * add the following command to your config script:
222 * @p(code) 223 * Program.sectMap[".resetVector"] = YourMemorySection;
224 * @p 225 */
226 metaonlyconfig Ptr resetVectorAddress;
227
228 /*!
229 * Error raised when Hwi is already defined
230 */
231 config Error.Id E_alreadyDefined = {
232 msg: "E_alreadyDefined: Hwi already defined: intr# %d"
233 };
234
235 /*!
236 * Error raised when Hwi handle referenced in Hwi_delete()
237 * is not found in the Hwi dispatch table
238 */
239 config Error.Id E_handleNotFound = {
240 msg: "E_handleNotFound: Hwi handle not found: 0x%x"
241 };
242
243 /*!
244 * Error raised when a secure context failed to be allocated
245 */
246 config Error.Id E_allocSCFailed = {
247 msg: "E_allocSCFailed: Alloc secure context failed"
248 };
249
250 /*!
251 * Error raised when a secure context failed to be registered
252 */
253 config Error.Id E_registerSCFailed = {
254 msg: "E_registerSCFailed: Register secure context failed"
255 };
256
257 /*!
258 * Error raised when an invalid interrupt number is passed in
259 */
260 config Error.Id E_invalidIntNum = {
261 msg: "E_invalidIntNum: Invalid interrupt number: intr# %d"
262 };
263
264 /*!
265 * Issued just prior to Hwi function invocation (with interrupts disabled)
266 */
267 config Log.Event LM_begin = {
268 mask: Diags.USER1 | Diags.USER2,
269 msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
270 };
271
272 /*!
273 * Issued just after return from Hwi function (with interrupts disabled)
274 */
275 config Log.Event LD_end = {
276 mask: Diags.USER2,
277 msg: "LD_end: hwi: 0x%x"
278 };
279
280 /*!
281 * enable Exception module for exception processing.
282 */
283 config Bool enableException = true;
284
285 // -------- Module Functions --------
286
287 /*!
288 * ======== disable ========
289 * Globally disable interrupts.
290 *
291 * Hwi_disable globally disables hardware interrupts and returns an
292 * opaque key indicating whether interrupts were globally enabled or
293 * disabled on entry to Hwi_disable().
294 * The actual value of the key is target/device specific and is meant
295 * to be passed to Hwi_restore().
296 *
297 * Call Hwi_disable before a portion of a function that needs
298 * to run without interruption. When critical processing is complete, call
299 * Hwi_restore or Hwi_enable to reenable hardware interrupts.
300 *
301 * Servicing of interrupts that occur while interrupts are disabled is
302 * postponed until interrupts are reenabled. However, if the same type
303 * of interrupt occurs several times while interrupts are disabled,
304 * the interrupt's function is executed only once when interrupts are
305 * reenabled.
306 *
307 * A context switch can occur when calling Hwi_enable or Hwi_restore if
308 * an enabled interrupt occurred while interrupts are disabled.
309 *
310 * Hwi_disable may be called from main(). However, since Hwi interrupts
311 * are already disabled in main(), such a call has no effect.
312 *
313 * @a(constraints) 314 * If a Task switching API such as
315 * {@link ti.sysbios.knl.Semaphore#pend Semaphore_pend()},
316 * {@link ti.sysbios.knl.Semaphore#post Semaphore_post()},
317 * {@link ti.sysbios.knl.Task#sleep Task_sleep()}, or
318 * {@link ti.sysbios.knl.Task#yield Task_yield()}
319 * is invoked which results in a context switch while
320 * interrupts are disabled, an embedded call to
321 * {@link #enable Hwi_enable} occurs
322 * on the way to the new thread context which unconditionally re-enables
323 * interrupts. Interrupts will remain enabled until a subsequent
324 * {@link #disable Hwi_disable}
325 * invocation.
326 *
327 * Swis always run with interrupts enabled.
328 * See {@link ti.sysbios.knl.Swi#post Swi_post()} for a discussion Swis and
329 * interrupts.
330 *
331 * @b(returns) opaque key for use by Hwi_restore()
332 */
333 @Macro
334 override UInt disable();
335
336 /*!
337 * ======== enable ========
338 */
339 @Macro
340 override UInt enable();
341
342 /*!
343 * ======== restore ========
344 */
345 @Macro
346 override Void restore(UInt key);
347
348 /*!
349 * ======== inUseMeta ========
350 * @_nodoc 351 * Check for Hwi already in use.
352 * For internal SYS/BIOS use only.
353 * Should be called prior to any internal Hwi.create().
354 *
355 * @param(intNum) interrupt number
356 */
357 metaonly Bool inUseMeta(UInt intNum);
358
359 /*!
360 * ======== eventMap ========
361 * Maps a GEM event to interrupt number
362 *
363 * Function maps a GEM event to an interrupt number so that the
364 * event is the interrupt source of the vector.
365 *
366 * @p(code) 367 * // Maps GEM event #65 as the interrupt source of int vector #7
368 * Hwi_eventMap(7, 65);
369 * @p 370 *
371 * @param(intNum) interrupt number
372 * @param(eventId) event ID
373 */
374 Void eventMap(Int intNum, Int eventId);
375
376 /*!
377 * ======== eventMapMeta ========
378 * Maps GEM Event to interrupt number statically
379 *
380 * Function maps a GEM event to an interrupt number so that the
381 * event is the interrupt source of the vector.
382 *
383 * @p(code) 384 * // Maps GEM event #65 as the interrupt source of int vector #7
385 * Hwi.eventMapMeta(7, 65);
386 * @p 387 *
388 * @param(intNum) interrupt number
389 * @param(eventId) event Id
390 */
391 metaonly Void eventMapMeta(Int intNum, Int eventId);
392
393 /*!
394 * ======== plug ========
395 * Plug an interrupt vector with an ISR address.
396 *
397 * Hwi_plug writes an Interrupt Service Fetch Packet (ISFP) into the
398 * Interrupt Service Table (IST), at the address corresponding to intNum
399 * The op-codes written in the ISFP create a branch to the function
400 * entry point specified by fxn:
401 *
402 * @p(code) 403 * stw b0, *SP--[1]
404 * mvk fxn, b0
405 * mvkh fxn, b0
406 * b b0
407 * ldw *++SP[1],b0
408 * nop 4
409 * @p 410 *
411 * Hwi_plug hooks up the specified function as the branch target of a
412 * hardware interrupt (fielded by the CPU) at the vector address
413 * specified in intNum. Hwi_plug does not enable the interrupt.
414 * Use Hwi_enableIER to enable specific interrupts.
415 *
416 * AN ISR PLUGGED WITH THIS API IS NOT SERVICED BY THE INTERRUPT
417 * DISPATCHER. CONSEQUENTLY, IT SHOULD NOT INVOKE ANY SYS/BIOS APIs
418 * (ie Semaphore_post())!!!
419 *
420 * @a(constraints) 421 * o interrupt function MUST NOT INTERACT WITH SYS/BIOS.
422 * (ie do not call Semaphore_post())
423 *
424 * o vecid must be a valid interrupt ID in the range of 0-15.
425 *
426 * @param(intNum) interrupt number
427 * @param(fxn) pointer to ISR function
428 */
429 Void plug(UInt intNum, PlugFuncPtr fxn);
430
431 /*!
432 * ======== plugMeta ========
433 * Statically plug an interrupt vector with an ISR address.
434 *
435 * @param(intNum) interrupt number
436 * @param(fxn) pointer to ISR function
437 */
438 metaonly Void plugMeta(UInt intNum, PlugFuncPtr fxn);
439
440 /*!
441 * ======== getEventId ========
442 * Returns event id associated with interrupt number
443 *
444 * If a bad interrupt number is passed in, it will return -1.
445 *
446 * @param(intNum) interrupt number
447 * @b(returns) event id associated with intNum
448 */
449 Int getEventId(UInt intNum);
450
451 /*!
452 * ======== getHandle ========
453 * Returns Hwi_handle associated with interrupt number
454 *
455 * @param(intNum) interrupt number
456 * @b(returns) handle associated with intNum
457 */
458 Handle getHandle(UInt intNum);
459
460 /*!
461 * ======== disableIER ========
462 * Disable certain maskable interrupts.
463 *
464 * Atomically disables specific interrupts by clearing the bits
465 * specified by mask in the Interrupt Enable Register (IER).
466 *
467 * The IER bits to be cleared should be set to 1 in the mask.
468 *
469 * @param(mask) bitmask of interrupts to disable
470 * @b(returns) previous IER settings bitmask
471 */
472 Bits16 disableIER(Bits16 mask);
473
474 /*!
475 * ======== enableIER ========
476 * Enable certain maskable interrupts.
477 *
478 * Atomically enables specific interrupts by setting the bits
479 * specified by mask in the Interrupt Enable Register (IER).
480 *
481 * The IER bits to be set should be set to 1 in the mask.
482 *
483 * @param(mask) bitmask of interrupts to enable
484 * @b(returns) previous IER settings bitmask
485 */
486 Bits16 enableIER(Bits16 mask);
487
488 /*!
489 * ======== restoreIER ========
490 * Restore maskable interrupts to the state they were in
491 * when either disableIER() or enableIER() was called.
492 *
493 * Atomically writes the given mask to the IER register. Typically used
494 * to restore the IER register to the state returned from a call to
495 * either {@link #disableIER()} or {@link #enableIER()}.
496 *
497 * @param(mask) bitmask of interrupts to restore
498 * @b(returns) previous IER settings bitmask
499 */
500 Bits16 restoreIER(Bits16 mask);
501
502 instance:
503
504 /*!
505 * Dispatcher auto-nesting interrupt disable mask.
506 *
507 * When the dispatcher's auto interrupt nesting support feature
508 * is enabled (see {@link #dispatcherAutoNestingSupport}),
509 * this mask defines which IER bits are disabled prior to invoking
510 * the user's ISR function with GIE = 1.
511 *
512 * disableMask bits set to 1 correspond to IER bits that will be cleared
513 * prior to invoking the ISR.
514 *
515 * The value of this mask is normally auto-calculated based on the
516 * value of the maskSetting. However, manual setting of this
517 * mask is enabled by setting the maskSetting to
518 * {@link #MaskingOption MaskingOption_BITMASK}.
519 *
520 * The default value is derived from the
521 * {@link #MaskingOption MaskingOption_SELF}
522 * maskSetting.
523 */
524 config Bits16 disableMask = 0;
525
526 /*!
527 * Dispatcher auto-nesting interrupt restore mask.
528 *
529 * When the dispatcher's auto interrupt nesting support feature
530 * is enabled (see {@link #dispatcherAutoNestingSupport}),
531 * this mask defines which IER bits are restored to their previous
532 * setting upon return from the user's ISR function.
533 *
534 * restoreMask bits set to 1 correspond to IER bits that will be restored.
535 *
536 * The value of this mask is normally auto-calculated based on the
537 * value of the maskSetting. However, manual setting of this
538 * mask is enabled by setting the maskSetting to
539 * {@link #MaskingOption MaskingOption_BITMASK}.
540 *
541 * The default value is derived from the
542 * {@link #MaskingOption MaskingOption_SELF}
543 * maskSetting.
544 */
545 config Bits16 restoreMask = 0;
546
547 /*!
548 * Interrupt priority. Not supported on this target.
549 */
550 overrideconfig Int priority = 0;
551
552 /*!
553 * ======== reconfig ========
554 * Reconfigures a dispatched interrupt.
555 *
556 * This function reconfigures the dispatched interrupt so the
557 * specified function is called with the specified parameters.
558 *
559 * @param(fxn) pointer to ISR function
560 * @param(params) pointer to Hwi parameter structure
561 */
562 Void reconfig(FuncPtr fxn, const Params *params);
563
564 internal: /* not for client use */
565
566 /*
567 * Swi and Task module function pointers.
568 * Used to decouple Hwi from Swi and Task when
569 * dispatcherSwiSupport or
570 * dispatcherTaskSupport is false.
571 */
572 config UInt (*swiDisable)();
573 config Void (*swiRestoreHwi)(UInt);
574 config UInt (*taskDisable)();
575 config Void (*taskRestoreHwi)(UInt);
576
577 /*
578 * ======== getIsrStackAddress ========
579 * Returns initial isrStack address.
580 * This API was developed solely for the Exception module
581 * to allow removal of the Hwi_link.xdt template definition
582 * of ti_sysbios_family_c64p_Hwi_isrStack which was not
583 * ROM-able
584 */
585 Char *getIsrStackAddress();
586
587 /* Interrupt Dispatcher */
588 Void dispatchC(Int intNum);
589
590 /* Interrupt dispatcher core */
591 Void dispatchCore(Int intNum);
592
593 /* unPlugged interrupt handler */
594 Void unPluggedInterrupt();
595
596 /* assembly language code that switches SP and calls dispatchCore */
597 Void switchAndDispatch(Int intNum);
598
599 /* setup a secure context */
600 Void setupSC();
601
602 /*
603 * ======== postInit ========
604 */
605 Int postInit(Object *hwi, Error.Block *eb);
606
607 /*!
608 * const array to hold all HookSet objects.
609 */
610 config HookSet hooks[length] = [];
611
612 /*! Meta World Only Hwi Configuration Object. */
613 metaonlystruct InterruptObj {
614 String name; /* symbol used for vector table entry */
615 Bool used; /* Interrupt already defined? */
616 Bool useDispatcher; /* Should dispatcher handle this Int? */
617 FuncPtr fxn; /* Dispatched ISR function */
618 PlugFuncPtr pfxn; /* "Hwi_plug'd" ISR function. */
619 };
620
621 /*!
622 * Meta-only array of interrupt objects.
623 * This meta-only array of Hwi config objects is initialized
624 * in Hwi.xs:module$meta$init().
625 */
626 metaonlyconfig InterruptObj interrupt[NUM_INTERRUPTS];
627
628 struct Instance_State {
629 Bits16 disableMask; // Interrupts to mask during ISR.
630 Bits16 restoreMask; // Interrupts to restore after ISR.
631 UArg arg; // Argument to Hwi function.
632 FuncPtr fxn; // Hwi function.
633 Irp irp; // current IRP
634 Ptr hookEnv[];
635 };
636
637 struct Module_State {
638 Char intEvents[16]; // Initial event mapping
639 Bits16 ierMask; // Initial IER mask
640 volatile Int intNum; // Interrupt number
641 Char *taskSP; // temporary storage of interrupted
642 // Task's SP during ISR execution
643 /* ROM */
644 Char *isrStack; // Points to isrStack address
645 Ptr vectorTableBase;// ti_sysbios_family_c64_Hwi0
646 Ptr bss; // bss address
647 Int scw; // secure context word
648
649 Handle dispatchTable[NUM_INTERRUPTS]; // dispatch table
650 };
651 }