1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== HeapStd.xdc ========
    15     *!  Open Issues: 
    16     *!  - Do not really know the largestFreeSize value in HeapStd_getStats() 
    17     */
    18    
    19    /*!
    20     *  ======== HeapStd ========
    21     *  Malloc/free based heap implementation.
    22     *
    23     *  This heap is based on the ANSI C Standard Library functions
    24     *  `malloc()` and `free()` and assumes that these functions are thread-safe.
    25     *  Please refer to the target specific documentation of the ANSI C Standard
    26     *  Library for details.
    27     *
    28     *  The largest free block that can be returned form `malloc()` cannot be
    29     *  determined. Therefore, the property `largestFreeSize` in
    30     *  `{@link Memory#Stats}` returned from `{@link #getStats()}` always returns
    31     *  0.
    32     * 
    33     *  @a(Constraints)
    34     *  The `{@link #alloc()}` function only supports alignment requests up to
    35     *  value returned from
    36     *  `{@link Memory#getMaxDefaultTypeAlign()}`.
    37     */
    38     
    39    @InstanceInitError  /* instance init can fail, call finalize if so */
    40    
    41    module HeapStd inherits xdc.runtime.IHeap {
    42        
    43        /*! @_nodoc */
    44        @XmlDtd
    45        metaonly struct Instance_View {
    46            Ptr             address;
    47            String          label;
    48            Memory.Size     remainSize;
    49            Memory.Size     startSize;
    50        }
    51        
    52        /*!
    53         *  ======== HEAP_MAX ========
    54         *  Maximum heap size of HeapStd
    55         *
    56         *  This parameter defines maximum heap size that can be allocated to a
    57         *  `HeapStd` instance. Using this parameter to create `HeapStd` instances 
    58         *  will disable the internal size checks in `HeapStd` module.
    59         */
    60        const SizeT HEAP_MAX = ~0U;
    61    
    62        /*!
    63         *  ======== E_noRTSMemory ========
    64         *  Error raised if all the RTS heap is used up
    65         *
    66         *  The total size of all `HeapStd` instance allocations added together
    67         *  cannot exceed the `malloc`/`free` heap size determined by
    68         *  `{@link xdc.cfg.Program#heap}`. 
    69         */
    70        config Error.Id E_noRTSMemory = { 
    71            msg: "The RTS heap is used up. Examine Program.heap."
    72        }; 
    73            
    74        /*!
    75         *  ======== A_zeroSize ========
    76         *  Assert that the `{@link #size}` is non-zero on the create
    77         */     
    78        config Assert.Id A_zeroSize = {
    79            msg: "HeapStd_create cannot have a zero size value"
    80        };
    81            
    82        /*!
    83         *  ======== A_align ========
    84         *  Assert that the `{@link #size}` is a power of 2
    85         */     
    86        config Assert.Id A_align = {
    87            msg: "HeapStd_alloc alignment must be a power of 2"
    88        };
    89    
    90        /*! 
    91         *  ======== A_invalidTotalFreeSize ========
    92         *  Assert that remaining size is less than or equal to starting size.
    93         *
    94         *  If this assertion is raised, it means that either incorrect sizes
    95         *  were passed to `{@link #free}` or multiple calls to `{@link #free}`
    96         *  were made with the same buffer.
    97         */     
    98        config Assert.Id A_invalidTotalFreeSize = {
    99            msg: "HeapStd instance totalFreeSize is greater than starting size"
   100        };
   101    
   102        /*!
   103         *  ======== A_invalidAlignment ========
   104         *  Assert that the alignment argument in alloc is valid
   105         *  @_nodoc
   106         *
   107         *  If this assertion is raised, it means that the requested alignment is
   108         *  greater than the maximum alignment allowed on the target.
   109         */
   110        config Assert.Id A_invalidAlignment = {
   111            msg: "HeapStd_alloc - requested alignment is greater than allowed"
   112        };
   113    
   114    instance:
   115    
   116        /*!
   117         *  ======== create ========
   118         *  Create a `HeapStd` heap
   119         *
   120         *  This heap uses the ANSI C Standard Library functions
   121         *  `malloc()` and `free()` to manage memory and assumes that these
   122         *  functions are thread-safe.
   123         *
   124         *  @see HeapStd#Params
   125         */
   126        create();
   127        
   128        /*! 
   129         *  ======== size ========
   130         *  Size (in MAUs) of the heap.
   131         *
   132         *  This parameter specifies the size of the heap managed by a
   133         *  `HeapStd` instance. `HeapStd` is built upon the ANSI C Standard
   134         *  Library functions `malloc()` and `free()`.
   135         *
   136         *  The total size of all `HeapStd` instance allocations added together
   137         *  cannot exceed the `malloc`/`free` heap size determined by
   138         *  `{@link xdc.cfg.Program#heap Program.heap}`. 
   139         *
   140         *  This is a required parameter. It must be set by the caller. Failure
   141         *  to do so, will result in a build error for the static create or an
   142         *  assert for the runtime create.
   143         */    
   144        config Memory.Size size = 0;    
   145    
   146        /*!
   147         *  ======== alloc ========
   148         *  Allocates a block of memory from the heap.
   149         *
   150         *  @a(Constraints)
   151         *  The only alignment currently supported is the default
   152         *  alignment returned by the underlying `malloc()` implementation. 
   153         *  The align value must be less than or equal to the value returned from 
   154         *  `{@link Memory#getMaxDefaultTypeAlign()}`.
   155         *
   156         *  @see IHeap#alloc
   157         */
   158        override Ptr alloc(SizeT size, SizeT align, Error.Block *eb);
   159        
   160        /*!
   161         *  ======== isBlocking ========
   162         *  Returns whether the heap may block during an `HeapStd_alloc()` or
   163         *  `HeapStd_free()`.
   164         *  
   165         *  @a(returns)      
   166         *  Since the implementation of the underlaying ANSI C Standard Library
   167         *  is not known, this function always returns the more restrictive case
   168         *  which is `TRUE`.
   169         */
   170        override Bool isBlocking();    
   171     
   172    internal:
   173    
   174        struct Module_State {
   175            Memory.Size remainRTSSize;      /* Remaining size of rts heap      */
   176        };
   177        
   178        struct Instance_State {
   179            Memory.Size remainSize;         /* Size of the remaining heap.      */
   180            Memory.Size startSize;          /* Starting size of the heap.       */
   181        };
   182    }
   183    /*
   184     *  @(#) xdc.runtime; 2, 1, 0,0; 12-9-2015 17:36:46; /db/ztree/library/trees/xdc/xdc-B06/src/packages/
   185     */
   186