1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*!
14 * ======== IInstance ========
15 * Common instance params
16 *
17 * Every module's instance parameter structure contains a pointer to an
18 * `IInstance.Params` structure named `instance`. So, every instance
19 * parameter defined in this interface may optionally be set when
20 * creating (or constructing) any module's instances.
21 */
22 @DirectCall
23
24 interface IInstance {
25
26 instance:
27
28 /*!
29 * ======== name ========
30 * Name of the instance
31 *
32 * It is possible to "bind" a name to each instance of any module
33 * at the time the instance is created (or constructed).
34 * @p(code) 35 * ModA_Params params;
36 * ModA_Params_init(¶ms);
37 * params.instance->name = "myInstance";
38 * ModA_create(¶ms, NULL);
39 * @p 40 *
41 * The name field must be assigned a pointer to a buffer that persists
42 * as long as the instance that it names exists. Only a reference to
43 * the name is retained in the instance, the name is not copied to a
44 * secondary buffer.
45 *
46 * The configuration parameters that controls if instance names are
47 * supported is `common$.namedInstance`. The parameter is a member of the
48 * structure `{@link xdc.runtime.Types#Common$ common$}`, available in each
49 * module. By default, this parameter is set to `false`, which disables
50 * support for instance names.
51 * Therefore, to enable instance names for a given module `Mod`, configure
52 * the module as follows in your configuration script:
53 * @p(code) 54 * var Mod = xdc.useModule('pkg.Mod');
55 * ModA.common$.namedInstance = true;
56 * @p 57 *
58 * Here is how the static instances are given names at the configuration
59 * time:
60 * @p(code) 61 * var inst = Mod.create();
62 * inst.instance.name = "myInstance";
63 * @p 64 *
65 * If instance names are enabled and used for statically created instances,
66 * the config parameter `{@link xdc.runtime.Text#isLoaded Text.isLoaded}`
67 * must be set to `true` to have these names available at runtime.
68 *
69 * At runtime, assign your instance a name:
70 * @p(code) 71 * #include <package/name/Mod.h>
72 * Mod_Params params;
73 * Mod_Params_init(¶ms);
74 * params.instance->name = "myInstance";
75 * Mod_create(¶ms, NULL);
76 * @p 77 *
78 * If instances have been configured to not support names, it is still
79 * possible to assign to the `instance.name` field of the parameter
80 * structure (as shown above). However, the pointer is not retained
81 * and methods that normally return an instance's name will return
82 * `NULL` instead.
83 */
84 config String name = null;
85 }
86 /*
87 * @(#) xdc.runtime; 2, 1, 0,471; 3-20-2014 17:05:46; /db/ztree/library/trees/xdc/xdc-A32x/src/packages/
88 */
89