![]() |
![]() |
This release note is divided into the following sections:
Introduction, Documentation, What's New, Upgrading And Compatibility Information, Host Support, Dependencies, Device Support, Validation Information, Known Issues, Benchmarks, Versioning, Technical Support And Product Updates,
The following documentation is provided with this release:
Release notes from previous releases are also available in the release notes archive directory.
back to topThis
release is based on DSP/BIOS 6.30.02.
Notes on this release:
BIOS 6.30 cannot be used with the DA830 ROM. BIOS 6.21 is the preferred version for DA830 ROM.
The
'ti.sdo.io' and 'ti.sdo.utils' packages are no longer provided with
SYS/BIOS
These packages are now provided in a separate "IPC" product. Users of these packages simply need to add this other product directory to their package path (XDCPATH) to build their applications.
The ti.sysbios.ipc package and its modules have been deprecated
The
Semaphore, Event, and Mailbox modules were moved from the
ti.sysbios.ipc package into the ti.sysbios.knl package. Please update
your applications to use the ti.sysbios.knl package versions of the
Semaphore, Event, and Mailbox modules. Using the ipc package versions
of these modules will result in build warnings. In a subsequent release
of BIOS, using any module within the ipc package will result in a build
error.
The ti.sysbios.family.arm.m3.Exception module has been deprecated
The
ti.sysbios.family.arm.m3.Exception module functionality has been
enhanced and merged into the ti.sysbios.family.arm.m3.Hwi module.
Please update your applications to use the ti.sysbios.family.arm.m3.Hwi
module to configure exception handling. By default, exceptions will be
reported to CIO with an Error message. Details of the exception can be
seen using Hwi module's "Exception" ROV view. At the expense of
additonal code size, some of this detailed information can ALSO be
routed to the CIO console by setting the Hwi.enableException
configuration flag to true.
Placing of sections using MEM configs is no longer supported (ie MEM.TEXTSEG is unsupported)
All
of the legacy MEM memory segment placment functionality has been
removed. Legacy BIOS users must use Program.sectMap to place memory
sections.
The ti.sysbios.family.c64p.Cache.initSize configuration item is no longer supported
The
ti.sysbios.family.c64p.Cache module no longer supports setting the
Cache sizes. These settings are now managed within a platform and can
be configured using the platform wizard.
SYS/BIOS no
longer
contains all the tools and objects you will need
The XDC tools now provide the SYS/BIOS configuration tools and Platform support. XDC also includes a minimal run-time environment that provides the LOG, System, Asserts, Error handling, Timestamp, and Memory Allocation APIs that will be used by SYS/BIOS applications. Please refer to the Getting Started Guide on where to download the XDC tools and run-time.
SYS/BIOS 6.x has different APIs compared to those in DSP/BIOS 5.x. Configuration scripts are also incompatible between the two releases. To provide easy migration of DSP/BIOS 5.x applications, an API compatibility layer is provided along with a conversion tool that converts configuration scripts to work with XDC and SYS/BIOS 6.x. The API compatibility layer provides 100% C source code compatibility with the exception of a few APIs that are no longer supported. For more complete details of migrating DSP/BIOS 5.x applications and configuration scripts, please refer to Migrating a DSP/BIOS 5 Application to SYS/BIOS 6.
Click here for the list of compilers used to build and validate this release (scroll down to Supported Targets section).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit
Major number, mm
is 2 digit minor number, pp
is a 2 digit patch number, and b
is an unrestricted set of digits used as an incrementing build counter.
To
support multiple side-by-side installations of the product, the product
version is encoded in the top level directory (e.g. bios_6_30_00_00).
Subsequent
releases of patch upgrades will be identified by the patch number, ex.
SYS/BIOS 6.30.01.15 with directory bios_6_30_01_15. Typically, these
patches only include critical bug fixes.
Please note that
version numbers and compatibility keys are NOT the same. For an
explanation of compatibility keys, please refer to the 'Upgrade and
Compatibility Information' section.
Last updated: September 16, 2010 Build Ver: 6.30.03.46 Rev: f46