1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== HeapMin.xdc ========
    15     */
    16    
    17    /*!
    18     *  ======== HeapMin ========
    19     *  Growth-only based heap implementation.
    20     *
    21     *  `HeapMin` is a minimal footprint heap implementation. This module is 
    22     *  is designed for applications that only create module instances and
    23     *  generally only allocate memory at runtime, but never delete created
    24     *  instances or free memory explicitly.
    25     *  
    26     *  For configuration-time `HeapMin.create`, the heap is aligned to 
    27     *  `{@link Memory#getMaxDefaultTypeAlignMeta()}` for those targets that support
    28     *  static alignment. For targets that do not support static alignment, the
    29     *  buffer alignment is undefined.
    30     *
    31     *  When calling `{@link #create()}` at runtime, the client 
    32     *  is responsible for aligning the buffer.
    33     */
    34    
    35    module HeapMin inherits xdc.runtime.IHeap {
    36    
    37        /*! @_nodoc */
    38        @XmlDtd
    39        metaonly struct Instance_View {
    40            Ptr             address;
    41            String          label;
    42            Ptr             buffer;
    43            Memory.Size     remainSize;
    44            Memory.Size     startSize;
    45        }
    46        
    47        /*!
    48         *  ======== A_zeroSize ========
    49         *  Assert that the `{@link #size}` is non-zero on the create
    50         */     
    51        config Assert.Id A_zeroSize  =
    52            {msg: "HeapMin_create cannot have a zero size value"};
    53            
    54        /*! 
    55         *  ======== E_freeError ========
    56         *  Error raised if `{@link #free()}` is called.
    57         *
    58         *  This error is only raised if a `{@link #free()}`
    59         *  is called and `{@link #freeError}` is true.
    60         */
    61        config Error.Id E_freeError = {
    62            msg: "free() invalid in growth-only HeapMin"
    63        };
    64    
    65        /*!
    66         *  ======== freeError ========
    67         *  Flag to control whether `{@link #E_freeError}` is enabled.
    68         * 
    69         *  If true, a `{@link #E_freeError}` error occurs when trying 
    70         *  to free a buffer. 
    71         *
    72         *  If false, no error occurs and the `{@link #free()}` does nothing.
    73         */
    74        config Bool freeError = true;
    75    
    76    instance:
    77    
    78        /*!
    79         *  ======== align ========
    80         *  Alignment of the buffer being managed by this heap instance.
    81         *
    82         *  In the static HeapMin.create() call, the buffer allocated for the
    83         *  HeapMin instance will have the alignment specified by this parameter
    84         *  on targets that support static alignment.
    85         *
    86         *  In the dynamic case, the client must supply the buffer, so it is the
    87         *  client's responsibility to manage the buffer's alignment, and there is
    88         *  no 'align' parameter.
    89         *
    90         *  The specified `align` parameter must be a power of 2.
    91         *
    92         *  The default alignment of zero causes the buffer to get aligned using
    93         *  {@link Memory#getMaxDefaultTypeAlignMeta()}.
    94         */
    95        metaonly config SizeT align;
    96    
    97        /*!
    98         *  ======== create ========
    99         *  Create a `HeapMin` heap
   100         *
   101         *  This heap is a growth-only heap that is intended to be used by
   102         *  systems that never delete objects or free memory.  Objects can be
   103         *  created at runtime based on values determined at runtime, but
   104         *  objects can not be deleted.
   105         *
   106         *  @see HeapMin#Params
   107         */
   108        create();
   109        
   110        /*!
   111         *  ======== sectionName ========
   112         *  Section name of the heap
   113         *
   114         *  When creating heaps during configuration, this parameter specifies
   115         *  where the heap's buffer will be placed. This parameter is passed as
   116         *  the section name in the `{@link Memory#staticPlace}` function.
   117         *
   118         *  @see Memory#staticPlace
   119         */
   120        metaonly config String sectionName = null;
   121    
   122        /*!
   123         *  ======== buf ========
   124         *  Buffer that will be managed by the heap instance.
   125         *
   126         *  When creating a heap at runtime, the user must supply the memory
   127         *  that the heap will manage.  It is up to the caller to align
   128         *  the buffer as needed.
   129         *
   130         *  This parameter is ignored when creating heaps during configuration.
   131         */
   132        config Ptr buf = 0;
   133    
   134        /*!
   135         *  ======== size ========
   136         *  Size (in MADUs) of the heap.
   137         *
   138         *  This parameter specifies the size of the heap managed by a
   139         *  `HeapMin` instance.  In the static case, a buffer of length `size` 
   140         *  will be created.  In the dynamic case, `size` specifies the size of 
   141         *  the buffer (i.e. parameter `buf`) that the caller provides.
   142         *
   143         *  This is a required parameter. It must be set by the caller. Failure
   144         *  to do so, will result in a build error for the static create or an
   145         *  `{@link #A_zeroSize}` assert for the runtime create.
   146         */
   147        config Memory.Size size = 0;
   148        
   149        /*!
   150         *  ======== alloc ========
   151         *  Allocate a block of memory from the heap.
   152         *
   153         *  @a(Constraints)
   154         *  The alignment must be a power of 2.
   155         *
   156         *  @see IHeap#alloc
   157         */
   158        override Ptr alloc(SizeT size, SizeT align, Error.Block *eb);    
   159    
   160        /*!
   161         *  ======== free ========
   162         *  Free a block of memory back to the heap.
   163         *
   164         *  This is a growth only heap. Calling the `HeapMin_free` function
   165         *  will result in a `{@link #E_freeError}` error unless
   166         *  `{@link #freeError}` is set to `false`.
   167         *
   168         *  @see IHeap#free
   169         */
   170        override Void free(Ptr block, SizeT size);
   171        
   172        /*!
   173         *  ======== isBlocking ========
   174         *  Can this heap block the caller
   175         *
   176         *  @a(returns)
   177         *  `HeapMin` always returns `FALSE` since it never blocks on a
   178         *  resource.
   179         */
   180        override Bool isBlocking();    
   181    
   182    internal:
   183    
   184        struct Instance_State {
   185            Char        buf[];             /* Address of buffer being managed  */
   186            Memory.Size remainSize;        /* Size of remaining heap           */
   187            Memory.Size startSize;         /* Size of heap at the start        */
   188        };
   189    }
   190    /*
   191     *  @(#) xdc.runtime; 2, 1, 0,438; 12-19-2013 19:53:36; /db/ztree/library/trees/xdc/xdc-z63x/src/packages/
   192     */
   193