1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== IHeap.xdc ========
15 *! - if we ever change the name of this interface, we should change it to
16 *! IMemoryProvider
17 */
18
19 /*!
20 * ======== IHeap ========
21 * Interface to heap functions.
22 *
23 * All heap implementations inherit from this interface.
24 * The implementations can have additional configuration
25 * parmeters and functions.
26 *
27 */
28 interface IHeap {
29
30 instance:
31
32 /*!
33 * ======== alloc ========
34 * Allocates a block of memory from the heap.
35 *
36 * This method returns a block of memory from the heap.
37 * It is called by the `{@link xdc.runtime.Memory#alloc()}` function.
38 *
39 * @param(size) size (in MADUs) of the block
40 * @param(align) alignment (in MADUs) of the block
41 * @param(eb) pointer to error block
42 *
43 * @a(returns) Returns the address of the allocated memory.
44 */
45 Ptr alloc(SizeT size, SizeT align, Error.Block *eb);
46
47 /*!
48 * ======== create ========
49 * Create a heap.
50 *
51 * See specific `IHeap` implementation for parameters used.
52 */
53 create();
54
55 /*!
56 * ======== free ========
57 * Free a block of memory back to the heap.
58 *
59 * This method gives back a block of memory to a heap.
60 * It is called by the `{@link xdc.runtime.Memory#free()}` function.
61 *
62 * @param(block) non-`NULL` address of allocated block to free
63 * @param(size) size (in MADUs) of the block of memory to free
64 */
65 Void free(Ptr block, SizeT size);
66
67 /*!
68 * ======== isBlocking ========
69 * Returns whether the heap may block during an `{@link #alloc()}` or
70 * `{@link #free()}`.
71 *
72 * @a(returns) If the heap might block, `TRUE` is returned.
73 * If the heap does not block, `FALSE` is returned.
74 */
75 Bool isBlocking();
76
77 /*!
78 * ======== getStats ========
79 * Retrieve the statistics from the heap.
80 *
81 * The caller passes in a pointer to a `{@link xdc.runtime.Memory#Stats}`
82 * structure and `getStats` fills in this structure.
83 *
84 * This function is called by the `{@link xdc.runtime.Memory#getStats()}`
85 * function.
86 *
87 * @param(stats) non-`NULL` pointer to an output buffer
88 */
89 Void getStats(Memory.Stats *stats);
90 }
91 /*
92 * @(#) xdc.runtime; 2, 1, 0,421; 6-24-2013 18:59:41; /db/ztree/library/trees/xdc/xdc-z52x/src/packages/
93 */
94