1    /*!
     2     *  ======== Reset ========
     3     *  Startup reset function manager
     4     *
     5     *  This module defines an initial reset function and can be used without
     6     *  requiring any other `xdc.runtime` module.  The reset function is called
     7     *  as early as possible in the application startup and is intended for
     8     *  platform-specific hardware initialization.
     9     *
    10     *  The reset function sequentially calls each of the functions added to the
    11     *  `{@link #fxns}` array starting from index 0.  If
    12     *  `{@link Startup#resetFxn Startup.resetFxn}` is defined, it is called
    13     *  before any of the functions defined by the `fxns` array.
    14     *
    15     *  By providing an array of startup functions, rather than a single function
    16     *  as `{@ilnk Startup}` does, modules that need very early initialization 
    17     *  can simply add their initialization to the list of functions to be called
    18     *  without having to implement a "chaining" mechanism or requiring the user
    19     *  to implement and maintain an application reset function.
    20     *
    21     *  @a(Warning)
    22     *  The reset function is _not_ supported on all platforms and, as a result,
    23     *  you should never place any "portable" code that is required for your
    24     *  application in this function.  Use the `@{link Startup}` module to
    25     *  define required application startup functions.
    26     *  
    27     *  @see Startup
    28     */
    29    @Template("xdc/runtime/Reset.xdt")
    30    metaonly module Reset
    31    {
    32        /*!
    33         *  ======== fxns ========
    34         *  List of functions to call at reset
    35         *
    36         *  This array defines the functions that will be executed by the reset
    37         *  initialization function (`xdc_runtime_Startup_reset__I`) _in addition
    38         *  to_ the function specified by `@{link Startup#resetFxn}`.
    39         *
    40         *  The following code fragment shows how to add the externally defined
    41         *  function `myReset()` to this array.
    42         *  @p(code)
    43         *      var Reset = xdc.useModule("xdc.runtime.Reset");
    44         *      Reset.fxns[Reset.fxns.length++] = "&myReset";
    45         *  @p
    46         *
    47         *  @a(Warning)
    48         *  Although the functions specified in `fxns[]` are ordinary C functions,
    49         *  they are often called _before_ the C runtime is fully initialized;
    50         *  e.g., they may be called _before_ static variables are initialized.
    51         *  Reset functions should only assume that a minimal execution stack has
    52         *  initialized.
    53         *
    54         *  @see Startup#resetFxn
    55         */
    56        metaonly config xdc.runtime.Startup.InitFxn fxns[] = [];
    57    }
    58    /*
    59     *  @(#) xdc.runtime; 2, 1, 0,384; 9-3-2012 16:22:19; /db/ztree/library/trees/xdc/xdc-y35x/src/packages/
    60     */
    61