1 /*
2 * Copyright (c) 2011, Texas Instruments Incorporated
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 *
9 * * Redistributions of source code must retain the above copyright
10 * notice, this list of conditions and the following disclaimer.
11 *
12 * * Redistributions in binary form must reproduce the above copyright
13 * notice, this list of conditions and the following disclaimer in the
14 * documentation and/or other materials provided with the distribution.
15 *
16 * * Neither the name of Texas Instruments Incorporated nor the names of
17 * its contributors may be used to endorse or promote products derived
18 * from this software without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31 * */
32 /*
33 * ======== MemoryProtect.xdc ========
34 *
35 *
36 */
37
38 package ti.sysbios.family.c64p;
39
40 /*!
41 * ======== MemoryProtect ========
42 * MemoryProtect Module
43 *
44 * This module provide an API to {@link #getPA() get} and to
45 * {@link #setPA() set} the permission attributes of a memory range.
46 * A memory range can be set to user {@link #MPPA_UX executable},
47 * user {@link #MPPA_UW writable}, user {@link #MPPA_UR readable},
48 * supervisor {@link #MPPA_SX executable}, supervisor
49 * {@link #MPPA_SW writable}, or supervisor {@link #MPPA_SR readable}.
50 * Setting a memory range to only user readable, writable or executable
51 * should be done with caution because BIOS executes in supervisor mode.
52 * Whenever setting the permission attributes of a memory range,
53 * the {@link #MPPA_LOCAL local} CPU access field must be set, if the
54 * local CPU accesses the memory range. If the local field is not set,
55 * an exception is generated if the CPU tries to access the memory range.
56 *
57 * This module is to be used in correlation with the
58 * {@link ti.sysbios.family.c64p.Exception Exception} module.
59 * When this module is in use, external exceptions are enabled by default.
60 * Any memory protection fault which arises generates an exception.
61 * This exception is processed and decoded by the Exception module.
62 *
63 * An example of setting Local L2 RAM to be supervisor read-only and
64 * CPU accessible:
65 *
66 * @p(code) 67 * UInt32 paMask;
68 * paMask = MemoryProtect_MPPA_LOCAL |
69 * MemoryProtect_MPPA_SR;
70 *
71 * MemoryProtect_setPA((Ptr)0x11800000, 0x40000, paMask);
72 * @p 73 *
74 * @p(html) 75 * <h3> Calling Context </h3>
76 * <table border="1" cellpadding="3">
77 * <colgroup span="1"></colgroup> <colgroup span="5" align="center"></colgroup>
78 *
79 * <tr><th> Function </th><th> Hwi </th><th> Swi </th><th> Task </th><th> Main </th><th> Startup </th></tr>
80 * <!-- -->
81 * <tr><td> {@link #getPA} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
82 * <tr><td> {@link #setPA} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
83 * <tr><td colspan="6"> Definitions: <br />
84 * <ul>
85 * <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
86 * <li> <b>Swi</b>: API is callable from a Swi thread. </li>
87 * <li> <b>Task</b>: API is callable from a Task thread. </li>
88 * <li> <b>Main</b>: API is callable during any of these phases: </li>
89 * <ul>
90 * <li> In your module startup after this module is started (e.g. Mod_Module_startupDone() returns TRUE). </li>
91 * <li> During xdc.runtime.Startup.lastFxns. </li>
92 * <li> During main().</li>
93 * <li> During BIOS.startupFxns.</li>
94 * </ul>
95 * <li> <b>Startup</b>: API is callable during any of these phases:</li>
96 * <ul>
97 * <li> During xdc.runtime.Startup.firstFxns.</li>
98 * <li> In your module startup before this module is started (e.g. Mod_Module_startupDone() returns FALSE).</li>
99 * </ul>
100 * </ul>
101 * </td></tr>
102 *
103 * </table>
104 * @p 105 */
106
107 @ModuleStartup
108
109 module MemoryProtect
110 {
111 // -------- Module Types --------
112
113 /*
114 * MPPA Permission Attribute Register bitmasks.
115 */
116 const UInt32 MPPA_UX = 0x00000001; /*! User mode may execute */
117 const UInt32 MPPA_UW = 0x00000002; /*! User mode may write */
118 const UInt32 MPPA_UR = 0x00000004; /*! User mode may read */
119 const UInt32 MPPA_SX = 0x00000008; /*! Supervisor mode may execute */
120 const UInt32 MPPA_SW = 0x00000010; /*! Supervisor mode may write */
121 const UInt32 MPPA_SR = 0x00000020; /*! Supervisor mode read */
122 const UInt32 MPPA_LOCAL = 0x00000100; /*! Local CPU may access */
123
124 /*!
125 * ======== getPA ========
126 * Gets the PA (Permission Attribute) corresponding to addr.
127 *
128 * @param(addr) address of memory location for which the PA applies
129 * @param(paMask) ptr to location where PA mask for addr is stored
130 *
131 * @b(returns) if address doesn't belong to any configured MPC then
132 * FALSE, otherwise TRUE and *paMask contains addr's
133 * MPPA setting
134 */
135 Bool getPA(Ptr addr, UInt32 *paMask);
136
137 /*!
138 * ======== setPA ========
139 * Sets the PA (Permission Attribute) corresponding to addr/size.
140 *
141 * The PA is applied to all addresses that are spanned by the
142 * memory block.
143 *
144 * @param(addr) begin address of memory block for which the PA applies
145 * @param(size) size of memory block
146 * @param(paMask) PA mask to assign for the memory block
147 *
148 * @b(returns) if address doesn't belong to any configured MPC then
149 * FALSE, otherwise TRUE and PA was written to addr's
150 * MPPA register
151 */
152 Bool setPA(Ptr addr, SizeT size, UInt32 paMask);
153
154 /*!@_nodoc 155 * ======== getPageSize ========
156 * Gets the page size corresponding to addr.
157 *
158 * @param(addr) address of memory location for which the PA applies
159 * @param(pageSize) pointer to location where the page size is stored
160 *
161 * @b(returns) FALSE - address doesn't belong to any configured MPC
162 * TRUE - *pageSize contains addr's MPC page size
163 */
164 Bool getPageSize(Ptr addr, UInt *pageSize);
165
166 /*!@_nodoc 167 * ======== getPrivMode ========
168 * Retrieves the current privilege mode
169 *
170 * @b(returns) current privilege mode
171 */
172 UInt getPrivMode();
173
174 /*!@_nodoc 175 * ======== setPrivMode ========
176 * Sets the privilege mode
177 *
178 * @param(mode) the privilege mode to set
179 */
180 Void setPrivMode(UInt mode);
181
182
183 internal:
184
185 /*!
186 * Struct defining the bit range of an address
187 */
188 struct BitRange {
189 Char msb;
190 Char lsb;
191 };
192
193 /*!
194 * Each MPC needs to implement MPLCK.
195 * DMC/PMC/UMA all conform to the struct below.
196 */
197 struct Lock {
198 volatile UInt32 mpLk0; /* lock bits 31-0 */
199 volatile UInt32 mpLk1; /* lock bits 63-32 */
200 volatile UInt32 mpLk2; /* lock bits 95-64 */
201 volatile UInt32 mpLk3; /* lock bits 127-96 */
202 volatile UInt32 mpLkCmd; /* lock command register */
203 volatile UInt32 mpLkStat; /* lock status register */
204 };
205
206 /*!
207 * Struct defining the fault registers
208 */
209 struct Fault {
210 volatile UInt32 mpFar; /* MPC Fault Address Register */
211 volatile UInt32 mpFsr; /* MPC Fault Status Register */
212 volatile UInt32 mpFcr; /* MPC Fault Clear Register */
213 };
214
215 /*!
216 * Key represents the 128-bit key used for locking
217 * and unlocking a controller's permission attribute entries.
218 * It is used for writing to the MPLK0-MPLK3 registers.
219 */
220 struct Key {
221 UInt32 key0; /* bits 0-31 of 128-bit key */
222 UInt32 key1; /* bits 32-63 of 128-bit key */
223 UInt32 key2; /* bits 64-95 of 128-bit key */
224 UInt32 key3; /* bits 96-127 of 128-bit key */
225 };
226
227 /*!
228 * Struct defining a controller
229 */
230 struct Controller {
231 Fault *mpFault; /* addr of MP Fault registers */
232 Lock *mpLck; /* addr of MP Lock registers */
233 UInt32 *mppaTab; /* addr of base of MP PA table */
234 UInt32 *mpCfg; /* addr of MP Configuration register */
235 UInt32 nPages; /* # pages in the MPC */
236 UInt32 evtNum; /* Event number for controller */
237 };
238
239 /*!
240 * The following values relate to indexing into the module state
241 * controller array. Subtract 1 from the value before using it as an
242 * index into the 0-based array (NONE isn't used to index the array).
243 */
244 const UInt NONE = 0;
245 const UInt UMAP0 = 1;
246 const UInt UMAP1 = 2;
247 const UInt DMC = 3;
248 const UInt PMC = 4;
249 const UInt UMC = UMAP0;
250
251 /*! lock/unlock values */
252 const UInt LCKUNLOCK = 0x00000001;
253 const UInt LCKLOCK = 0x00000002;
254 const UInt LCKKEYR = 0x00000004;
255 const UInt LKSTATLK = 0x00000001;
256
257 /*! The key values used for locking/unlocking PA table */
258 config Key key = {
259 key0: 0x90abcdef,
260 key1: 0x12345678,
261 key2: 0x87654321,
262 key3: 0xfedcba09
263 };
264
265 /*!
266 * Region Extract Masks table indexed by [controller(0-3)][region(0-1)].
267 * The constants used are fixed based on the GEM architecture spec.
268 * They are based on the minimum theoretical page size (lower constant)
269 * and the number of pages (higher constant minus lower constant).
270 * However, in reality, the actual minimum page size is floored at
271 * some minimum (i.e., the "size" parameter can't, per the
272 * HW design spec, be lower than some minimum (2 for DMC/PMC, 6 for UMC).
273 */
274 config BitRange regExtMasks[4][2];
275
276 /*!
277 * This array is used to map the MegaByte field of an address
278 * (0x00N00000) to the controller that controls that address.
279 * An MPC's address range falls within and is wholy contained
280 * in the MegaByte hex digit.
281 */
282 config Char megaByte2MPC[16];
283
284 /*!
285 * Array of addresses that mark the begin of region 0 for each MPC.
286 * Each MPC contains two regions (0 & 1), however, the first two
287 * entries correspond to the two "regions" of UMC (UMC_P0 & UMC_P1),
288 * and as such the entries for them are forced to the max address
289 * value such that any compare that uses them will be < them,
290 * thus indicating region 0.
291 */
292 config UInt regionCompare[4];
293
294 /*!
295 * Array of addresses that mark the end of region 0 for each MPC.
296 */
297 config UInt regionEnd[4];
298
299 /*! L1 program memory controller */
300 config Controller pmcCtrl;
301
302 /*! L1 data memory controller */
303 config Controller dmcCtrl;
304
305 /*! L2 unified memory controller */
306 config Controller umcCtrl;
307
308 /*!
309 * ======== decodeRegion ========
310 * Determine the beginning and end page numbers for region.
311 *
312 * Validate begAddr/endAddr range to be within internal address space.
313 * Return region (UMAP0/UMAP1/DMC/PMC), beginning and ending page
314 * numbers if valid. Returns -1 if complete address range is not valid.
315 */
316 Int decodeRegion(UInt32 begAddr, UInt32 endAddr,
317 UInt32 *begPage, UInt32 *endPage);
318
319 /*!
320 * ======== getAddrPageSize ========
321 * Returns the page size corresponding to addr.
322 */
323 Int getAddrPageSize(Ptr addr);
324
325 /*!
326 * ======== lock ========
327 * Locks the permission attribute.
328 *
329 * Locks the permission attribute table entries for the
330 * specified controller, using the specified key.
331 */
332 Void lock(Controller *ctrl, Key *key);
333
334 /*!
335 * ======== makeLocal ========
336 * Convert address into a local address
337 *
338 * Validate addr to be a GEM internal address & convert addr into
339 * its local address if global. Returns TRUE if addr is a valid GEM
340 * internal address, and fills space with local/global code (1/0).
341 * Returns FALSE if addr is not a valid GEM internal address. space
342 * is valid only when TRUE is returned.
343 */
344 Bool makeLocal(UInt *addr, UInt *space);
345
346 /*!
347 * ======== readPA ========
348 * Reads the permission attribute
349 *
350 * Returns the permission attribute for the specified
351 * page within the specified controller.
352 */
353 UInt32 readPA(Controller *ctrl, UInt page);
354
355 /*!
356 * ======== unlock ========
357 * Unlocks the permission attribute.
358 *
359 * Unlocks the permission attribute table entries for the
360 * specified controller, using the specified key.
361 */
362 Void unlock(Controller *ctrl, Key *key);
363
364 /*!
365 * ======== writePA ========
366 * Writes the permission attribute
367 *
368 * Writes the permission attribute perm for the specified
369 * page within the specified controller. The permission attribute
370 * entries need to be unlocked first and then locked afterwards.
371 */
372 Void writePA(Controller *ctrl, UInt page, UInt32 perm);
373
374 /* Module state */
375 struct Module_State {
376 Controller *controllers[];
377 }
378 }
379 /*
380 * @(#) ti.sysbios.family.c64p; 2, 0, 0, 0,453; 1-20-2011 12:27:53; /db/vtree/library/trees/avala/avala-o26x/src/ xlibrary
381 382 */
383