Benchmark | Cycles |
Interrupt latency | 87 |
HWI_enable | 16 |
HWI_disable | 24 |
HWI_dispatch: Interrupt prolog for calling C function | 64 |
HWI_dispatch: Interrupt epilog following C function call | 64 |
SEM_ipost: Hardware interrupt to blocked task | 568 |
SWI_post: Hardware interrupt to software interrupt | 192 |
SWI_enable | 72 |
SWI_disable | 24 |
SWI_post: Post software interrupt again | 32 |
SWI_post: Post software interrupt, no context switch | 56 |
SWI_post: Post software interrupt, context switch | 120 |
TSK_enable | 88 |
TSK_disable | 48 |
TSK_create: Create a task, no context switch | 664 |
TSK_create: Create a task, context switch | 760 |
TSK_delete | 424 |
TSK_setpri: Set a task priority, no context switch | 272 |
TSK_setpri: Lower the current task own priority, context switch | 368 |
TSK_setpri: Raise a ready task priority, context switch | 368 |
TSK_yield | 232 |
SEM_post: Post a semaphore, no waiting task | 32 |
SEM_post: Post a semaphore, no context switch | 184 |
SEM_post: Post a semaphore, context switch | 264 |
SEM_pend: Pend on a semphore, no context switch | 24 |
SEM_pend: Pend on a semphore, context switch | 232 |
MBX_post: Post a mailbox, no tasks waiting | 112 |
MBX_post: Post a mailbox, no context switch | 272 |
MBX_post: Post a mailbox, context switch | 424 |
MBX_pend: Pend on a mailbox, no context switch | 120 |
MBX_pend: Pend on a mailbox, context switch | 248 |
LCK_post: Post a lock, no ownership relinquishment | 16 |
LCK_post: Post a lock, no context switch | 32 |
LCK_post: Post a lock, context switch | 280 |
LCK_pend: Pend on a self-owned lock | 32 |
LCK_pend: Pend on a lock, no context switch | 40 |
LCK_pend: Pend on a lock, context switch | 240 |
CLK_gethtime | 64 |
CLK_getltime | 16 |
LOG_event | 24 |
LOG_printf | 32 |
STS_add | 24 |
STS_delta | 16 |
STS_set | 16 |
MEM_alloc: Memory allocated on first block | 208 |
MEM_alloc: Memory allocated on second block | 216 |
MEM_alloc: Memory allocated on third block | 224 |
MEM_alloc: Memory allocated on fourth block | 240 |
MEM_free: Memory coalesces no block | 216 |
MEM_free: Memory coalesces one block | 224 |
MEM_free: Memory coalesces two blocks | 232 |
PIP_alloc | 104 |
PIP_free | 96 |
PIP_get | 104 |
PIP_put | 96 |
PIP_peek | 24 |
QUE_dequeue | 8 |
QUE_empty | 0 |
QUE_enqueue | 8 |
QUE_get | 16 |
QUE_insert | 8 |
QUE_put | 8 |
QUE_remove | 8 |
MSGQ_alloc | 112 |
MSGQ_put | 56 |
MSGQ_get with messages | 56 |
MSGQ_get with no messages | 72 |
MSGQ_free | 56 |