DSP/BIOS 5.41.08.30is
a patch release based on DSP/BIOS 5.41. This release includes
separate installers for CCSv3 and CCSv4. The target content
(libraries and .h files) are identical in both installations. The
main difference is that different tools are provided in each release as
necessary to work with CCSv3 or CCSv4. It is ok to install both CCS versions on the same computer but they must not be installed under same root directory.
The main changes in this release are bug fixes (listed below).
CCSv4
users will need to check their installed CCS version has XDCtools
version 3.16.03 or higher to use the product for evm5515. The XDCtools product can be
downloaded here.
Enchanements and Defects Fixed:
id
Headline SDOCM00074379
BIOS 5: add makefile for hello example for each target for CCSv4
version and update Setup Guide CCSv4 SDOCM00074259 update RTA plugin for BIOS 5.41.0x to bypass RTDX on CCSv5 Linux environment SDOCM00073575 BIOS 5 RTA plugin issue in CCSv5
For new versions and updates to the BIOS product please check the Target Content Infrastructure site here.
DSP/BIOS 5.41.08.30 is binary compatible with DSP/BIOS 5.33 (and all the way
back to DSP/BIOS 5.21). Users do not need to recompile your source
files or libraries when updating to BIOS 5.41. However users *must*
rebuild their configuration since the generated linker .cmd file
(<prog>cfg.cmd) is different.
Solaris host is no longer supported in this release.
Customer-critical bug
fixes to earlier releases will be available to Solaris users if
required.
DSP/BIOS 5.41 does not support TMS320C54xx devices. Users of
such devices
should continue use DSP/BIOS 5.31.xx earlier releases. For
customer-critical
54xx-related issues, TI will continue to provide fixes to earlier
versions when
needed.
Compatibility Key Definitions
Compatibility keys are intentionally independent of Marketing
product
numbers and are intended to:
Enable tooling to
identify incompatibilities between components, and
Convey a level of
compatibility between different releases to set end user expectations.
Compatibility keys are composed of 3 comma-delimited numbers -
M,S,R -
where:
M = Major.
A difference in M indicates a break in compatibility.
S = Source.
A difference in S indicates source compability.
That is, the user's source doesn't require change, but does
require rebuilding.
R = Radix.
A difference in R indicates an introduction of new features, but
compatibility with previous interfaces has not broken. If libraries are
provided by the package, an application must re-link with the new
libraries, but not rebuild from source.
The following issues are known to affect this release:
To
operate within TMS320C6748 and OMAPL138 device constraints, it must be
ensured that no off-chip accesses to DDR memories occur while PLL1 is
bypassed. The BIOS Power Manager (PWRM) provides two sleep modes
where this constraint is a concern: PWRM_SLEEP, when PLL1 is allowed to
be bypassed, and PWRM_DEEPSLEEP.
PWRM, and the
underlying PSCL and PMI layers have been implemented with the goal of
minimizing the impact of this constraint upon the user. However,
there remain some user-domain memory placement requirements, for
invoking these two sleep modes.
The following items must
be placed in on-chip memory. Either L2 or L3 memory (referred to
as IRAM or L3_CBA_RAM in BIOS configuration) can be used. Note
that L2 memory will provide faster performance compared to L3.
Where applicable, examples of how to control this with textual
configuration are shown in brackets.
1) The .bios section. [bios.MEM.BIOSSEG = prog.get("IRAM");] 2) The .hwi_vec section. [bios.MEM.HWIVECSEG = prog.get("IRAM");] 3) The .bss section. [bios.MEM.BSSSEG = prog.get("IRAM");] 4) The .pmonchip section. [bios.PWRM.ONCHIPMEMSEG = prog.get("IRAM");] 5) The .clk section (if CLK is enabled as a wakeup interrupt). [bios.CLK.OBJMEMSEG = prog.get("DDR");] 6)
The stack of the task from which PWRM_sleepDSP is being invoked. [To
default all task stacks to IRAM: bios.TSK.STACKSEG = prog.get("IRAM");] 7) The interrupt stack (the .stack section) if the HWI dispatcher is used. [bios.MEM.STACKSEG = prog.get("IRAM");] 8) Any user-provided CLK functions (if CLK is enabled as a wakeup interrupt) (code
and data). 9) Any user-provided wakeup ISR functions (code and data). 10) Any runtime library functions (e.g., math routines) required by the user functions that run in the context of a wakeup ISR.
The
new Power Manager (PWRM module) for C6748 devices optionally uses two
packages (PMI and PSCL) for implementing low-level power control
functionality. When the PWRM module is enabled in your DSP/BIOS
configuration, it will attempt to link to the libraries in these
packages. This requires that the paths to the PMI and PSCL
libraries be included in the linker search path. These paths are
included by default in the CCSv3 project files for the DSP/BIOS
examples for
the evm6748 and evmOMAPL138 platforms. If you are creating your
own CCSv3 project files you should similarly include the following
paths
for the linker: -i"%BIOS_INSTALL_DIR%/packages/ti/pscl/lib"
-i"%BIOS_INSTALL_DIR%/packages/ti/pmi/lib". CCSv4 projects using
PWRM will also require the user to add the libraries to the linker
search path.
The
default V/F setpoints for PWRM are not included in the documentation.
The following table represents the default V/F setpoints.
For the evm6748 and evmOMAPL138 platforms, the default setpoints supported by the default scaling configuration libraries are: For the CPU domain (PLL0):
I2C
communication instabilities have been seen on certain Beta C6748 and
OMAPL138 SOMs. The instability occurs after commanding the DCDC3
output of the TPS65070 to move to or from 1.0V. The output
voltage changes as expected, but further I2C communication with the
TPS65070 may fail. (No issue has been seen for setpoints with
voltages of 1.1V and 1.2V.) For affected SOMs, scaling to/from
1.0V should be avoided, until the root cause and a workaround are
identified.
PWRM does not update DDR timing parameters
as part of scaling PLL1 on the C6748 and OMAPL138 devices. This
is not clearly described in current documentation. Depending upon
your DDR configuration, it may be necessary for you to update timing
parameters, after calling PWRM_changeSetpoint() to scale PLL1.
After
creating a sleep6x project for BIOS 5.41.08.30 for evm6748 or
evmOMAPL138 and adding the supplied sleep6x.c and sleep6x.tcf files
from the example folders, the user will still be required to go to
"build properties" for the project. The user will need to add the
pmi.a674 and pmi_ctl_null.a674 libraries from the C:\Program
Files\Texas Instruments\bios_5.41.08.30\packages\ti\pmi\lib directory
to the include search path.
Click on the "+" button to add a directory to the search path. Add --> "C:\Program Files\Texas Instruments\bios_5.41.08.30\packages\ti\pmi\lib" or "${BIOS_LIB_DIR}\..\..\pmi\lib" NOTE:
make sure this is added as the last entry in the search path
items. You can move it up or down with the arrows to the right of
the window pane.
For the vfscale6x example follow the steps above but add the pmi and pcsl library directories to the include search path.
"C:\Program Files\Texas Instruments\bios_5.41.08.30\packages\ti\pmi\lib" or "${BIOS_LIB_DIR}\..\..\pmi\lib" "C:\Program Files\Texas Instruments\bios_5.41.08.30\packages\ti\pscl\lib" or "${BIOS_LIB_DIR}\..\..\pscl\lib"
Id Headline
SDOCM00068761 Update platform-related readme.txt files, add links to .hlp from top-level release notes SDOCM00066599 PWRM_changeSetpoint API description should clarify it doesn't update DDR timings SDOCM00066598
I2C communication failures with PMIC during transitions to/from 1.0V on
some C6748 and OMAPL138 Beta SOMs SDOCM00065264 MPC settings are incorrect for 643x SDOCM00062971
BIOS 5.41.01 PWRM sleep6x and vfscale6x examples for
evm6748/evmOMAPL138 requires user to add libraries to project manually SDOCM00060862 DM648 CLK_countspms() returns # of clock cycles SDOCM00058656 BIOS 5 ROV - LOG view should use RTA decoder SDOCM00058389 Stairstep RTA example does not run correctly for simulator SDOCM00058088 BIOS 5 RTA - Primus simulator requires reset in between loads SDOCM00058087 BIOS 5 RTA - On primus simulator, fails if RTA already open SDOCM00057506 BIOS 5 RTA control panel should separate STS and CPU Load SDOCM00057326 BIOS 5 RTA - Support LOG_printf4 SDOCM00056732 BIOS 5 RTA - CPU Load broken on 55x simulator SDOCM00056731 BIOS 5 RTA - Over XDS560, RTDX fails if RTA is open when program loaded SDOCM00056730 BIOS 5 RTA Over USB or 510USB, RTDX fails after 2nd time program is loaded SDOCM00054997 RTA stops streaming for the stairstep example on 64P targets when program reloaded
All
releases have 4 digits (M.mm.pp.bb). This includes GA and
pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with
a suffix (e.g. 5.41.00.17_eng or 5.41.00.17_beta).
This
product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as
an incrementing build counter.
To support
multiple side-by-side installations of the product, the product version is
encoded in the top level directory, ex. bios_5_41_00_17.
Subsequent
releases of patch upgrades will be identified by the patch number, ex. BIOS 5.41.01.18 with directory bios_5_41_01_18. Typically, these patches
only include critical bug fixes.
Please note
that version numbers and compatibility keys are NOT the same. For an explanation
of compatibility keys, please refer to the 'Upgrade and Compatibility
Information' section.