DSP/BIOS 5.33.05 Release Notes

This release note is divided into the following sections:

Introduction, Documentation, What's New, Upgrading And Compatibility Information, Host Support, Dependencies, Device Support, Validation Information, Known Issues, Benchmarks, Versioning, Technical Support And Product Updates,


Introduction

DSP/BIOS 5.33.05 is a patch release based on DSP/BIOS 5.33.04:

Please read the Setup Guide for help installing and setting up your environment to use DSP/BIOS 5.33.05.

back to top

Documentation

The following documentation is provided with this release:

Additional release note documentation:

Release notes from previous releases are also available in the release notes archive directory.

back to top

What's New

Defects Fixed: 
Id                              Headline
SDOCM00057038    CLK_gethtime() can return incorrect value (too small by one internal timer period) on faster 28x devices
SDOCM00056832    enable timer should be set to true for evm6747
SDOCM00056786    BIOS 55x configuration files should use LARGE model as default
SDOCM00056725    BIOS should use a separate lock for MEM and RTS to avoid deadlock in filesystem/USB app
SDOCM00056575    enable RTA/RTDX channels to simpify CCSv4-based RTA
SDOCM00056484    validate 28x BIOS with latest 5.2.0 codegen tools
SDOCM00056305    add support for 28x Piccolo (2802x/2803x) and Delfino (2834x) devices
SDOCM00053866    add BIOS support for 6748 and OMAPL138 device families
SDOCM00053801    add BIOS support for DRA457 and DRA459 devices
SDOCM00053517    SYS_printf() should support %f for the 28x floating point libraries (.a28FP)
back to top

Upgrading And Compatibility Information

DSP/BIOS is binary compatible with DSP/BIOS 5.32 (and all the way back to DSP/BIOS 5.21). Users do not need to recompile your source files or libraries when updating to BIOS 5.33. However users *must* rebuild their configuration since the generated linker .cmd file (<prog>cfg.cmd) is different.

Solaris host is no longer supported in this release. Customer-critical bug fixes to earlier releases will be available to Solaris users if required.

DSP/BIOS 5.33 does not support TMS320C54xx devices. Users of such devices should continue use DSP/BIOS 5.31.xx earlier releases. For customer-critical 54xx-related issues, TI will continue to provide fixes to earlier versions when needed.

Compatibility Key Definitions

Compatibility keys are intentionally independent of Marketing product numbers and are intended to:

  1. Enable tooling to identify incompatibilities between components, and
  2. Convey a level of compatibility between different releases to set end user expectations.

Compatibility keys are composed of 3 comma-delimited numbers - M,S,R - where:

back to top

Host Support

back to top

Dependencies

back to top

Device Support

This release supports the following devices:

  Device


28x F2801, F2806, F2808, F2810, F2811, F2812, F28232, F28234, F28235, F28332, F28334, F28335, F2802x, F2803x, F2834x

55x 5501, 5502, 5503, 5505, 5507, 5509A, DA255,  DA295, DA300, 5510, 5510A, 5561, DA255, DA295, DA300, OMAP1035, OMAP1510, OMAP1610, OMAP1710, OMAP5903, OMAP5905, OMAP5910, OMAP5912, OMAP5944, OMAP5946, OMAP5948, OMAP2320, OMAP2420, TNETV1050, TNETV1055
62x 6202, 6203, 6203B, 6204, 6205, 6211, 6211B
64x 6410, 6411, 6412, 6413, 6414, 6415, 6416, 6418, DM415, DM420, DM421, DM425, DM426, DM640, DM641, DM642, DRI300
64x+ 6421, 6424, 6428, 6452, 6454, 6455, 6474, DM6431, DM6433, DM6435, DM6437, DM6441, DM6443, DM6446, DM6467,  DM357, DM647, DM648, TCI6482,  DRA402, DRA404, DRA406,  DRA414, DRA416, DRA442, DRA444, DRA446, F761990, OMAP2420, OMAP2430, OMAP2431, OMAP2530, OMAP2531, OMAP3425, OMAP3430, OMAP3525,  OMAP3530, TCI6482, TCI6484, TCI6486, TCI6487, TCI6488, TCI6486,  TNETV2685

67x 6701, 6711, 6711 - 250, 6712, 6713, 6713 - 300
67x+ 6722, 6726, 6727, DA700, DA705, DA707, DA710

674xOMAPL137, OMAPL138, DA830, 6747, 6748

 
back to top

Validation Information

This release was built using the following components:

This release was validated using the following components:

back to top

Known Issues

The following issues are known to affect this release:

 Please check the following link for additional information when upgrading from 4.90 to 5.x -- Knowledge base with known 4.90 to 5.x upgrade issues  back to top

Benchmarks

back to top

Versioning

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. bios_5_33.

Subsequent releases of patch upgrades will be identified by the patch number, ex. BIOS 5.33.03 with directory bios_5_33_03. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top

Technical Support And Product Updates

back to top

Last updated: Apr 27, 2009