DSP/BIOS 5.32.01 Release Notes

This release note is divided into the following sections:

Introduction, Documentation, What's New, Upgrading And Compatibility Information, Host Support, Dependencies, Device Support, Validation Information, Known Issues, Benchmarks, Versioning, Technical Support And Product Updates,


Introduction

DSP/BIOS 5.32.01 is a patch release of DSP/BIOS 5.32.

Please read the Setup Guide for help installing and setting up your environment to use DSP/BIOS 5.32.01.

back to top

Documentation

The following documentation is provided with this release:

Additional release note documentation:

Release notes from previous releases are also available in the release notes archive directory.

back to top

What's New

5.32.01.05 Release (this release)

back to top

Upgrading And Compatibility Information

Solaris host is no longer supported in this release. Customer-critical bug fixes to earlier releases will be available to Solaris users if required.

DSP/BIOS 5.32 does not support TMS320C54xx devices. Users of such devices should continue use DSP/BIOS 5.31.xx earlier releases. For customer-critical 54xx-related issues, TI will continue to provide fixes to earlier versions when needed.

DSP/BIOS 5.32 no longer contains RTDX examples. DSP/BIOS 5.32 does continue to provide the RTDX libraries so existing applications using RTDX will continue to build and execute without any issues. To obtain RTDX examples, users should download the RTDX 2.0 release from:

https://www-a.ti.com/downloads/sds_support/targetcontent/index.html

Compatibility Key Definitions

Compatibility keys are intentionally independent of Marketing product numbers and are intended to:

  1. Enable tooling to identify incompatibilities between components, and
  2. Convey a level of compatibility between different releases to set end user expectations.

Compatibility keys are composed of 3 comma-delimited numbers - M,S,R - where:

back to top

Host Support

back to top

Dependencies

back to top

Device Support

This release supports the following devices:

  Device Runtime Model



28x F2801, F2806, F2808, F2810, F2811, F2812, F28335 Large model

55x 5501, 5502, 5503, 5507, 5509A, DA255,  DA295, DA300, 5510, 5510A, 5561, OMAP5903, OMAP5905, OMAP5910, OMAP5912, OMAP5944, OMAP5946, OMAP5948, OMAP1035, OMAP1510, OMAP1610, OMAP1710 (OMAP), OMAP2320, OMAP2420, TNETV1055 Large model on Laijin 2.x core devices
62x 6202, 6203, 6204, 6205, 6211 Big and Little Endian
64x 6410, 6411, 6412, 6413, 6414, 6415, 6416, 6418, DRI300,  DM420, DM640, DM641, DM642
Big and Little Endian
64x+ DM420, DM415, DM425, DM426, DM647, DM648, DM6431, DM6433, DM6435, DM6437, DM6443, DM6446, 6421, 6424, 6452, 6454, 6455, TCI6482, TCI6486, TCI6487, TCI6488, DRA442, DRA446, OMAP2430, OMAP3430, TNETV2685
Big and Little Endian

67x 6701, 6711, 6711 - 250, 6712, 6713, 6713 - 300
Big and Little Endian
67x+ 6727, DA705, DA707, DA710 Little Endian


 
back to top

Validation Information

This release was built using the following components:

This release was validated using the following components:

back to top

Known Issues

The following issues are known to affect this release:

 Please check the following link for additional information when upgrading from 4.90 to 5.x -- Knowledge base with known 4.90 to 5.x upgrade issues  back to top

Benchmarks

back to top

Versioning

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. bios_5_32.

Subsequent releases of patch upgrades will be identified by the patch number, ex. BIOS 5.32.01 with directory bios_5_32_01. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top

Technical Support And Product Updates

back to top

Last updated: Oct 31, 2007