![]() |
![]() |
This release note is divided into the following sections:
Introduction, Documentation, What's New, Upgrading And Compatibility Information, Host Support, Dependencies, Device Support, Validation Information, Known Issues, Benchmarks, Versioning, Technical Support And Product Updates,
DSP/BIOS 5.32.01 is a patch release of DSP/BIOS 5.32.
Please read the Setup Guide for help installing and setting up your environment to use DSP/BIOS 5.32.01.The following documentation is provided with this release:
Release notes from previous releases are also available in the release notes archive directory.
back to top5.32.01.05 Release (this release)
Solaris host is no longer supported in this release. Customer-critical bug fixes to earlier releases will be available to Solaris users if required.
DSP/BIOS 5.32 does not support TMS320C54xx devices. Users of such devices should continue use DSP/BIOS 5.31.xx earlier releases. For customer-critical 54xx-related issues, TI will continue to provide fixes to earlier versions when needed.
DSP/BIOS 5.32 no longer contains RTDX examples. DSP/BIOS 5.32 does continue to provide the RTDX libraries so existing applications using RTDX will continue to build and execute without any issues. To obtain RTDX examples, users should download the RTDX 2.0 release from:
https://www-a.ti.com/downloads/sds_support/targetcontent/index.html
Compatibility keys are intentionally independent of Marketing product
numbers and are intended to:
Compatibility keys are composed of 3 comma-delimited numbers - M,S,R -
where:
This release supports the following devices:
Device | Runtime Model | |
---|---|---|
28x | F2801, F2806, F2808, F2810, F2811, F2812, F28335 | Large model |
55x | 5501, 5502, 5503, 5507, 5509A, DA255, DA295, DA300, 5510, 5510A, 5561, OMAP5903, OMAP5905, OMAP5910, OMAP5912, OMAP5944, OMAP5946, OMAP5948, OMAP1035, OMAP1510, OMAP1610, OMAP1710 (OMAP), OMAP2320, OMAP2420, TNETV1055 | Large model on Laijin 2.x core devices |
62x | 6202, 6203, 6204, 6205, 6211 | Big and Little Endian |
64x | 6410, 6411, 6412, 6413, 6414, 6415, 6416, 6418, DRI300, DM420, DM640, DM641, DM642 |
Big and Little Endian |
64x+ |
DM420, DM415, DM425,
DM426, DM647, DM648, DM6431, DM6433, DM6435, DM6437, DM6443, DM6446,
6421, 6424, 6452, 6454, 6455, TCI6482, TCI6486, TCI6487, TCI6488,
DRA442, DRA446, OMAP2430, OMAP3430, TNETV2685 |
Big and Little Endian |
67x | 6701, 6711, 6711 - 250, 6712, 6713, 6713 - 300 |
Big and Little Endian |
67x+ | 6727, DA705, DA707, DA710 | Little Endian |
This release was built using the following components:
This release was validated using the following components:
Memory heap issue when updating existing configuration files -- Prior versions of the configuration tool allowed for an inconsistent memory heap configuration. The tool allowed users to enable heaps when no heaps were actually configured and the default for bios.MEM.MALLOCSEG and bios.MEM.SEGZERO were still set to 'MEM_NULL'. This was causing problems in applications since malloc() and MEM_alloc() were failing even when user thought they had configured BIOS for dynamic memory allocation. The configuration tool is now checking to make sure that configurations that have heaps also have bios.MEM.MALLOCSEG and bios.MEM.SEGZERO set to a valid heap. Update from existing projects might yield an error message. The work around is to either remove the 'bios.enableMemoryHeaps(prog);' line from your configuration, or to add a heap and set bios.MEM.MALLOCSEG and bios.MEM.SEGZERO accordingly. See the ti/bios/examples/common/evmDM6446_common.tci file (or others) for an example of how to do this.
BIOS RTA has problems reading data in stop mode for some 64x+ devices -- Currently, stop mode reads will only work for DaVinci. This is tracked by SDSCM00010400
DSP/BIOS examples that are using RTA halt when run every other time on
DSK5510/DSK5509A via XDS560. This is tracked by
SDSCM00005820.
CCS window closes on refreshing KOV Window when it receives illegal values -- KOV will crash if Module Objects have illegal values. For e.g if a dynamic task has a bad name, KOV will try to print the illegal name and crash. This is tracked by SDSCM00006694.
KOV window shows wrong names for dynamic objects -- This is tracked by SDSCM00007151.
KOV displays wrong names for memory sections -- This is tracked by SDSCM00004917.
Incorrect platform name in Tconf User's Guide in "Create New Platform" section -- The spru0007h.pdf document contains the correct instructions for creating a new platform using the Tconf's User's Guide, the help files were not updated to reflect the same naming convention. This is tracked by SDSCM00003471.
RTDX tutorial examples do not all execute as expected when run on TCI6482 simulator little endian -- This is tracked by SDSCM00010736.
RTDX Hot-Connect does not work for C64P -- This is tracked by SDSSCM00011954.
DSP/BIOS RTA Control Panel does not update values correctly when using comma decimal separator in Windows -- The RTA Control Panel does not work as expected when using Windows Regional Settings where ',' is used instead of '.' for the decimal separator. Only workaround is to use Regional Settings where '.' is the decimal separator, or use default 1 second update rate. This is tracked by SDSCM00017755.
HWI_isHwi() documentation has contradictory statement -- In previous versions of DSP/BIOS, " calling HWI_isHWI() from main() resulted in TRUE. This is no longer the case;" main() is identified as part of the TSK context. This is tracked by SDSCM00020436
Some of the help files in BIOS 5.32 refers to BIOS 5.31 -- This is tracked by SDSCM00020437
back to top
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. bios_5_32.
Subsequent releases of patch upgrades will be identified by the patch number, ex. BIOS 5.32.01 with directory bios_5_32_01. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
back to topLast updated: Oct 31, 2007