DLPC3478 Firmware v9.2.0 Release Notes
February 2, 2023
Table of Contents
Overview
These are the release notes for the following firmware image file:
- Firmware Version: 9.2.0
- Embedded Software Version: 9.2.0
- Generated from DLP Composer Version: 13.19.14
- Minimum GUI version: 3.2.0.7
- DMD: DLP3010LC
- Controller: DLPC3478
- PMIC: DLPA2005
Configuration Settings
- I2C Address: 0x36
- DMD Pin Mapping: 1
- Rlim value: 39mΩ
- Light Control Sequence Database Version: 0.7.1
Supported Features
- Light Control
- Internal Pattern Streaming Mode: - Trigger-In/Free-running modes (Mono 1 Bit/8 Bit, RGB 1 Bit/8 Bit, Vertical + Horizontal Pattern Generation, Pattern Invert)
- External Pattern Streaming Mode (Mono 1 Bit/8Bit, RGB 1 Bit/8Bit)
- Zero dark time external pattern display for illumination time less than 400 uSec
- Splash Patterns (Mono 1 Bit/ 8 Bit)
- Display
- External video input
- IntelliBright™ video processing algorithms
- Splash Screens
- Source frame rates supported - 0 to 123 HZ
- Four 2D looks (cool, medium, warm, and other) and one 3D look
- Supported pattern timings in Sequence Database v0.5.71:
- Internal Pattern Mode Timings:
| Pattern Type |
Exposure Time Range (us) |
Sequence Min Pre-Exposure Dark Time (us) |
Sequence Min Post-Exposure Dark Time (us) |
| 1-bit Monochrome |
200 - 399 |
171 |
31 |
| 400 - 799 |
171 |
31 |
| 800 - 1799 |
171 |
31 |
| 1800 - 3799 |
171 |
31 |
| 3800 - 7799 |
171 |
31 |
| 7800 - 15799 |
171 |
31 |
| 15800 - 31799 |
171 |
31 |
| 31800 - 63799 |
171 |
31 |
| 63799 - 127598 |
171 |
31 |
| 1-bit RGB |
600 - 1799 |
171 |
31 |
| 1800 - 3799 |
171 |
31 |
| 3800 - 7600 |
171 |
31 |
| 8-bit Monochrome |
| 1677 - 3351* |
171 |
31 |
| 3464 - 7126 |
171 |
31 |
| 7127 - 14505 |
171 |
31 |
| 14506 - 29012 |
171 |
31 |
8-bit RGB |
10912 - 21824 |
171 |
31 |
4-bit Monochrome |
| 585 - 1368 |
171 |
31 |
| 1369 - 2937 |
171 |
31 |
| 2938 - 5876 |
171 |
31 |
5-bit Monochrome |
| 693 - 1585 |
171 |
31 |
| 1586 - 3172 |
171 |
31 |
6-bit Monochrome |
| 887 - 1973 |
171 |
31 |
| 1974 - 3948 |
171 |
31 |
Notes:
*This is a special sequence that displays 7-bit patterns. The least significant bit of the 8-bit pattern data
- For internal patterns, there will be an additional variable delay of ~3000 us at the beginning of every pattern set.
- Exposure times shorter than the above values are not possible. Longer exposure times will operate with decreased timing accuracy and behavior is not guaranteed.
- Shorter dark times are not possible. Longer dark times can be used. The maximum possible dark times for a desired exposure time are:
- Tmax pre-exposure dark time = ( 27306us + tsequence min pre-exposure dark time ) * (Tdesired exposure / tsequence minimum exposure)
- Tmax post-exposure dark time = ( 27306us + tsequence min post-exposure dark time ) * (Tdesired exposure / tsequence minimum exposure)
- External Pattern Streaming Timings:
| Pattern Type |
Exposure Time Range (us) |
Sequence Min Pre-Exposure Dark Time (us) |
Sequence Min Post-Exposure Dark Time (us) |
| 1-bit Monochrome |
200 - 399 |
171 |
31 |
| 400 - 799 |
171 |
31 |
| 800 - 1799 |
171 |
31 |
| 1800 - 3799 |
171 |
31 |
| 3800 - 7600 |
171 |
31 |
| 1-bit RGB |
451 - 799 |
171 |
31 |
| 800 - 1799 |
171 |
31 |
| 1800 - 3799 |
171 |
31 |
| 3800 - 7600 |
171 |
31 |
| 8-bit Monochrome |
2555 - 5110 |
171 |
31 |
| 8-bit RGB |
10912 - 21824 |
171 |
31 |
Notes:
- Exposure times shorter than the above values are not possible. Longer exposure times will operate with decreased timing accuracy and behavior is not guaranteed.
- Shorter dark times are not possible. Longer dark times can be used. The maximum possible dark times for a desired exposure time are:
- Tmax pre-exposure dark time = ( 6553us + tsequence min pre-exposure dark time ) * (Tdesired exposure / tsequence minimum exposure)
- Tmax post-exposure dark time = ( 6553us + tsequence min post-exposure dark time ) * (Tdesired exposure / tsequence minimum exposure)
- Splash Pattern Mode Timings:
| Pattern Type |
Exposure Time Range (us) |
Sequence Min Pre-Exposure Dark Time (us) |
Sequence Min Post-Exposure Dark Time (us) |
| 8-bit Monochrome |
7737 - 17034 |
171 |
31 |
Notes:
- The maximum pattern period (pre-exposure + exposure + post-exposure) cannot exceed 2184us for 1-bit splash patterns and 17476us for 8-bit splash patterns.
- The listed minimum dark times are applicable for the minimum exposure time of each sequence. The dark times scale along with the exposure time as per the following equation:
- Tmin required pre-exposure dark time = tsequence min pre-exposure dark time * (Tdesired exposure / tsequence minimum exposure)
- Tmin required post-exposure dark time = tsequence min post-exposure dark time * (Tdesired exposure / tsequence minimum exposure)
- I2C command 0x9D (Read Validate Exposure Time) returns the minimum required pre-exposure and post-exposure dark times for a specific pattern type and given exposure time.
Updates in this release
- Firmware will support the systems with the Light Control DMDs (DLP2010LC, DLP3010LC) only.
- Feature additions :
- Issue related to internal patterns not displaying in the proper order are fixed, GUI v3.2.0.7 should be used
- Issue related to internal pattern RGB illumination not illuminating Red and Green are fixed
Known Limitations
- Internal Patterns 8 bit RGB sequence - post dark time does not match specified value.
- Non uniformity is seen at the display borders while running 1 bit internal patterns with 0 pre,post exposure times.
- External Streaming - Signals/Patterns Incorrect in case of VSYNC jitter.
- When switching from internal pattern mode to splash pattern mode make sure that the internal pattern display is stopped.
- While using the update firmware feature of GUI, make sure that size of splash image are as small as possible and prefer selecting RGB color space if the images are of PNG format.
- LC splash pattern dispaly is only supported in RGB format.
- Only RGB888 input source format supported in External Pattern Streaming Mode.
- 3D glasses not locking to 3D source
- Internal Pattern control pause/step buttons meant for debuggin only due to potential for image artifacts to be seen
- Unsupported Features:
- DSI/BT656 Input
- CPU Interface
- LABB with Ambient Light Sensor support
- Shallow Gradient
- White Point Correction
- I2C at 400KHz
- Flashless configuration
- Idle mode
- Power management, clock gating and scaling
- CAIC is not supported in LC, system will not boot up in LC mode with CAIC enabled
Technical Support and Product Updates
Thermistor Processing Documentation
- Using System Temperature via I2C commands:
- Read System Temperature (0xd6)
- Note: The temperature of the thermistor is read in degrees Celsius in a magnitude of 10 times the reading of thermistor. Bit 11 (the most significant bit) denotes the sign temperature. A '0' means a positive temperature, while '1' denotes a negative temperature.
- Example #1: b(11:0) = 000110101010; 426d / 10d = 42.6degC
- Example #2: b(11:0) = 100110101010; 426d / 10d = -42.6degC
- Note: This temperature reading will need to be calibrated per the design and specific thermsitor chosen of custom boards. Offset to determine the true temperature of the thermistor reading. Texas Instruments DLP hardware uses Murata's NCP15WF104F03RC.
Additional Links