| ID |
Summary |
State |
Reported In Release |
Target Release |
Workaround |
Release Notes |
| CODEGEN-3597 |
ELF header field e_phoff should be 0 when no program header is present |
Fixed |
ARM_17.6.0.STS |
ARM_17.9.0.STS |
|
ELF header field e_phoff should be 0 when no program header is present, and ELF header field e_shoff should be 0 when no section headers are present. |
| CODEGEN-2372 |
C2000 hex utility emits spurious warning about creating an extra output file |
Fixed |
ARM_17.6.0.STS |
ARM_17.9.0.STS |
Ignore the warning or suppress it with option --diag_suppress=21117. |
The Hex utility sometimes emits spurious warnings about writing data to auto-generated files. |
| CODEGEN-2371 |
Compiler library automatic build with mklib fails |
Fixed |
ARM_17.6.0.STS |
ARM_17.9.0.STS |
Add quotes around argument to offending 'echo' command in lib/src/Makefile of the tool's installation. |
|
| CODEGEN-2286 |
palign(8) of .init_array messes up __TI_INITARRAY_Limit address |
Fixed |
ARM_17.9.0.STS |
ARM_17.9.0.STS |
In the linker command file, replace
.init_array > FLASH, palign(8), fill = 0xffffffff
with the following GROUP statement:
GROUP
{
.init_array
} > FLASH, palign(8)
The palign(8) on GROUP will ensure that any required padding is added after .init_array. However, both the size of .init_array and the value of __TI_INITARRAY_Limit remain unchanged. |
Applying palign(8) to .init_array caused __TI_INIT_ARRAY_Limit to be set to the end of .init_array including the padding. This broke RTS startup code responsible for calling constructors because the table of constructors now includes invalid data. This bug has been fixed and __TI_INIT_ARRAY_Limit is no longer affected by padding. |
| CODEGEN-2209 |
Link error with gcc debug information |
Fixed |
ARM_17.3.0.STS |
ARM_17.6.0.STS |
None |
When linking against GCC code, a project failed to build due to a relocation error, generating the message "fatal error #10232". Specifically, the problem was caused by debug information left in the GCC object file for eliminated comdat sections. GCC puts debug information into a common section called .debug_info. Once the comdat section was eliminated, the debug symbol pointed to a deleted section, causing an error in the TI linker. |
| CODEGEN-2123 |
Compiler manuals incorrectly document option --gen_preprocessor_listing as --gen_parser_listing |
Fixed |
ARM_17.3.0.STS |
ARM_17.3.0.STS |
|
The correct name of the compiler option is --gen_preprocessor_listing. |
| CODEGEN-2119 |
Stack usage assistant call graph misses callee relationship for some direct calls |
Fixed |
ARM_17.6.0.STS |
ARM_17.6.0.STS |
|
The Object File Display utility failed to detect function callees when generating call graph information for functions that contain nested blocks. |
| CODEGEN-2113 |
Hex utility mishandles space in directory name of output file |
Fixed |
ARM_17.6.0.STS |
ARM_17.6.0.STS |
Use directory names without spaces for output files. |
The hex utility did not correctly handle spaces in output directory and file names. |
| CODEGEN-2098 |
Temp filename collisions on Windows with many parallel invocations |
Fixed |
ARM_17.3.0.STS |
ARM_17.6.0.STS |
|
In some cases with a large number of compilations in parallel on Windows, the compiler could create temporary files with colliding names, resulting in strange compilation failures. |
| CODEGEN-2065 |
Compiler documentation implies --check_misra compiler option not needed if pragma used |
Fixed |
ARM_17.3.0.STS |
ARM_17.3.0.STS |
|
The --check_misra compiler option is required to enable MISRA checking even if the CHECK_MISRA pragma is used. |
| CODEGEN-2060 |
Even though option --buffer_diagnostics is not used, compiler issues diagnostic that says it is deprecated |
Fixed |
|
ARM_17.3.0.STS |
None |
The --buffer_diagnostics compiler option was deprecated as of MCU compilers v16.6.0.STS because this setting became the default behavior for the compiler. However, the option was passed to the linker and the linker issued a remark stating the option was deprecated. |
| CODEGEN-2053 |
Compiler incorrectly reorders struct assign for small, volatile structs with bit-fields |
Fixed |
|
ARM_17.3.0.STS |
Use optimization level 0 or off (option --opt_level) |
For a very specific optimization, the optimizer may drop a volatile qualifier from a struct assignment. In some cases, the compiler may later perform an incorrect optimization, most commonly incorrectly reordering volatile assignments.
This bug can only happen in a function compiled with optimization level 1 or higher which contains both of the following: 1) A struct assign where the destination is volatile, and the source is a known constant, and the struct contains a bit-field, and the struct is of size "int" or smaller. 2) Any bit-field access (read or write) other than as part of a struct assign or initialization expression. That is, the name of the bit-field is present in the access expression. Note that the optimizer can create this situation by inlining functions, so 1 and 2 might be in different functions in the source code.
Consider a tree x = y where x and y are of type struct S. If the value of y is known at compile time (e.g. a const value), the optimizer will try to turn the struct constant into an integer constant (possibly combining bit-fields) and rewrite the tree to look like this: "(unsigned *)x = 32;" However, if y is volatile, that should be "*(volatile unsigned *)x = 32;" Because the access is not volatile, instruction scheduling could cause this instruction to drift past nearby volatile accesses. |
| CODEGEN-2050 |
Use of -o4 causes linker XML map file to have missing input_file entries |
Fixed |
|
ARM_17.3.0.STS |
|
|
| CODEGEN-2047 |
CMSIS Core v5 is not compliant with TI ARM Compiler |
Fixed |
|
ARM_17.3.0.STS |
The __INLINE macro in the TI compiler RTS linkage.h is no longer used and can be removed. |
CMSIS v5 defines the macro __INLINE, which interferes with the TI compiler RTS definition of the same macro in linkage.h. |
| CODEGEN-1976 |
Value of __cplusplus is wrong |
Fixed |
|
ARM_17.3.0.STS |
If possible, use the -ps or --strict_ansi options. This mode will use the strict definition of __cplusplus, which is 199711L. |
Our parser mimicked G++ behavior for the value of this macro in relaxed ANSI mode. This reproduced a bug in G++ versions v.4.7 and v.4.3 that has since been fixed. |
| CODEGEN-1705 |
Compiler documentation and RTS disagree on function names _TI_start_pprof_collection and _TI_stop_pprof_collection |
Fixed |
|
ARM_16.12.0.STS |
|
|
| CODEGEN-1656 |
Using --gen_profile_info does not work with -o4 |
Fixed |
ARM_17.6.0.STS |
ARM_17.6.0.STS |
Lower the optimization level to -o3. |
Previously, link time optimization failed when profiling options --gen_profile_info and use_profile_info were specified in combination with the --opt_level=4 option. The errors were because profiling options were not supported when used in combination with --opt_level=4.
Application profiling during whole program optimization is now supported. Profiling options --gen_profile_info and --use_profile_info may now be combined with --opt_level=4. |
| SDSCM00052878 |
Documentation error: #pragma pack should be lower case |
Fixed |
|
ARM_16.12.0.STS |
|
|