| CODEGEN-2259 |
Multi-statement macro with statement before declaration does not compile |
Accepted |
ARM_17.6.0.STS |
|
I believe this is known issue CODEGEN-1979. If your source code has a statement (";") before a declaration ("int retVal = getVal();"), and the declaration does not have white space in front of it, the parser will emit an incorrect error ("error: expected a "}""). When you put code like that into the preprocessor, it strips all whitespace, so even though there actually is a space in the macro, there is no space when the parser gets to work. You'll need to rearrange your macro so that there are no statements before any of the declarations. |
|
| CODEGEN-2238 |
Compiler incorrectly emits MISRA 10.1 for function argument |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00052872 |
#pragma LOCATION and palign do not work together |
Open |
ARM_17.6.0.STS |
|
One workaround is to use specific placement in the linker command file. In the C code, replace the #pragma LOCATION with a #pragma DATA_SECTION ...
#pragma DATA_SECTION(device_fw_info_ptr, "for_device");
And in the linker command file, replace the whole .TI.bound line with this ...
for_device > 0x00018000, palign(8), fill = 0xffffffff
|
|
| SDSCM00052868 |
Automatic library build fails when an exact library name is used |
Open |
ARM_17.6.0.STS |
|
Don't specify the name of the library. |
|
| SDSCM00052849 |
Compiler and assembler disagree on format for IT instruction |
Open |
ARM_17.6.0.STS |
|
|
|
| SDSCM00052780 |
The armhex command does not handle spaces in the name of the output binary |
Open |
ARM_17.6.0.STS |
|
|
|
| CODEGEN-1458 |
Consider splitting up unified_locale.cpp to save code space |
Open |
ARM_17.6.0.STS |
|
|
|
| CODEGEN-1445 |
Compiler inserts unnecessary register copy |
Open |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051660 |
When the imaginary part of z is INFINITY, cprojf(z) is NOT equivalent to INFINITY + I * copysign(0.0, cimagf(z)) |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051484 |
Compiler does not respect partial overrides in C99 designated initializers |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051367 |
Disable diagnostic 1558 (--float_operations_allowed diagnostic) in standard header files |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051353 |
MISRA does not recognize #pragma as preprocessing directive for 19.1 |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051165 |
Should accept "LDRD R8,[R1]" in Thumb-2 mode |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051114 |
Missing half-precision float conversion functions |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051113 |
Missing __aeabi_read_tp |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051111 |
Missing AEABI_COMPATIBILITY_MODE link-time constants |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051086 |
Assembler accepts but mistranslates BLLT in v7 thumb mode |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00051069 |
Should allow "ADD R0, R1, #0xfff" for v6m0 |
Accepted |
ARM_17.6.0.STS |
|
Use the syntax "ADDW R0, R1, #0xfff" instead. |
|
| SDSCM00051065 |
Should accept 2-operand SUB SP in Thumb1/UAL mode |
Accepted |
ARM_17.6.0.STS |
|
Use ADD SP, SP, # instead
|
|
| SDSCM00050861 |
Should accept 2-operand add in ARM mode |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00050499 |
The .label assembler directive should not be accepted when assembling for ELF. |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00050131 |
Local struct with non-constant initializer treated as static scope variable |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00049911 |
__aeabi_dcmpun returns 1 for Inf and -Inf |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00049284 |
Compiler misreports Misra warning 10.1 |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00049280 |
Ill advised enum scalar usage gets MISRA diagnostic, but similar usage of enum array does not |
Open |
ARM_17.6.0.STS |
|
|
|
| SDSCM00049278 |
Array that is correctly initialized erroneously gets a MISRA diagnostic about size not being specified |
Open |
ARM_17.6.0.STS |
|
|
|
| SDSCM00048267 |
Warning generated when using __curpc intrinsic on Thumb 2 |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00047902 |
Predefined macro __TI_FPv4SPD16_SUPPORT__ should be __TI_FPV4SPD16_SUPPORT__ |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00047077 |
Incorrectly reduced double constant to float when ultimate destination is short |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00046352 |
Disassembler does not emit certain instructions in UAL form by default |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00046102 |
MISRA 12.8 and MISRA 10.5 false positives |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00046074 |
Cortex-M0 library lacks uread4, etc. |
Open |
ARM_17.6.0.STS |
|
If using the TI compiler, the TI compiler doesn't call any of these functions, so no workaround should be necessary.
If using any other vendor's compiler and linking with the TI toolchain, link with the other vendor's toolchain. |
|
| SDSCM00044038 |
float library functions misbehave with --abi=eabi -mv5e -me --float_support=fpalib |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00044035 |
float library functions misbehave with -me --float_support=fpalib |
Accepted |
ARM_17.6.0.STS |
|
Use --float_support=vfplib instead. |
|
| SDSCM00042945 |
-pdse=195 causes an error under EABI if any standard header file is included |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00040934 |
Structure is not initialized correctly when using -o2 or -o3 optimization |
Accepted |
ARM_17.6.0.STS |
|
The initialization will have to be done at run-time, through a __sti initialization routine. You can see this routine when compiling without optimization. To workaround the compiler removing this initialization routine, initialize the object at the beginning of main:
Info2.mSize = ((unsigned)_end_isr_stack - (unsigned)_start_isr_stack);
|
|
| SDSCM00040523 |
The _ssat16 intrinsic allows literals in the range of 0-31, but the SSAT16 instruction only accepts values from 1-16 |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00040522 |
_ssatl intrinsic allows 3rd argument to be 0 resulting in an assembler error. |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00039636 |
When creating a partial linked ELF object file, the linker uses virtual addresses instead of relative addresses. |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00039626 |
ARM assembler does not issue a warning for PC-relative loads when --embedded_constants=off |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00039220 |
Assembler does not accept the SP operand of the SRSDB instruction |
Accepted |
ARM_17.6.0.STS |
|
Omit the SP! operand and the instruction should assemble correctly. |
|
| SDSCM00038278 |
ARM floating point conversion routines do not support NaN |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00037227 |
ARM disassembler error for VMRS instruction |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00037086 |
ARM assembler allows incorrect VFP registers for some instructions on D16 VFP architectures |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00037008 |
Linker outputting wrong build attribute name for EABI TAG_VFP_arch on ARM targets |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00036874 |
Section relative ELF symbol values in partially linking object files should hold the section offset for the symbol |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00036773 |
LDM/STM -DA/FA/IB/ED viariant instructions erroneously accepted by assembler for Cortex-M3 |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00036770 |
LDREXD and STREXD instructions erroneously generate errors on Cortex A8 and R4 |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00018691 |
Linker gives misleading warning when dot expressions used in SECTION directive for .stack section |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00014430 |
calloc doesn't check arguments to make sure the requested size is reasonable |
Accepted |
ARM_17.6.0.STS |
|
|
|
| SDSCM00008685 |
DWARF does not correctly represent variables stored in register pairs |
Accepted |
ARM_17.6.0.STS |
|
Although 'var1' and 'var2' are shown to be in single registers, a
debugger could determine that they are actually stored in register
pairs by looking at the type of the variables:
[00000113] DW_TAG_base_type
DW_AT_name long long
DW_AT_encoding 0x5
DW_AT_byte_size 0x8
The base type indicates that the size of the variables is 0x8 bytes.
Since a single register can only store 0x4 bytes of information, it
would take two registers to hold this values.
On TI architectures, values stored in multiple registers are always
stored in consecutive registers. Thus, the debugger would know that
if the entire value could not fit in A4, the rest of the value must be
in A5. A5 would contain the upper 32 bits of the value.
|
|
| SDSCM00008543 |
Forward reference in .space generates an internal error |
Accepted |
ARM_17.6.0.STS |
|
none
|
|
| SDSCM00008465 |
Language Conformance: crash because of void pointer dereference |
Accepted |
ARM_17.6.0.STS |
|
Please describe the workaround for this problem.
|
|
| SDSCM00008248 |
Compilers on PC will not work without TMP set |
Accepted |
ARM_17.6.0.STS |
|
Set the TMP environment variable, even if just set to . (current directory)
|
|