| ID |
Summary |
State |
Reported In Release |
Target Release |
Workaround |
Release Notes |
| CODEGEN-5387 |
Loop with early exit may peel incorrectly when unrolling (as with -mf3 or above) |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.10.LTS |
Add "#pragma UNROLL(1)" to the affected loop to inhibit unrolling, or compile with --opt_for_speed=2 or lower which inhibits unrolling of all loops. |
The compiler may unroll loops to speed them up. If it doesn't know the exact trip count, it needs to "peel" some iterations to make sure it does the extras if they don't fit exactly into the unrolled loop.
If the loop has an early exit -- in this case, it looks roughly like
while (flen-- && isdigit(*s)) ...
-- then there's a problem, because when the unrolled loop finishes, it could be because it's done, or it could be because isdigit(*s) returned false. If the unrolled part is done, we need to do the peeled part, but if isdigit() returned false, we don't, and the logic isn't ready for that conundrum and does the wrong thing. |
| CODEGEN-5236 |
Register allocation failure |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.9.LTS |
No practical workaround |
The compiler may, in rare cases, allocate registers incorrectly. The most common symptom would be an internal error indicating that register allocation has failed. This problem has only been observed on C28x compiler version 8.1.3.LTS, but could occur for other ISAs. |
| CODEGEN-5127 |
Linker fails with INTERNAL ERROR: no match for COMMA |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.10.LTS |
Compile with --opt_level=3, or ensure that all constituent files are either compiled with --neon or without --neon. |
Combining object files compiled with --neon and without --neon in a --opt_level=4 final compilation, even if they're all compiled with -mv7a8, can cause a compiler abort. |
| CODEGEN-5032 |
Loop over array, preceded by shuffle of the array using scalar temp repeatedly, may produce incorrect results |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.10.LTS |
The test case uses the same temp, nTemp, repeatedly in the shuffle function. Using different temps for each assignment will avoid the problem. Using "#pragma UNROLL(1)" to inhibit unrolling of the affected loops may also avoid the problem. |
The problem case looks something like
x = a[0]
a[1] = x
x = a[2]
a[3] = x
for (i = 0; i < N; i++) {
a[i] = ...
... a[i] ...
}
It shuffles data in an array a[] using the scalar x, then loops over array a[]. This particular arrangement, with the right optimisations, will do the wrong thing with the shuffle code. The wrong thing is part of optimising the loop, so both parts are required for there to be a problem. A workaround is to use a separate scalar variable for each assignment in the shuffle, ie, "x1 = a[0]; a[1] = x1" and "x2 = a[2]; a[3] = x2". |
| CODEGEN-4912 |
Including stddef.h may disable MISRA diagnostics |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.9.LTS |
Add "#pragma diag_pop" after the inclusion of these files. SInce they're sometimes included from other system include files, it may take some digging to realise that this is necessary. |
Two include files -- stddef.h and string.h -- each lacked one diag_pop pragma to match the diag_push pragma, which meant that including those files would inadvertently disable certain MISRA warnings. |
| CODEGEN-4885 |
See MISRA diagnostics when compiling stdio.h |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.10.LTS |
none |
A program that includes <stdio.h> and checks for MISRA warnings may see some from stdio.h itself, which should not happen. |
| CODEGEN-4700 |
Incorrect diagnostic when using macro that comes from macro library |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.10.LTS |
Unpack all of the macro libraries and re-pack them into a single unified library, or rename all macros to names with less than 15 characters |
If you are using assembler macro libraries, and you have more than one library, and two or more of those libraries have macros with names that are longer than 15 characters, you may get an incorrect error message from the assembler saying "Bad archive entry" |
| CODEGEN-4678 |
Incorrect error due to typedef of very large object |
Fixed |
ARM_16.9.7.LTS |
ARM_16.9.8.LTS |
As a workaround, remove the typedef. Where the typedef was used, instead use the type the typedef refers to. |
The TI compiler infrastructure is incapable of handling user-declared objects above a certain size, because it mistakenly truncates the size of very large objects. Formerly, this resulted in quiet corruption, which was defect CODEGEN-449. Now that CODEGEN-449 is fixed, the compiler will emit an error if the user attempts to create a type larger than the tool can handle. However, this error check is not quite right for typedefs. A typedef for a very large object that is still within the compiler's limit may cause the parser to mistakenly emit an error that the object is greater than the maximum supported size. |
| CODEGEN-4668 |
Macro with temp label causes assembler to crash |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.9.LTS |
The problem will not occur without macro labels. If labels are required, no workaround is known. |
The assembler may crash or report a memory misuse when using an assembly macro containing a label, if the label appears in an instruction in a position that requires extra lookahead to parse.
The original example is a register name followed by a comma and a label use; for that assembler, the thing following the comma might be a shift specifier, so it requires expanding the macro label. That extra step frees some memory that it shouldn't, causing the problem. |
| CODEGEN-4655 |
DWARF type incorrect for char function formal parameter |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.8.LTS |
|
The compiler does not emit the correct type for function formal parameters that have integer type smaller than int. This only matters when trying to inspect the formal parameters before the prolog has executed. |
| CODEGEN-4638 |
When shift counts are higher than 32, compiler sometimes optimizes to an incorrect shift count |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.8.LTS |
Turn off optimization by using optimization level off.
Otherwise, avoid a left-shift by a constant as an operand of the listed operations. However, compiler optimizations could interfere with this. Try keeping the shift count in a global variable instead of as a literal, or computing the shift separately into a variable (a global or volatile local) and doing the |, +, etc, on the variable. |
Left shifts by 32 or more, as an operand of +, -, &, |, or ^, (eg, ((X<<56) | (Y<<48))) may produce incorrect results. |
| CODEGEN-4634 |
Use of stdarg.h va_start macro causes a write to the wrong local variable |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.9.LTS |
The test case for codegen-4634 has both a va_list declaration and a use of va_start. If the two are placed together, by moving the va_list declaration into the scope with the va_start, the problem does not occur.
The general workaround is to ensure an expression appears before the first nested scope. Exactly how to do that will depend on the situation. |
A function with a nested scope that declares local variables and appears before any expressions in the function, and also declares top-level locals after that, may mishandle the local variables in a way that acts as though some share a location though they're supposed to be distinct. I.e.,
int test(int arg, ...)
{
{ int a = 0; }
int b;
may mishandle a, b, arg, or any extra arguments.
Known cases all involve the ellipsis (...) parameter, but it is not known if that is also a necessary prerequisite. |
| CODEGEN-4623 |
Compiler incorrectly optimizes away member functions which arise from explicit template instantiation |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.10.LTS |
Compiling at -o2 helps, but sacrifices some optimisation. Adding a FUNC_CANNOT_INLINE pragma may also help, if it isn't an automatically-defined function. |
Compiling at -o3 may not retain external symbols for functions that are completely inlined within the file but which are declared extern, when using versions of the compiler from before 2017 -- ie, C6000 8.2.x, C2000/MSP430/TMS470 16.9.x. |
| CODEGEN-4605 |
Incompatible redeclaration error with -o4 when using anonymous unions |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.8.LTS |
Do not use anonymous structs or unions; give all struct members a name, even if it is never used. |
Anonymous structs and unions are a GCC extension. They are members of a parent structure and have no names. You access the elements inside them as if they were direct members of the parent class. If you have an anonymous struct or union inside a union and you use -O4 optimization, you may get the mistaken error "symbol so-and-so redeclared with incompatible type" at link time. This bug can only happen in COFF mode.
Essentially the same bug was previously fixed for EABI and was known as CODEGEN-1191. |
| CODEGEN-4600 |
Warning when using pragma RETAIN with attribute((noinit)) |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.9.LTS |
|
When using pragma RETAIN with attribute((noinit)) on the same symbol for an EABI target, a .clink directive is erroneously emitted in the assembly file, leading to a warning that the .CLINK directive is being ignored because the symbol already has .RETAIN specified. |
| CODEGEN-4525 |
Unreachable code in linear assembly may lead to crash |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.9.LTS |
Remove the unreachable code before compiling, or compile with -o1, -o0, or -ooff, or use --symdebug:none which happens to avoid the problem. |
The compiler may crash if given a linear assembly file containing some code that has a label but is not reachable. It's theoretically possible to create the same problem with C/C++ code, but we haven't been able to do it and the risk is quite small. |
| CODEGEN-4419 |
Compiler erroneously speculates indexed load from the stack |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.8.LTS |
Modify the source code of the offending function to make local variables "volatile." There's no obvious way to pre-determine that a function will suffer from this bug; you just have to wait for the bug to happen, look at the line number of the offending instruction (which will always be a load with indexed addressing with base register SP), and go to the function at that line number. Make every local variable in that function "volatile." If it's a C++ function, you may need to make the function "volatile." |
The compiler moves instructions from one block to another to increase parallelism. Usually this is done by predicating (adding a condition to) every instruction that is moved above a branch. However, in some cases, the compiler will "speculate" the instruction, which means removing the condition entirely. This is done when the instruction's side-effects are judged to be safe, such as load of a local variable. In the case that the instruction's condition would have been false, this load will be useless, but at least it will be safe, because the stack pointer (SP) is at a legal location, and there won't be a memory fault. However, when a local variable's value is read with an indexed expression, the index register is not necessarily speculated exactly when the load is, so the index register may have a garbage value. In this test case, the load was speculated, but the index register definition wasn't, so in the false branch, the computed address was garbage, and we would read a random memory address, causing a memory fault. (Even though SP was perfectly valid, the index register was garbage, so SP+index might point anywhere in memory.) |
| CODEGEN-4407 |
Not using const causes unexpected build error when calling std::sort |
Fixed |
|
ARM_16.9.8.LTS |
Remove unnecessary const from helper in s__algo.c |
|
| CODEGEN-4280 |
Using ULP advisor with C++ templates may cause the compiler to crash |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
|
The compiler may crash when using ULP advisor on C++ code that contains templates |
| CODEGEN-4182 |
Should ignore option --pending_instantiations when compiling C files |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.8.LTS |
If the user wishes to use the option --pending_instantiations, they must add this option individually to each C++ file. |
The compiler option --pending_instantiations only makes any sense when used with C++ code. It cannot have any effect on C code. Indeed, when passed as an option to a compilation of C code, the compiler will stop and emit an error, "pending instantiations option can be used only when compiling C++"
This is troublesome when trying to compile a mixture of C and C++ files in CCS. If the user wishes to use the option --pending_instantiations, they cannot just add this option to the global compiler options list; they must add this option individually to each C++ file. |
| CODEGEN-4113 |
Assembler computes wrong result for expression 0x232800 % 0x10000 |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
In some instances, as in the original test case, the AND operator can be used instead, but that is not a general workaround. |
The modulo operator in the TI assembler, for releases made in mid-to-late 2016 and all of 2017, is unreliable. In some cases it will produce an incorrect answer. |
| CODEGEN-4078 |
LInker takes over 5 minutes to finish |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
None. If the linker command file wants to be that specific about memory ranges, then the work has to be done, and the option to disable the work has its own bug. |
Linking may take excessively long when the linker command file specifically places a lot of variables at specific addresses, especially for C2000. The original report was placing more than 300 variables. The --no_placement_optimization option is not a workaround because it causes a linker crash. Both problems are fixed together. |
| CODEGEN-3931 |
Compiler crashes while handling 0 length array in zero sized struct |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.8.LTS |
None |
The compiler crashes while parsing a struct or class with zero-sized members in C++ mode. |
| CODEGEN-3923 |
DWARF CFI information lost due to microoptimizations |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.8.LTS |
No practical workaround. |
Some optimizations in the compiler would change instructions but fail to retain debugging directives attached to those instructions. This could impact the accuracy of the DWARF debugging information in various ways. |
| CODEGEN-3880 |
Compiler generates invalid instruction with VFP registers |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
No practical workaround |
When using --float_support, it is sometimes possible for VFP registers to show up in regshift operands. If you do not get an error from the assembler, you are not suffering from this bug. |
| CODEGEN-3876 |
Code incorrectly removed from functions calling "naked" attribute functions |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
|
The compiler supports the GCC attribute "naked," which means that a function shall not have prolog or epilog code. The idea is that this makes a blank function that the user may fill with assembly code.
The compiler also keeps track of the register usage behavior of previous functions in the same module, so that it can do some small optimizations like allocate caller-saved registers or eliminate unused code.
In this case, the compiler mistakenly assumed that a naked function did not use its input. The truth is that naked functions are essentially hand-coded assembly functions; while the compiler can assume they obey the C calling convention, the compiler can't know register behavior because it cannot parse the assembly instructions. |
| CODEGEN-3858 |
OFD gets DIE attribute offset wrong when using --dwarf_display=none,dinfo |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
If you use --dwarf_display=none,dinfo, use --dwarf_display=none,dinfo,types instead |
You can use OFD to display the DWARF debugging information in your object files by using the option '--dwarf' (or -g). You can narrow the categories of DWARF information displayed by using the '--dwarf_display' option. If you use the option --dwarf_display=none,dinfo you will see the DWARF DIE objects in the .dwarf_info section, but you will not see any DW_AT_type attributes unless you also use the "types" flag. This is not a bug. However, when OFD skips a DW_AT_type attribute, it displays the offset of the skipped DW_AT_type for the next attribute instead of the next attribute's correct offset. |
| CODEGEN-3801 |
Linker crashes with INTERNAL ERROR (unhandled exception) |
Fixed |
ARM_16.9.4.LTS |
ARM_16.9.6.LTS |
|
The linker experiences a segmentation fault when there is a reference from a debug section to a symbol without a section (for example, an absolute symbol). |
| CODEGEN-3794 |
False warning for MISRA 10.1/10.2 when commutative binary operands swapped |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
|
In certain cases, the compiler could emit an unwarranted MISRA diagnostic about type conversion. This would occur when using a commutative binary arithmetic operator with mixed operand types. The compiler mistakenly compared one operand's type to the other type. It should have compared each type to the promoted type of the operation. |
| CODEGEN-3711 |
Uses of __strex intrinsics are deleted |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
The compiler supports synchronization primitive intrinsics, but always deletes calls to __strex, __strexb, __strexh, and __strexd.
|
| CODEGEN-3650 |
Linker crashes when printing module list to map file |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
Add linker option --mapfile_contents=all,nomodules |
When creating a linker map file, and a summary of modules is written to the linker map file, and the entry point is undefined, the linker may crash. |
| CODEGEN-3619 |
pragma triggers false MISRA-C:2004 19.1/A warning |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
N/A |
Certain pragmas appearing prior to #include statements, such as #pragma RESET_MISRA, would cause MISRA warning 19.1/A to be issued:
MISRA-C:2004 19.1/A: #include statements in a file should only be preceded by other preprocessor directives or comments |
| CODEGEN-3617 |
gmtime incorrect when invoked in timezones east of GMT |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
Set the timezone to 0 (UTC) until the fix is in place |
|
| CODEGEN-3597 |
ELF header field e_phoff should be 0 when no program header is present |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
ELF header field e_phoff should be 0 when no program header is present, and ELF header field e_shoff should be 0 when no section headers are present. |
| CODEGEN-3595 |
Stack usage under reports stack amount used because it fails to handle function aliases |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.8.LTS |
|
CCS Stack Assistant did not accurately track aliased functions-- functions whose definitions are represented by a different symbol name. Now, the alias function will be used to determine stack size correctly, and the aliased function call name will be replaced with its alias. Currently, the Stack Assistant GUI is not capable of showing both the aliased and alias function names for calls to aliased functions-- this will require a future update. |
| CODEGEN-3591 |
When using fill value, linker may crash or hang |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
Upgrade to 17.6.0.STS or higher |
When using a fill value on a memory range, the linker may get into a corrupted state and either crash or enter an infinite loop. |
| CODEGEN-2373 |
Internal linker error triggered by function alias |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
Linker sometimes generates "Assertion failed" message and aborts. |
| CODEGEN-2320 |
ARM compiler fails to truncate scaled offset to byte |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
Compile with --opt_level=off. This is not an optimization bug; however, the bug does not manifest at --opt_level=off. |
The compiler matches X[(unsigned char)(Y >> 16)] with an indexed addressing mode, but it can't because that doesn't truncate the array index to 8 bits.
|
| CODEGEN-2286 |
palign(8) of .init_array messes up __TI_INITARRAY_Limit address |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.4.LTS |
In the linker command file, replace
.init_array > FLASH, palign(8), fill = 0xffffffff
with the following GROUP statement:
GROUP
{
.init_array
} > FLASH, palign(8)
The palign(8) on GROUP will ensure that any required padding is added after .init_array. However, both the size of .init_array and the value of __TI_INITARRAY_Limit remain unchanged. |
Applying palign(8) to .init_array caused __TI_INIT_ARRAY_Limit to be set to the end of .init_array including the padding. This broke RTS startup code responsible for calling constructors because the table of constructors now includes invalid data. This bug has been fixed and __TI_INIT_ARRAY_Limit is no longer affected by padding. |
| CODEGEN-2257 |
Using --no_stm may discard regsave debugging information |
Fixed |
|
ARM_16.9.6.LTS |
Don't use --no_stm unless you are sure it is necessary |
When using the --no_stm silicon workaround option for Cortex-R4, some debugging information may be lost, leading to the debugger having trouble unwinding functions, and thus being unable to show the call stack. |
| CODEGEN-2238 |
Compiler incorrectly emits MISRA 10.1 for function argument |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
|
| CODEGEN-2214 |
Compiler optimizes away function which calls assert |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.4.LTS |
Make sure there is some other visible effect in the function -- a call, a use of a volatile variable, something like that. |
A function whose only visible effect is to call assert() may be optimised away at --opt_level=0 or higher. |
| CODEGEN-2209 |
Link error with gcc debug information |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.4.LTS |
None |
When linking against GCC code, a project failed to build due to a relocation error, generating the message "fatal error #10232". Specifically, the problem was caused by debug information left in the GCC object file for eliminated comdat sections. GCC puts debug information into a common section called .debug_info. Once the comdat section was eliminated, the debug symbol pointed to a deleted section, causing an error in the TI linker. |
| CODEGEN-2143 |
Anonymous struct in union causes type merging failure at -O4 |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.4.LTS |
Do not use anonymous structs or unions; give all struct members a name, even if it is never used. |
Anonymous structs and unions are a GCC extension. They are members of a parent structure and have no names. You access the elements inside them as if they were direct members of the parent class. If you have an anonymous struct or union inside a union and you use -O4 optimization, you may get the mistaken error "symbol so-and-so redeclared with incompatible type" at link time. |
| CODEGEN-2119 |
Stack usage assistant call graph misses callee relationship for some direct calls |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.3.LTS |
|
The Object File Display utility failed to detect function callees when generating call graph information for functions that contain nested blocks. |
| CODEGEN-2113 |
Hex utility mishandles space in directory name of output file |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.4.LTS |
Use directory names without spaces for output files. |
The hex utility did not correctly handle spaces in output directory and file names. |
| CODEGEN-2098 |
Temp filename collisions on Windows with many parallel invocations |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.3.LTS |
|
In some cases with a large number of compilations in parallel on Windows, the compiler could create temporary files with colliding names, resulting in strange compilation failures. |
| CODEGEN-2060 |
Even though option --buffer_diagnostics is not used, compiler issues diagnostic that says it is deprecated |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.3.LTS |
None |
The --buffer_diagnostics compiler option was deprecated as of MCU compilers v16.6.0.STS because this setting became the default behavior for the compiler. However, the option was passed to the linker and the linker issued a remark stating the option was deprecated. |
| CODEGEN-2053 |
Compiler incorrectly reorders struct assign for small, volatile structs with bit-fields |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.2.LTS |
Use optimization level 0 or off (option --opt_level) |
For a very specific optimization, the optimizer may drop a volatile qualifier from a struct assignment. In some cases, the compiler may later perform an incorrect optimization, most commonly incorrectly reordering volatile assignments.
This bug can only happen in a function compiled with optimization level 1 or higher which contains both of the following: 1) A struct assign where the destination is volatile, and the source is a known constant, and the struct contains a bit-field, and the struct is of size "int" or smaller. 2) Any bit-field access (read or write) other than as part of a struct assign or initialization expression. That is, the name of the bit-field is present in the access expression. Note that the optimizer can create this situation by inlining functions, so 1 and 2 might be in different functions in the source code.
Consider a tree x = y where x and y are of type struct S. If the value of y is known at compile time (e.g. a const value), the optimizer will try to turn the struct constant into an integer constant (possibly combining bit-fields) and rewrite the tree to look like this: "(unsigned *)x = 32;" However, if y is volatile, that should be "*(volatile unsigned *)x = 32;" Because the access is not volatile, instruction scheduling could cause this instruction to drift past nearby volatile accesses. |
| CODEGEN-2050 |
Use of -o4 causes linker XML map file to have missing input_file entries |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.2.LTS |
|
|
| CODEGEN-2047 |
CMSIS Core v5 is not compliant with TI ARM Compiler |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.2.LTS |
The __INLINE macro in the TI compiler RTS linkage.h is no longer used and can be removed. |
CMSIS v5 defines the macro __INLINE, which interferes with the TI compiler RTS definition of the same macro in linkage.h. |
| CODEGEN-2025 |
Linker crash message incorrectly suggests submitting a preprocessed file |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.3.LTS |
|
|
| CODEGEN-2010 |
Decomp error involving packed class |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.2.LTS |
|
Fixed an issue that could result in a "Decomposition error" abort of the compiler. |
| CODEGEN-1979 |
Statements before declarations with no white space (aggravated by macros) may cause incorrect parser error |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
Do not start any statement in the left-most column
Rearrange your code so that there are no statements before declarations. |
C99 and C++ allow statements before declarations in functions. This is not allowed by the C89 language, but as an extension, the TI compiler allows such statements in relaxed mode. However, in certain circumstances, the compiler may emit the 'error: expected "}"' for otherwise legal code which has statements before declarations.
This problem can only occur in relaxed C89 mode (which is the default mode), and 1) you have a function with statements that start in the left-most column, or 2) you use macros where the macro body contains C code with statements before declarations. |
| CODEGEN-1976 |
Value of __cplusplus is wrong |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.2.LTS |
If possible, use the -ps or --strict_ansi options. This mode will use the strict definition of __cplusplus, which is 199711L. |
Our parser mimicked G++ behavior for the value of this macro in relaxed ANSI mode. This reproduced a bug in G++ versions v.4.7 and v.4.3 that has since been fixed. |
| CODEGEN-1703 |
Designated initializer plus struct hack hangs compiler |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.1.LTS |
Avoiding using string constants to initialize objects with flexible array members. Instead, use a brace-initialized array. For example:
struct { int a; char b[]; } mystruct = {0, {'h', 'e', 'l', 'l', 'o'} }; |
Fixed a compiler hang caused by initializing flexible array members with string constants.
struct {int a; char b[]; } mystruct = {0, "hello"} /* Would cause the compiler to hang and/or crash */ |
| CODEGEN-1656 |
Using --gen_profile_info does not work with -o4 |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.4.LTS |
Lower the optimization level to -o3. |
Previously, link time optimization failed when profiling options --gen_profile_info and use_profile_info were specified in combination with the --opt_level=4 option. The errors were because profiling options were not supported when used in combination with --opt_level=4.
Application profiling during whole program optimization is now supported. Profiling options --gen_profile_info and --use_profile_info may now be combined with --opt_level=4. |
| CODEGEN-1640 |
MISRA 19.1 misreported: #include statements should only be preceded by other preprocessor directives |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.1.LTS |
No practical workaround |
|
| CODEGEN-1639 |
MISRA-C:2004 17.6/R false positive when assigning local struct member to static struct member |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.4.LTS |
|
|
| CODEGEN-1634 |
MISRA 7.1 misreported: octal tokens in token paste |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.1.LTS |
No practical workaround |
|
| CODEGEN-1632 |
MISRA 15.2 misreported: switch clause unconditional break |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.1.LTS |
Put an explicit break at the end of the compound statement |
|
| CODEGEN-1555 |
Incorrect result for ullong expression passed to abs |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.1.LTS |
Use llabs instead of abs |
abs(x-y) may compute an incorrect result when x and y are unsigned long long variables. |
| CODEGEN-1517 |
#pragma FUNCTION_OPTIONS meaningless unless at least -o0 is used |
Fixed |
|
ARM_16.9.0.LTS |
|
|
| CODEGEN-1429 |
Software pipelined loop generates different results than loop not pipelined |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.0.LTS |
Avoid unsigned expressions in subscripts or in computing subscripts, or compile with -o1 or -o0. |
|
| SDSCM00052814 |
TMS570LC4357 ECC algorithm not supported |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.1.LTS |
There is a backdoor in the implementation that you can use to realize this new algorithm. Use this algorithm specification:
ECC {
algo_name : address_mask = 0xffffffff
hamming_mask = /* address */
0x53aaa750, 0xeb45d688,
0xa6d54da8, 0x9e353c68,
0x7e0cfc18, 0xfe03fc00,
0x01fffc00, 0xfe0003f8,
/* upper */
0x2E4B2E4B, 0x57155715,
0x99A699A6, 0xE338E338,
0xFCC0FCC0, 0x00FF00FF,
0xFF0000FF, 0xFF0000FF,
/* lower */
0xD1B4D1B4, 0x57155715,
0x99A699A6, 0xE338E338,
0xFCC0FCC0, 0x00FF00FF,
0xFF0000FF, 0x00FFFF00,
parity_mask = 0x0c
mirroring = F021
}
If you value your sanity, do not ask where the constants come from. |
Some devices, such as TMS570LC4357 Hercules, have a FLASH bank in high memory, and ECC uses the high bits of the address in the ECC calculation. Therefore, we need to extend the participating address bits mask in the linker-generated ECC handling. |
| CODEGEN-1333 |
Structure assignment causes compiler to fail with INTERNAL ERROR: Decomposition error |
Fixed |
|
ARM_16.9.0.LTS |
Replace struct assignments involving packed structures with a memcpy() call to copy the contents of the RHS of the struct assign to the LHS. |
|
| CODEGEN-1312 |
RTS header errno.h no longer defines POSIX macros like EFAULT |
Fixed |
|
ARM_16.9.1.LTS |
|
|
| CODEGEN-1287 |
Compiler and documentation disagree on default for --enum_type |
Fixed |
|
ARM_16.9.0.LTS |
|
|
| SDSCM00040386 |
Remove -olength option from hex utility's help summary and Users Guides |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.0.LTS |
|
|
| SDSCM00052902 |
Assembler incorrectly issues error message: Address must be of a non-global defined in the current section |
Fixed |
|
ARM_16.9.0.LTS |
The suggested workaround is to go back to 15.12.3.LTS until the next ARM compiler release is available.
Alternately, alter the code such that the target label is a non-global symbol defined in the same section as the branch. If the symbol must be global, add a second non-global label such as fake_label and change the branch to "B fake_label". |
|
| SDSCM00052734 |
Internal error in trampoline generation when user defines data symbol named "signal" |
Fixed |
|
ARM_16.9.0.LTS |
It is a user error to have two different objects in the system with the same name. Rename one of the objects. |
|
| SDSCM00051485 |
Incorrect reordering of nested op= with ++ |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.0.LTS |
Don't embed "X op= Y++" under another assignment operator. |
An expression like "a += b += c++" will produce the wrong answer. The problem is specific to sub-expressions of the form "X op= Y++" that occur under another assignment operator. |
| SDSCM00051067 |
Width-modified LDR/STREX instructions should be rejected on V6 |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
While LDREX and STREX are available on v6, all of the other EX instructions aren't available until v6k, which we do not support. For TI hardware, we begin to support these instructions in v7. The assembler should reject the instructions LDREXH, LDREXB, LDREXD, STREXH, STREXB, and STREXD for v6, including v6M0. We already treat CLREX correct and reject it for v6. |
| SDSCM00051066 |
Should reject MLS on pre-Thumb-2 devices |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
MLS is a Thumb2 instruction; it should be rejected on earlier architectures, including Cortex-M0 |
| SDSCM00046352 |
Disassembler fails to emit certain instructions in UAL form |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
For certain instructions combining the S flag and a condition code, UAL requires the S to appear before the condition code, but the disassembler puts it afterward, in the pre-UAL style.
|
| SDSCM00043877 |
Emit error message when objects too large for infrastructure (roughly 512MiB, or 256MiWords) are truncated |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.7.LTS |
N/A |
Due to an internal limitation, the code generation tools cannot presently allocate objects larger than roughly 512MiB (roughly 256MiWords). Data objects larger than this are silently truncated to a much smaller size. When such objects are declared in the code, they are silently truncated and compilation continues without any diagnostics. |
| SDSCM00043334 |
Should reject illegal MOVS instruction which cannot set status |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
The assembler accepts instructions like "MOVS R0, R10" in thumb mode, but should not. There is no instruction which can perform this move while setting the status bits. |
| SDSCM00037227 |
Bad disassembly for VMRS APSR_nzcv, FPSCR |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
The ARM disassembler mistakenly disassembles "VMRS APSR_nzcv, FPSCR" as "VMRS PC, FPSCR" |
| SDSCM00037086 |
ARM assembler allows incorrect VFP registers for some instructions on D16 VFP architectures |
Fixed |
ARM_16.9.0.LTS |
ARM_16.9.6.LTS |
|
For devices with VFP D16, the assembler should not allow instructions using registers D16-D31, but it does. |