TI PRU C/C++ CODE GENERATION TOOLS 2.3.0 Release Notes July 2018 =============================================================================== Contents =============================================================================== 1) New Device Support 2) 64-bit Tools 3) Features Available as of 2.2.0 4) Support Information ------------------------------------------------------------------------------- 1) New Device Support ------------------------------------------------------------------------------- The PRU CGT v2.3.0 adds support for silicon version 4 (--silicon_version=4). Silicon version 4 supports the TSEN instruction. ------------------------------------------------------------------------------- 2) 64-bit Tools ------------------------------------------------------------------------------- The PRU CGT v2.3.0 contains 64-bit compiler tools for Linux, Mac and Windows. 2.1) Array Output Format for Hex Utility 2.2) New Assembler Option 2.3) Support abbreviated formats for SET/CLR instructions 3) Option Cleanup ------------------------------------------------------------------------------- 3. Features Available as of 2.2.0 ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- 3.1) Array Output Format for Hex Utility ------------------------------------------------------------------------------- This release adds support for the --array option to the Hex Utility for specifying array output format. Output arrays contain data in initialized sections of an executable file. Arrays may be compiled along with a host program, such as ARM, and used to initialize the PRU at runtime. 3.1.1) Array Formation ---------------------- Arrays are formed by collecting initialized sections from the input executable. There are two ways arrays are formed: a. Using the ROMS directive. Each memory range that is given in the ROMS directive denotes an array. The romname is the array name. The origin and length parameters are required. The memwidth, romwidth, and files parameters are invalid and ignored. b. Default Array Formation. If no ROMS directive is given, arrays are formed by combining initialized sections within each page, starting with the first initialized section. Arrays will reflect any gaps that exist between sections. The default array names for test.out are 3.1.2) Array names ------------------ When ROMS directive is used, romnames are the default array names. When ROMS directive is not used, prefixes "executable_name_image_" are used for array names. For example, the default array names for test.out are test_image_0[] and test_image_1[] mapping to data on pages 0 and 1 respectively. Default prefixes for array names may be overridden by specifying array:name_prefix="prefix" 3.1.3) Data Types for Array Elements ------------------------------------ The default type for page 0 array elements is uint32_t while the type for page 1 array elements is uint8_t. However, the type for page0 array elements may be changed to uint8_t by specifying option array:page0_type_size=8. ------------------------------------------------------------------------------- 3.2) New Assembler Option ------------------------------------------------------------------------------- A new assembler option --code_address_listing_unit=byte|word was added for selecting byte or word unit for code section program counter field in assembler listing file. ------------------------------------------------------------------------------- 3.3) Support abbreviated formats for SET/CLR instructions ------------------------------------------------------------------------------- This release adds support for SET/CLR Rn.tx which is equivalent to SET/CLR Rn,Rn.tx with the same source and destination register. ------------------------------------------------------------------------------- 4. Support Information ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- 4.1) List of Fixed and Known Defects ------------------------------------------------------------------------------- The fixed and known defects can be found in the files Open_defects.html and Closed_defects.html. For open bugs, a status of Open or Accepted means that the bug has not been examined yet, whereas a status of Planned means that an evaluation or fix is in progress. ------------------------------------------------------------------------------- 4.2) Compiler Wiki ------------------------------------------------------------------------------- A Wiki has been established to assist developers in using TI Embedded Processor Software and Tools. Developers are encouraged to read and contribute to the articles. Registered users can update missing or incorrect information. There is a large section of compiler-related material. Please visit: http://processors.wiki.ti.com/index.php?title=Category:Compiler ------------------------------------------------------------------------------- 4.3) TI E2E Community ------------------------------------------------------------------------------- Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The "Development Tools" forum can be found at: http://e2e.ti.com/support/development_tools/f/default.aspx ------------------------------------------------------------------------------- 4.4) Defect Tracking Database ------------------------------------------------------------------------------- Compiler defect reports can be tracked at the Development Tools bug database, SDOWP. The log in page for SDOWP, as well as a link to create an account with the defect tracking database is found at: https://cqweb.ext.ti.com/pages/SDO-Web.html A my.ti.com account is required to access this page. To find an issue in SDOWP, enter your bug id in the "Find Record ID" box once logged in. To find tables of all compiler issues click the queries under the folder: "Public Queries" -> "Development Tools" -> "TI C-C++ Compiler" With your SDOWP account you can save your own queries in your "Personal Queries" folder.