| SDSCM00050131 |
Local struct with non-constant initializer treated as static scope variable |
Accepted |
PRU_2.2.0 |
|
|
|
| SDSCM00046695 |
Floating point addition rounding error |
Accepted |
PRU_2.2.0 |
|
|
|
| SDSCM00046114 |
RTS float arithmetic functions rounding error |
Open |
PRU_2.2.0 |
|
|
The expression 1+DBL_EPSILON/2 should be rounded DOWN to 1.0 for only mode the TI compiler supports: "round to even". |
| SDSCM00040934 |
Structure is not initialized correctly when using -o2 or -o3 optimization |
Accepted |
PRU_2.2.0 |
|
The initialization will have to be done at run-time, through a __sti initialization routine. You can see this routine when compiling without optimization. To workaround the compiler removing this initialization routine, initialize the object at the beginning of main:
Info2.mSize = ((unsigned)_end_isr_stack - (unsigned)_start_isr_stack);
|
|
| SDSCM00018691 |
Linker gives misleading warning when dot expressions used in SECTION directive for .stack section |
Accepted |
PRU_2.2.0 |
|
|
|
| SDSCM00014430 |
calloc doesn't check arguments to make sure the requested size is reasonable |
Accepted |
PRU_2.2.0 |
|
|
|
| SDSCM00008543 |
Forward reference in .space generates an internal error |
Accepted |
PRU_2.2.0 |
|
none
|
|