PRU C/C++ CODE GENERATION TOOLS 2.1.3 September 2016 Defect History ------------------------------------------------------------------------------- Table of Contents ------------------------------------------------------------------------------- 1. Defects fixed in PRU Code Generation Tools release 2.1.3 2. Defects fixed in PRU Code Generation Tools release 2.1.2 3. Defects fixed in PRU Code Generation Tools release 2.1.1 4. Defects fixed in PRU Code Generation Tools release 2.1.0 5. Current Known Issues =============================================================================== 1. Defects fixed in PRU Code Generation Tools release 2.1.3 =============================================================================== The following defects were fixed in PRU Code Generation Tools release 2.1.3, released September 2016. ------------------------------------------------------------------------------- FIXED CODEGEN-1273 / SDSCM00052734 ------------------------------------------------------------------------------- Summary : Internal error in trampoline generation when user defines data symbol named "signal" Fixed in : 2.1.3 Severity : S2 - Major Affected Component : Linker Workaround: It is a user error to have two different objects in the system with the same name. Rename one of the objects. ------------------------------------------------------------------------------- FIXED CODEGEN-1444 ------------------------------------------------------------------------------- Summary : The PRU 2.1.x compiler is TSPA, but includes a LICENSE.txt file with the old non-TSPA license. Fixed in : 2.1.3 Severity : S2 - Major Release Notes: The PRU compiler is TSPA, but includes a LICENSE.txt file with a non-TSPA license. The LICENSE.txt file should be removed. ------------------------------------------------------------------------------- FIXED CODEGEN-1333 ------------------------------------------------------------------------------- Summary : Structure assignment causes compiler to fail with INTERNAL ERROR: Decomposition error Fixed in : 2.1.3 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Workaround: Replace struct assignments involving packed structures with a memcpy() call to dpy the contents of the RHS of the struct assign to the LHS. ------------------------------------------------------------------------------- FIXED CODEGEN-1255 / SDSCM00052833 ------------------------------------------------------------------------------- Summary : Structure assignment causes compiler to fail with Linker INTERNAL ERROR with object files with DWARF information compiled by IAR compiler Fixed in : 2.1.3 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Workaround: Add option --compress_dwarf=off ------------------------------------------------------------------------------- FIXED CODEGEN-1246 / SDSCM00052723 ------------------------------------------------------------------------------- Summary : Compiler seg faults with use of --opt_level=4 Fixed in : 2.1.3 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Workaround: Use optimization level 3 or below. ------------------------------------------------------------------------------- FIXED CODEGEN-1243 / SDSCM00052699 ------------------------------------------------------------------------------- Summary : Compiler discards write to a volatile local struct member Fixed in : 2.1.3 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) ------------------------------------------------------------------------------- FIXED SDSCM00050005 ------------------------------------------------------------------------------- Summary : Compiler mistakenly issues MISRA diagnostic 12.9 for a float point type Fixed in : 2.1.3 Severity : S3 - Minor Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00050841, SDSCM00052908 Release Notes: The compiler will mistakenly emit a warning for MISRA-C:2004 12.9/R ("The unary minus operator shall not be applied to an expression whose underlying type is unsigned") when the unary minus operator is applied to any type that is not a signed integral type, such as a floating-point type. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00052468 ------------------------------------------------------------------------------- Summary : Inline assembly may cause codegen to segmentation fault Fixed in : 2.1.3 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: Inline assembly may cause the code generator to segmentation fault. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00052529 ------------------------------------------------------------------------------- Summary : Optimizer assumes enum variable can only have value of enumeration constants Fixed in : 2.1.3 Severity : S2 - Major Affected Component : Optimizer Release Notes: If an enumerated type is defined to have only two constants that evaluate to 0 and 1, then the compiler will assume that only those two values are possible. However, the C++ and C standards allow variables of enumerated types to hold other values as well; if other values are used, the compiler may produce incorrect code. Workaround: Don't make enumerated types with constants only for 0 and 1 if other values may be used. Either add a third value, or use values different than 0 and 1, or avoid using values that aren't the enumeration constants. =============================================================================== 2. Defects fixed in PRU Code Generation Tools release 2.1.2 =============================================================================== The following 19 defects were fixed in PRU Code Generation Tools release 2.1.2, released November 2015. ------------------------------------------------------------------------------- FIXED SDSCM00050834 ------------------------------------------------------------------------------- Summary : Assembler doesn't generate relocation entry for weak symbol Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Assembler Release Notes: The assembler may not generate a relocation entry for a weak symbol. This may result in a call being permanently bound to the local definition. Workaround: Use --gen_func_subsections. ------------------------------------------------------------------------------- FIXED SDSCM00051602 ------------------------------------------------------------------------------- Summary : Parser may seg fault on template arguments with ! operator Fixed in : 2.1.2 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: If the parser encounters a template argument of the form !foo, it may segmentation fault. This behavior is related to GNU mode and may be avoided with the --strict_ansi option. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 - 2.1.1 Workaround: Using the --strict_ansi option will avoid this behavior. If this is not possible, changing template arguments of the form !foo to 0==foo will also avoid this behavior. ------------------------------------------------------------------------------- FIXED SDSCM00051668 ------------------------------------------------------------------------------- Summary : Using -o4 with cout or cin will cause an incompatible types error Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Runtime Support Libraries (RTS) Release Notes: Link time optimization may cause an incompatible types error with C++ code that uses iostream. This is caused by how the standard streams (cout, cin, etc) are initialized. Defect occurs in PRU Compiler versions: 2.1.0 - 2.1.1 Workaround: Don't use link time optimization with iostream. ------------------------------------------------------------------------------- FIXED SDSCM00051708 ------------------------------------------------------------------------------- Summary : Loop downcounter may be mistakenly typed too small Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Optimizer Release Notes: When optimized, a loop may be restructured to use a downcounter, essentially of the form "while (--i)". However, in some cases, the downcounter may receive a type that is too small. In particular, if the loop may run for more iterations than MAX_INT, all iterations may not execute. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 - 2.1.1 Workaround: Lower the level of optimization. ------------------------------------------------------------------------------- FIXED SDSCM00051740 ------------------------------------------------------------------------------- Summary : AP modified before V4 saved, potentially corrupting the stack pointer Fixed in : 2.1.2 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: When compiling a function with a large frame for Thumb2 mode, the compiler can generate a frame allocation sequence that uses AP as a temporary register, corrupting the frame pointer (V4). Defect occurs in PRU Compiler versions: 2.1.0 - 2.1.1 Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00051762 ------------------------------------------------------------------------------- Summary : Dot expression adding align(64) computes hugely incorrect size Fixed in : 2.1.2 Severity : S2 - Major Affected Component : ELF Linker Release Notes: When computing the size to be added for a dot expression (e.g. ". += align(64)"), the linker may mistakenly compute a large value and fail to place the section: "lnk.cmd", line 56: error: program will not fit into available memory. placement with alignment fails for section ".foo" size 0x0 . Available memory ranges: BMEM size: 0x2000000 unused: 0x1ff8ff0 max hole: 0x1ff8ff0 Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 - 2.1.1 Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00051809 ------------------------------------------------------------------------------- Summary : "if (P) X=A; else X=B;" may compile incorrectly when A and B are 0/1 and P is 0/1 with a side effect Fixed in : 2.1.2 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: "if (P) X=A; else X=B;" may compile incorrectly when A and B are either 0 or 1, P is known to return only 0 and 1, and P has side effect (eg, it is a function that modifies a global variable and then returns 0 or 1). The compiler tries to reduce the IF to a simpler form like "X=P", but it does so via an intermediate form that uses P twice, which is incorrect when P has side effects. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 - 2.1.1 Workaround: Typically such an IF is equivalent to "X=P" or "X=!P"; write it that way to avoid the problem. Adding statements to either arm of the IF can also help. ------------------------------------------------------------------------------- FIXED SDSCM00052014 ------------------------------------------------------------------------------- Summary : Cannot read files with inode > 4B Fixed in : 2.1.2 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: Large file support (LFS) was not previously provided. The would result in messages such as "could not open source file" on some files on some file systems when one of the file attributes, such as the inode, cannot be represented in 32 bits. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00052114 ------------------------------------------------------------------------------- Summary : Windows Stack Size for Parser Should be Raised Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Parser Release Notes: By default, the parser only allows 64 pending template instantiations. By using the --pending_instantiations option, more may be allowed. While it is very unlikely to overflow the stack when parsing with the default maximum of 64 levels of recursion in a template instantiation, raising the limit may lead to a stack overflow. This will occur at lower values for -- pending_instantiations on Windows since the default stack size is 1MB. On Linux, this behavior may still occur but only at higher values since the most common default stack size for user applications on Linux is 8MB. Workaround: There are at least two options: 1. On Windows, if you have Visual Studio available, the stack for an executable may be raised with editbin. For example, to raise the stack to 8MB for the acpia6x parser, you would use: editbin /stack:8388608 acpia6x.exe 2. Use the linux toolchain. The default stack is much higher. Even if that limit is reached, the soft limit for the stack size of user applications may be raised with ulimit. For example, to raise the stack to 16MB, you would use: ulimit -S -s 16384 (This could be placed in the startup script, such as .bashrc) ------------------------------------------------------------------------------- FIXED SDSCM00052144 ------------------------------------------------------------------------------- Summary : RTS libraries do not get automatically built if the library is missing (Mac OS X) Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Runtime Support Libraries (RTS) Release Notes: On Mac OS X, the RTS lib does not get auto generated if it is missing like it does on Windows/Linux. mklib, which is responsible for building the libraries, is not currently supported on Mac OS X. Workaround: Copy the libraries from a Windows/Linux machine. ------------------------------------------------------------------------------- FIXED SDSCM00052212 ------------------------------------------------------------------------------- Summary : PRU does not issue a NOP between writing the source registers of the MAC unit and reading the result Fixed in : 2.1.2 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: This bug occurs when the MAC instructions are used in a hardware loop block. Workaround: The workaround is to use the --silicon_version=2 option. This option will prevent the compiler from using the hardware loop instruction. ------------------------------------------------------------------------------- FIXED SDSCM00052238 ------------------------------------------------------------------------------- Summary : Strong function symbol removed from linked ICODE with -o4 Fixed in : 2.1.2 Severity : S2 - Major Affected Component : ELF Linker Release Notes: At --opt_level=4, weak symbols will be used when a strong symbol should be preferred. Workaround: Use --opt_level=3 or below. ------------------------------------------------------------------------------- FIXED SDSCM00052257 ------------------------------------------------------------------------------- Summary : Use of --opt_level=4 causes link to fail with message symbol "name" redeclared with incompatible type Fixed in : 2.1.2 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00050982 Release Notes: When using -O4 optimization, the linker would sometimes incorrectly emit a "redeclared with incompatible type" error for global symbols declared with types that are at some depth defined with structs (or classes, or unions) with anonymous members. Workaround: Change all anonymous members of the types involved to have an explicit name. ------------------------------------------------------------------------------- FIXED SDSCM00052265 ------------------------------------------------------------------------------- Summary : Flexible array with initializer not handle correctly Fixed in : 2.1.2 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: Zero-length arrays is a GCC extension supported by TI compilers. The zero- length array extension also defines static initialization of C99 flex arrays. Static initialization of flex arrays should work in C99 mode when GCC extensions are enabled. Although the parser accepted these initializations, they were not output in assembly. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00052281 ------------------------------------------------------------------------------- Summary : ARM Parser Segfaults on OSX at Template Class Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Parser Duplicate Defects : SDSCM00052282 Release Notes: Parsers built for OSX may segmentation fault upon encountering a template. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00052301 ------------------------------------------------------------------------------- Summary : Linker crashes when --ecc:ecc_error is used Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Linker Release Notes: The --ecc:ecc_error option is used to inject errors into ecc information. The option takes the location of memory with ecc coverage and translates that location to the location of the corresponding ecc information. However, the translation from the program address to the ecc address was incorrect which could lead to unexpected errors, changing unexpected information, or even a segmentation fault in the linker. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00052339 ------------------------------------------------------------------------------- Summary : demangler --output option does not work at all Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Demangler (dem) Release Notes: The --output option of armdem does not work at all. You will always get the error message ">> Cannot open output file '(null)'" Workaround: armdem file.asm > file.dis ------------------------------------------------------------------------------- FIXED SDSCM00052375 ------------------------------------------------------------------------------- Summary : In some instances, compiler computes 64-bit add incorrectly Fixed in : 2.1.2 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: The instruction combinations ADD/ADC, SUB/SUC, and RSB/RSC which are used to implement 64 bit arithmetic may be scheduled in reverse order for PRU compilers 2.1.* and newer. This behavior may cause incorrect results for operations in which the operands are large enough that the carry bit must be used. Workaround: If more than 32 bits of precision are needed, there is no workaround. Otherwise, using 32 bit integers will avoid this issue. ------------------------------------------------------------------------------- FIXED SDSCM00052397 ------------------------------------------------------------------------------- Summary : Optimizer crashes on unreachable integer divide-by-zero Fixed in : 2.1.2 Severity : S2 - Major Affected Component : Optimizer Release Notes: The optimizer crashes on an unreachable integer divide-by-zero. INTERNAL ERROR: c:\drives\i\C2000\V64~1.6\compiler\cgtools\bin\opt2000.exe experienced a segmentation fault Workaround: None. =============================================================================== 3. Defects fixed in PRU Code Generation Tools release 2.1.1 =============================================================================== The following 16 defects were fixed in PRU Code Generation Tools release 2.1.1, released March 2015. ------------------------------------------------------------------------------- FIXED SDSCM00050103 ------------------------------------------------------------------------------- Summary : Buffer the output of warning and error messages to facilitate better error reporting during parallel compilation Fixed in : 2.1.1 Severity : S2 - Major Classification : Enhancement Affected Component : C/C++ Compiler (cl) Release Notes: The added --buffer_diagnostics option may be used to force compiler diagnostics to be printed by line instead of by character. This will reduce mangling of diagnostics when multiple instances of the compiler are ran in parallel. Defect occurs in PRU Compiler versions: 2.1.0 Workaround: Workaround is to manually buffer the compiler output using a script or with the --write_diagnostics_file option. ------------------------------------------------------------------------------- FIXED SDSCM00050764 ------------------------------------------------------------------------------- Summary : Bound function has incorrect address in DWARF debug info Fixed in : 2.1.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00049433 Release Notes: The TI compiler allows a function to be bound to a specific address, usually with "#pragma location". There was a bug in the way the TI assembler recorded the DWARF debugging information for a bound function that corrupted the DWARF debugging information. This would cause CCS to report "no source available" when stepping attempting to step into such a function. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 Workaround: Set a breakpoint at the bound function and run to it, rather than attempting to step into it. ------------------------------------------------------------------------------- FIXED SDSCM00050959 ------------------------------------------------------------------------------- Summary : SIGSSEGV when using % in an option argument Fixed in : 2.1.1 Severity : S2 - Major Affected Component : Shell Release Notes: In some cases, the compiler passes user-created identifiers directly to a function which behaves like printf without using a format string. If the user's identifier contains any printf-special characters, the compiler may crash. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 Workaround: Don't use any printf-special characters like % in a compiler argument ------------------------------------------------------------------------------- FIXED SDSCM00050992 ------------------------------------------------------------------------------- Summary : The optimizer should not make a symbol an alias if it has either the location or code_section pragmas applied. Fixed in : 2.1.1 Severity : S2 - Major Affected Component : Compiler Consultant (ci) Release Notes: For a reason external to the expression of the program, the user relies on function X being at a particular address A. The only method the user has to do this is to put the function in its own special subsection and place it at A in the linker command file. Workaround: Available workarounds are to: 1. Reduce the optimization level to -o2. 2. If using a COFF abi, you can move the functions into separate files. 3. Add an __asm("NOP") to the function which will prevent an alias from being created. ------------------------------------------------------------------------------- FIXED SDSCM00051004 ------------------------------------------------------------------------------- Summary : Compiler emits a reference to a symbol without declaring it in assembly. Fixed in : 2.1.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00051049 Release Notes: Under some circumstances, a constant global variable with a constant initialiser may be miscompiled in a way that causes an undefined-symbol error in the assembler. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00051097 ------------------------------------------------------------------------------- Summary : Output section splitting creates a zero-length section Fixed in : 2.1.1 Severity : S2 - Major Affected Component : ELF Linker Release Notes: In certain rare cases, the linker might split an output section into several output sections such that one of them had zero length. The linker really ought not to create split zero-length sections, as it doesn't improve the linkability of the program. This can only happen if one of the input sections is of zero length. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 Workaround: 1) Do not split the section in question. 2) Change the zero-length section so that it has at least one more byte. ------------------------------------------------------------------------------- FIXED SDSCM00051128 ------------------------------------------------------------------------------- Summary : Alias missed on address of local passed as function argument Fixed in : 2.1.1 Severity : S2 - Major Affected Component : Optimizer Duplicate Defects : SDSCM00047553 Release Notes: In certain cases, the compiler may produce incorrect code when a local variable whose address is passed to a function is then modified by the function, such as in the following example (where y is the affected local written by modf()): double f(double x) { double y = 0.; if(modf(x, &y) < 0.) return y - 1; else return y; } Workaround: Use the -ma (--aliased_variables) option. ------------------------------------------------------------------------------- FIXED SDSCM00051212 ------------------------------------------------------------------------------- Summary : MSP 4.4.0 changes to _lock.h declaration of _nop(void) instead of _nop() breaking driverlib Fixed in : 2.1.1 Severity : S2 - Major Affected Component : Runtime Intrinsics Release Notes: MSP 4.4.0 RTS file _lock.h changed prototype for _nop() to _nop(void) which errors in parser for driverlib projects. Workaround: Update _lock.h in the rts source folder, rename the library you are using, and it will automatically be rebuilt during next compile. To find compiler install location, click on project properties and click on: Resource->Linked Resources The "Path Variable" will have an entry for: CG_TOOL_ROOT c:\install_location\ccsv6\tools\compiler\msp430_4.3.4 Within above folder look for: .\lib\src\_lock.h .\include\_lock.h Edit both of above files and change below line 47: _CODE_ACCESS void _nop(void); to remove void argument and instead be: _CODE_ACCESS void _nop(); Rename the library you are using with suffix .old: .\lib\rtsx_lc_sd_eabi.lib change to a temp name .\lib\rtsx_lc_sd_eabi.lib.old Rebuild your project and the rts should automatically rebuild. ------------------------------------------------------------------------------- FIXED SDSCM00051241 ------------------------------------------------------------------------------- Summary : Output section splitting creates a zero-length section Fixed in : 2.1.1 Severity : S2 - Major Affected Component : ELF Linker Release Notes: In certain rare cases, the linker might split an output section into several output sections such that one of them had zero length. The linker really ought not to create split zero-length sections, as it doesn't improve the linkability of the program. This can only happen if one of the input sections is of zero length. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 Workaround: 1) Do not split the section in question. 2) Change the zero-length section so that it has at least one more byte. ------------------------------------------------------------------------------- FIXED SDSCM00051261 ------------------------------------------------------------------------------- Summary : The exception handling (_eh) version of runtime library is not automatically built when --exceptions option is enabled Fixed in : 2.1.1 Severity : S2 - Major Affected Component : Runtime Support Libraries (RTS) Release Notes: The exception handling (_eh) version of runtime library is not automatically built for projects that have --exceptions option enabled. This results in "undefined symbol" linker errors due to the incorrect rts library being linked in. This is caused by a missing build attribute in assembly files. This may be confirmed by examining the assembly for "Tag_Exceptions". Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 Workaround: You can build the library manually. In a command terminal, browse to the lib dir of the code gen folder (ex. C:\ti\ccsv6\tools\compiler\c2000_6.2.7\lib) and run the following command: > set PATH=%PATH%;C:\ti\ccsv6\tools\compiler\c2000_6.2.7\bin > mklib --pattern=rts2800_eh.lib --index=libc.a -- > install_to=C:/ti/ccsv6/tools/compiler/c2000_6.2.7/lib Update the paths to the CGT folder to match your install. Change the library name that is passed to the --patter option to build the other libraries for floating point (rts2800_fpu32_eh.lib) or large memory model (rts2800_ml_eh.lib). ------------------------------------------------------------------------------- FIXED SDSCM00051312 ------------------------------------------------------------------------------- Summary : Linker mistakenly issues output section warning diagnostic for sections pre-bound to hard coded addresses Fixed in : 2.1.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00051310 Release Notes: The warning is incorrectly issued for bound sections. Bound sections, created by the location pragma, are created by default by the linker, but since this is part of the implementation the linker should not issue a warning. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 Workaround: Ignore the warning ------------------------------------------------------------------------------- FIXED SDSCM00051464 ------------------------------------------------------------------------------- Summary : If a host image file is the first object file on the command line, the linker will issue an ABI incompatibility error Fixed in : 2.1.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00051482 Release Notes: If a host image file generated by the hex utility is included before any other files, the linker will emit an error such as: error: ABI version of "arm.obj" (5) is incompatible with "ti_load_image.obj" (0). Defect occurs in PRU Compiler versions: 2.1.0 Workaround: Reorder the inputs to armcl so that a host image file is not the first input. ------------------------------------------------------------------------------- FIXED SDSCM00051472 ------------------------------------------------------------------------------- Summary : Conditionals that use shift operator may be optimized out Fixed in : 2.1.1 Severity : S2 - Major Affected Component : Optimizer Release Notes: Shift operations in conditional statements may be optimized out, treating the result as 0. This will result in the entire conditional block being removed. NOTE: Intrinsics that perform shifts may be affected. In the observed test case, a shift was not explicitly used -- the C6x intrinsic _extu, which performs two shifts, was affected. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 Workaround: This behavior may be avoided by lowering the optimization level to -o1 or -o0. Moving the conditional check result to a variable so that the shift is not in the conditional may in some cases also avoid this behavior. ------------------------------------------------------------------------------- FIXED SDSCM00051555 ------------------------------------------------------------------------------- Summary : The instruction LDI R3, ((0x4<<8) | (0x2<<1)) Fixed in : 2.1.1 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: The instruction LDI R3, ((0x4<<8) | (0x2<<1)) causes assembly errors. This is legal syntax that should be supported by the assembler. Workaround: Removing the parenthesis around the shift operations allows the instruction to assemble. LDI R3, (0x4<<8 | 0x2<<1) ------------------------------------------------------------------------------- FIXED SDSCM00051621 ------------------------------------------------------------------------------- Summary : Redeclaring extern "C" function as static causes parser to hang Fixed in : 2.1.1 Severity : S2 - Major Affected Component : Parser Release Notes: Redeclaring an extern "C" function function as static may cause the parser to hang. For example: extern "C" namespace N { extern void foo(); void bar(); static inline void foo() {} } will result in the parser hanging due to the redeclaration of foo(). Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2, 2.1.0 Workaround: Use consistent function declarations. ------------------------------------------------------------------------------- FIXED SDSCM00051629 ------------------------------------------------------------------------------- Summary : Compiler seg faults in C++ copy constructor call Fixed in : 2.1.1 Severity : S2 - Major Affected Component : Parser Release Notes: This segmentation fault may occur in calls to copy constructors. For example: new CLASS( myCLASS ); Defect occurs in PRU Compiler versions: 2.1.0 Workaround: In some cases, using a different ABI option may avoid this error. However, the most safe option is to avoid the use of a copy constructor. =============================================================================== 4. Defects fixed in PRU Code Generation Tools release 2.1.0 =============================================================================== The following 15 defects were fixed in PRU Code Generation Tools release 2.1.0, released October 2014. ------------------------------------------------------------------------------- FIXED SDSCM00045417 ------------------------------------------------------------------------------- Summary : bool and _Bool are not defined correctly in strict ANSI C mode Fixed in : 2.1.0 Severity : S3 - Minor Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00048227, SDSCM00048226 Release Notes: The size and type of "bool" and "_Bool" must be the same in all modes so that declarations of the same object in different modules are compatible. However, in strict ANSI C89 mode, stdbool.h defines _Bool as "unsigned int," which means a C++ module using bool and a C module including stdbool.h and using bool are using incompatible types. _Bool and stdbool.h are C99 features, so a strictly-conforming C89 program does not use them, but the TI compiler provides them as an extension. This would cause a problem when attempting to mix C++ files and C files which both declare The ARM EABI Procedure Call Standard for the ARM Architecture (ARM IHI 0042D) section 7.1.1 ("Arithmetic Types") requires that both C++ bool and C99 _Bool be unsigned byte types. However, the TI toolset does not conform to that requirement. Workaround: The compiler and library now agree on a single definition of bool and _Bool in all modes; its format is equivalent to "unsigned char." Unfortunately, this represents a backward incompatibility with older object files which match all of these conditions: - C source code - includes stdbool.h - compiled in strict C89 mode (the default in older compilers) - module interface uses type _Bool or bool (i.e. a global variable, function argument, or function return value of type derived from bool, or struct containing a type derived from bool.) To work around the problem, either recompile with the latest version of the compiler, or ensure that you aren"t using any _Bool or bool objects in the module interface. ------------------------------------------------------------------------------- FIXED SDSCM00048498 ------------------------------------------------------------------------------- Summary : MISRA-C rule 12.8 incorrectly reported for an expression like ((uint32_t)2U << 8U); Fixed in : 2.1.0 Severity : S2 - Major Affected Component : Parser Release Notes: A violation warning for the MISRA 12.8 rule was reported for the expression: ((uint32_t)2U << 8U); The MISRA 12.8 rule states that "The right-hand operand of a shift operator shall lie between zero and one less than the width in bits of the underlying type of the left-hand operand". The underlying type is determined by section 6.10 of the MISRA Guidelines. For a literal it is defined as being the smallest type of the same sign that can represent the literal, so for 2U the type is unsigned char. In that case the diagnostic is correct. However, the cast to uint32_t should make the underlying type unsigned int, making the operation legal. Defect occurs in PRU Compiler versions: 2.0.0B1 Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00049271 ------------------------------------------------------------------------------- Summary : INTERNAL ERROR results when building code that uses features from C++ testing framework Fixed in : 2.1.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Duplicate Defects : SDSCM00050480 Release Notes: The compiler correctly handles const variables that are referenced in a program using templates. Workaround: declare VAR as "extern const int VAR = 1;" ------------------------------------------------------------------------------- FIXED SDSCM00049326 ------------------------------------------------------------------------------- Summary : RTTI is enabled by default with no way to disable it. For C++ code, this can cause data size to double. Fixed in : 2.1.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: For COFF executables, when --rtti is not used, the compiler will suppress RTTI information, leaving the executable file a bit smaller. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00049603 ------------------------------------------------------------------------------- Summary : C Initialization records are created for NOLOAD sections Fixed in : 2.1.0 Severity : S3 - Minor Affected Component : ELF Linker Release Notes: A NOLOAD output section is not allocated in the executable file created by the linker. If RAM model is used as the initialization method, the section will not be initialized by the loader since it is not allocated in memory. If ROM model is used it will be initialized because the linker creates initialization records in the .cinit section even if the section is marked NOLOAD This is a bug. Defect occurs in PRU Compiler versions: 2.0.0B1 Workaround: Specify the type as NOINIT in addition to NOLOAD ------------------------------------------------------------------------------- FIXED SDSCM00049859 ------------------------------------------------------------------------------- Summary : Compiler fails with INTERNAL ERROR message Fixed in : 2.1.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: The attached test case fails with this message ... INTERNAL ERROR: armacpia experienced a segmentation fault while processing function startExciteSequence file file.c line 441 This is a serious problem. Please contact Customer Support with this message and a copy of the input file and help us to continue to make the tools more robust. >> Compilation failure Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00049997 ------------------------------------------------------------------------------- Summary : Loop with volatile loop control expression removed Fixed in : 2.1.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: In some cases, the optimizer can remove apparently-empty loops that have a loop test which compares the loop control variable with a volatile value. This is not legal; the volatile value could change, so the loop must be left in the code. Defect occurs in PRU Compiler versions: 1.2.0B1, 2.0.0B1 - 2.0.0B2 Workaround: Declare the loop counter variable as volatile ------------------------------------------------------------------------------- FIXED SDSCM00050014 ------------------------------------------------------------------------------- Summary : Missing copyright notice on mklib.c source Fixed in : 2.1.0 Severity : S2 - Major Affected Component : Runtime Support Libraries (RTS) Release Notes: The source code for mklib (mklib.c) is part of the product but lacks a proper copyright statement. This file should have the same copyright as the other TI-generated source files in the RTS library source code. Defect occurs in PRU Compiler versions: 1.2.0B1, 2.0.0B1 - 2.0.0B2 Workaround: Not applicable ------------------------------------------------------------------------------- FIXED SDSCM00050023 ------------------------------------------------------------------------------- Summary : SIGSEGV when using pragma on a template function Fixed in : 2.1.0 Severity : S2 - Major Affected Component : Parser Release Notes: The compiler may emit an internal error (SIGSEGV) when the user attempts to apply a pragma to a template class function. Defect occurs in PRU Compiler versions: 1.2.0B1, 2.0.0B1 - 2.0.0B2 Workaround: Do not apply any pragma to a template function. Move the function outside the template class. ------------------------------------------------------------------------------- FIXED SDSCM00050243 ------------------------------------------------------------------------------- Summary : Scary but harmless warning: FAILURE in mark_use_of_function_local_static() Fixed in : 2.1.0 Severity : S2 - Major Affected Component : Optimizer Release Notes: Compiling for C++ and using -pm or -o4 may produce a warning like FAILURE in mark_use_of_function_local_static() fname1: __sti fname2: __sti_ symbol: _$P$T62$2$1 This warning, despite its dramatic wording, is harmless. The compiler will build the program just as it should, and the warning does not indicate any change in behavior. It's a debugging message that should not have been visible outside the development team. Defect occurs in PRU Compiler versions: 1.2.0B1, 2.0.0B1 - 2.0.0B2 Workaround: Avoid -pm or -o4. But the warning doesn't indicate any change of the compiler's behavior, so you might as well ignore it. ------------------------------------------------------------------------------- FIXED SDSCM00050520 ------------------------------------------------------------------------------- Summary : strip crashes on files with more than 64k sections Fixed in : 2.1.0 Severity : S2 - Major Affected Component : Strip Utility Release Notes: The strip utility will abnormally terminate if its input is an ELF file with more than 64k sections (actually exactly 0xff00), and its output would be less than 64k sections. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2 Workaround: Don't strip the file ------------------------------------------------------------------------------- FIXED SDSCM00050713 ------------------------------------------------------------------------------- Summary : Optimization level -o3 inlines weak function body Fixed in : 2.1.0 Severity : S2 - Major Affected Component : Optimizer Release Notes: A function declared as weak may be inlined, which is incorrect because the linker may override the weak definition later. Defect occurs in PRU Compiler versions: 2.0.0B1 - 2.0.0B2 Workaround: Use the FUNC_CANNOT_INLINE pragma to directly inhibit inlining. ------------------------------------------------------------------------------- FIXED SDSCM00050763 ------------------------------------------------------------------------------- Summary : Only the C6000 compiler accepts the GCC builtin function __builtin_constant_p Fixed in : 2.1.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: Error emitted that GNU __builtin_constant_p function not supported. Workaround: None. ------------------------------------------------------------------------------- FIXED SDSCM00050826 ------------------------------------------------------------------------------- Summary : PRU NOP is encoded as ADD r0.b0, r0.b0, r0.b0, which is not a NOP Fixed in : 2.1.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: NOP was being encoded incorrectly. Defect occurs in PRU Compiler versions: 2.0.0B2 Workaround: Use AND r0.b0,r0.b0,r0.b0 instead of NOP ------------------------------------------------------------------------------- FIXED SDSCM00050971 ------------------------------------------------------------------------------- Summary : PRU compiler mistakenly issues error diagnostics when building with --opt_level=4 Fixed in : 2.1.0 Severity : S2 - Major Affected Component : C/C++ Compiler (cl) Release Notes: No Information Available; please see defect details. Workaround: None. =============================================================================== 5. Current Known Issues =============================================================================== The following 9 known issues exist for PRU Code Generation Tools release 2.1.3 as of September 2016. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00052791 ------------------------------------------------------------------------------- Summary : A combination of volatile accesses of __R30 and function calls is incorrectly scheduled Affected Component : C/C++ Compiler (cl) ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00046114 ------------------------------------------------------------------------------- Summary : C6000 RTS float arithmetic functions do not round correctly Affected Component : Runtime Support Libraries (RTS) Description : The expression 1+DBL_EPSILON/2 should be rounded DOWN to 1.0 for the only mode the TI compiler supports: "round to even". ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00008543 ------------------------------------------------------------------------------- Summary : Forward reference in .space generates an internal error Affected Component : Assembler Description: If you attempt to assemble: .space 0+a b a .set 1 the assembler will generate an internal error. This happens with v3.83 and v4.1.0B1 on Solaris. If you change the code to: .space a b b .set 1 the correct error message is generated, 'Absolute, well-defined integer value expected'. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00014430 ------------------------------------------------------------------------------- Summary : calloc doesn't check arguments to make sure the requested size is reasonable Affected Component : Runtime Support Libraries (RTS) Description: The function calloc() is required to return a pointer to memory representing "nelem" copies of "size" bytes, or NULL if the request cannot be satisfied. However, for some values of "nelem" and "size" (specifically when the result of nelem*size wraps around), calloc can return a pointer to an object that is not large enough, rather than NULL. For example, on a 32-bit target, if the user calls calloc(0x00010001, 0x00010001), even though each argument by itself is reasonable, the request cannot be satisfied because the product is 0x000100020001, which exceeds size_t. (Note that we cannot check for overflow by checking if the product is less than either argument, which is commonly done for unsigned addition.) Arguably, we can try to claim that it is undefined behavior to make a call to calloc where the product would exceed size_t, but there doesn't seem to be anything in the standard which says so. The problem is worse on 16-bit targets, where calloc(0x0101, 0x0101) is enough to overflow size_t. It may not be obvious to the user that this overflows. Another concern is that it is hard to figure out whether a multiplication will overflow without having a double-width multiply available. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00018691 ------------------------------------------------------------------------------- Summary : Linker gives misleading warning when dot expressions used in SECTION directive for .stack section Affected Component : Linker Description: Linker gives the warning: warning: creating ".stack" section with default size of 0x800; use the -stack option to change the default size even when the application does not link in boot code from RTS lib. A linker command file is used that contains a specialized SECTION directive for the ".stack" section. Because of a series of ". += " assignments in the section spec, the linker is forced to increase the size of the .stack section to 0xc00. The linker is doing the correct thing by making a .stack section large enough to accommodate the dot expressions, but the diagnostic is misleading, as 0x800 isn't the final size of the .stack section. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00040934 ------------------------------------------------------------------------------- Summary : Structure is not initialized correctly when using -o2 or -o3 optimization Affected Component : Optimizer Description: There is a problem with the initialization of a structure using symbols generated in the linker command file. We use symbols generated in the linker cmd file using the dot operator. These symbols are used as an initial value for a class/struct with a constructor. In our case we want the difference of two addresses that the linker generates. When using optimization -o2 or -o3, the compiler generates .cinit entries instead of the constructor call. In those .init-entries it doesn't use the difference of the addresses; instead it uses the first symbol. When turning off optimization or using lower level of opt than -o2, the constructor calls are generated and the struct is initialized correctly. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00046695 ------------------------------------------------------------------------------- Summary : FP rounding error, 1 ULP makes P70590.c fail Affected Component : Runtime Support Libraries (RTS) Description: IEEE-754 requires exact rounding for float addition. GCC gets 4056cf03 290a0f79 const folding gets 4056cf03 290a0f79 C6000 RTS gets 4056cf03 290a0f79 C6740 simulator gets 4056cf03 290a0f78 C6600 simulator gets 4056cf03 290a0f78 correct answer is ???? ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00050131 ------------------------------------------------------------------------------- Summary : Local struct with non-constant initializer treated as static scope variable Affected Component : Parser Description: We've discovered a problem where the C++ compiler places a local structure variable not on the stack but in the data segment, as if it was a static structure. The problem is especially insidious because the issue will only have an impact on re-entrance. The problem seems to occur only for C++ files, and only if the structure initializer list contains a variable. Constant initializer lists do not trigger the issue. The structure in the first function will be allocated on the stack, but the structure in the second will be compiled as if it was declared static. ------------------------------------------------------------------------------- KNOWN ISSUE SDSCM00052163 ------------------------------------------------------------------------------- Summary : The PRU Compiler Guide states that we do not provide floating point emulation routines for PRU. This is wrong. Affected Component : C/C++ Compiler (cl) Description: Under the description for --fp_mode, the guide says: * Note that the PRU does not provide hardware floating point support or floating point emulation routines. This is wrong. We do provide floating point emulation routines.