TMS320C6000 C/C++ CODE GENERATION TOOLS 8.0.0 Release Notes September 2014 The C6000 CGT v8.0.0 release is intended for MCSDK, OpenMP, and/or OpenCL project development. For new and existing general purpose C6000-based application development projects, we recommend the use of the latest available C6000 CGT v7.4.x release (v7.4.9 as of August 2014). =============================================================================== Contents =============================================================================== 1) Support Information 1.1) List of Fixed and Known Defects 1.2) Compiler Wiki 1.3) Compiler Documentation Errata 1.4) TI E2E Community 1.5) Defect Tracking Database 2) Changes to Support of Legacy ABIs and Processor Variants 2.1) Discontinued Support for COFF 2.2) Discontinued Support for Legacy Processor Variants 2.3) Guidance and Recommended Usage 3) STLport C++ RTS 4) Support for Vector Data Types 4.1) Basic Usage 4.2) Vector Data Types and Operations ------------------------------------------------------------------------------- 1) Support Information ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- 1.1) List of Fixed and Known Defects ------------------------------------------------------------------------------- The list of defects fixed in this release as well as known issues can be found in the file DefectHistory.txt. ------------------------------------------------------------------------------- 1.2) Compiler Wiki ------------------------------------------------------------------------------- A Wiki has been established to assist developers in using TI Embedded Processor Software and Tools. Developers are encouraged to read and contribute to the articles. Registered users can update missing or incorrect information. There is a large section of compiler-related material. Please visit: http://tiexpressdsp.com/wiki/index.php?title=Category:CGT ------------------------------------------------------------------------------- 1.3) Compiler Documentation Errata ------------------------------------------------------------------------------- Errata for the "TMS320C6000 Optimizing Compiler User's Guide" and the "TMS320C6000 Assembly Language User's Guide" is available online at the Texas Instruments Embedded Processors CG Wiki: http://tiexpressdsp.com/wiki/index.php?title=Category:CGT under the 'Compiler Documentation Errata' link. ------------------------------------------------------------------------------- 1.4) TI E2E Community ------------------------------------------------------------------------------- Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The "Development Tools" forum can be found at: http://e2e.ti.com/support/development_tools/f/default.aspx ------------------------------------------------------------------------------- 1.5) Defect Tracking Database ------------------------------------------------------------------------------- Compiler defect reports can be tracked at the Development Tools bug database, SDOWP. The log in page for SDOWP, as well as a link to create an account with the defect tracking database is found at: https://cqweb.ext.ti.com/pages/SDO-Web.html A my.ti.com account is required to access this page. To find an issue in SDOWP, enter your bug id in the "Find Record ID" box once logged in. To find tables of all compiler issues click the queries under the folder: "Public Queries" -> "Development Tools" -> "TI C-C++ Compiler" With your SDOWP account you can save your own queries in your "Personal Queries" folder. ------------------------------------------------------------------------------- 2) Changes to Support of Legacy ABIs and Processor Variants ------------------------------------------------------------------------------- ------------------------------------------------------------------------------- 2.1) Discontinued Support for COFF ------------------------------------------------------------------------------- v8.0 no longer supports the COFF object file format. Only ELF is supported. In addition, the --abi option is deprecated. The default and only ABI is "eabi" and likewise, the default and only object file format is ELF. ------------------------------------------------------------------------------- 2.2) Discontinued Support for Legacy Processor Variants ------------------------------------------------------------------------------- v8.0 no longer supports older CPUs. v8.0 supports -mv6400+ (-mv6400p), -mv6740, and -mv6600. This release no longer supports -mv6200, -mv6400, -mv6700, -mv6700+ (-mv6700p), or -mvtesla. ------------------------------------------------------------------------------- 2.3) Guidance and Recommended Usage ------------------------------------------------------------------------------- The C6000 CGT v8.0 is a *NEW* compiler: * v8.0 will support C6400+, C6740, and C6600 in ELF EABI mode only * v7.4.x will continue to support all C6000 processor variants in ELF EABI or COFF ABI mode * C++ object code generated by older compilers is *NOT* compatible with v8.0 RTS object libraries You should use v8.0 if you are: * Developing new applications for OpenCL, OpenMP, or HPC-MCSDK * Developing new applications that utilize new compiler features that are available only in v8.0 and beyond (Native Vector Types, for example) You should use v7.4.x if you are: * Maintaining an existing code base that you don't want or need to transition to a new compiler * Developing new applications or maintaining existing applications that use the COFF ABI * Developing new applications or maintaining existing applications on C6200, C6400, C6700, C6700+, or Tesla. ------------------------------------------------------------------------------- 3) STLport C++ RTS ------------------------------------------------------------------------------- v8.0 introduces the STLport C++03 RTS. The move to STLport will break ABI compatibility with previous C++ RTS releases. Attempting to link old C++ object code with the new RTS will result in a link-time error. Suppressing this error will likely result in undefined symbols or undefined behavior during execution. Breakages are known to occur in particular for object code using locale, iostream, and string. In most cases, recompiling old source code with the new RTS should be safe. However, for non-standard API extensions to the C++ library, compatibility is not guaranteed. This includes usage of hash_map, slist, and rope. Dependence between locale and iostream is increased in STLport. Usage of one will likely cause the other to be linked as well. This may cause an additive increase in both code size and initialization time. C ABI compatibility will not be affected by this change. ------------------------------------------------------------------------------- 4) Support for Vector Data Types ------------------------------------------------------------------------------- Beginning with the C6000 CGT v8.0.0 alpha 3 release, the C/C++ compiler now supports the use of OpenCL-like vector data types in C/C++ source files. ------------------------------------------------------------------------------- 4.1) Basic Usage ------------------------------------------------------------------------------- Support for vector data types is available on all C6x architecures this compiler release supports (see section 2). Support for vector data types is enabled when the "--vectypes" option is specified on the compiler command line when compiling a source file for one of the above target architectures. For example: %> cl6x -mv6600 --vectypes -o1 example.c Support for vector data types requires the use of the optimizer. That is, the "--vectypes" option must be specified in combination with "-o0", "-o1", "-o2", or "-o3" on the compiler command line. All of the vector data types and related built-in functions that are supported in the C6x programming model are specified in the "c6x_vec.h" header file that you can find in the "include" sub-directory where your C6000 CGT was installed. Any C/C++ source file that utilizes vector data types or any of the built-in functions must "#include " in that source file. ------------------------------------------------------------------------------- 4.2) Vector Data Types and Operations ------------------------------------------------------------------------------- Vector Data Types ----------------- A vector type name is a concatenation of element type name with a number representing vector length. A vector with such type consists of vector length number of vector elements. The C6x programming model implementation of vector data types and operations follows the OpenCL C language specification very closely. For a more detailed description of OpenCL vector data types and operations, please see "The OpenCL Specification" version 1.2 which is available from the Khronos OpenCL Working Group: http://www.khronos.org/opencl/ Chapter 6, section 6.1.2 of "The OpenCL Specification" version 1.2 provides a detailed description of the built-in vector data types supported in the OpenCL C programming language. The C6x programming model provides the following built-in vector data types: o Element type names and sizes char char, 8 bits uchar unsigned char, 8 bits short short, 16 bits ushort unsigned short, 16 bits int int, 32 bits uint unsigned int, 32 bits longlong long long, 64 bits ulonglong unsigned long long, 64 bits float IEEE single precision floating-point, 32 bits double IEEE double precision floating-point, 64 bits NOTE: In order to avoid confusion between C6000's definition of long (32-bits) and OpenCL's definition of long (64-bits), native vector types with a base type of long or unsigned long (ulong) have not been provided. In order to use native vector types like long2, the user can simply implement a simple preprocessor macro such as: #define long2 longlong2 or #define long2 int2 depending what element type and size is desired. o Valid vector lengths: 2, 3, 4, 8, 16 For example, a "uchar8" is a vector of 8 unsigned chars. Its length is 8 and its size is 64 bits. The C6x programming model also provides an extension to the OpenCL C programming language for representing vectors of complex type. A prefix of 'c' is used to indicate a complex type name. Each complex type vector element contains a real part and an imaginary part with the real part occupying the lower address in memory. o Complex element type names and sizes: cchar complex char type, 16 bits cshort complex short type, 32 bits cint complex int type, 64 bits clonglong complex long long type, 128 bits cfloat complex float type, 64 bits cdouble complex double type, 128 bits o Valid lengths for complex type vectors: 1, 2, 4, 8 For example, a "cfloat2" is a vector of 2 complex floats. Its length is 2 and its size is 128 bits. Each "cfloat2" vector element contains a real float and an imaginary float. Vector Operations: component access ----------------------------------- A component access can occur on the left-hand-side (lhs) or right-hand-side (rhs) of an assignment operator. If specified on the lhs of an assignment, each component must be uniquely identifiable. The C6x programming model implementation supports OpenCL C like swizzle operators: o A suffix of ".x", ".y", ".z", or ".w" can be used to access an element of a vector whose length is <= 4. char4 my_c4 = (char4)(1, 2, 3, 4); char tmp = my_c4.y * my_c4.w; /* ".y" accesses 2nd element * ".w" accesses 4th element * tmp = 2 * 4 = 8; */ o A suffix of ".s0", ".s1", ..., ".s9", ".sa", ..., ".sf" can be used to access one of up to 16 elements in a vector. uchar16 ucvec16 = (uchar16)(1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16 ); uchar8 ucvec8 = (uchar8)(2, 4, 6, 8, 10, 12, 14, 16); int tmp = ucvec16.sa * ucvec8.s7; /* ".sa" is 11th element of ucvec16 * ".s7" is 8th element of ucvec8 * tmp = 10 * 16 = 160; */ o A suffix of ".even" or ".odd" can be used to access the even or odd elements of a vector. ushort4 usvec4 = (ushort4)(1, 2, 3, 4); ushort2 usvecodd = usvec4.odd; /* usvecodd = (ushort2)(2, 4); */ ushort2 usveceven = usvec4.even; /* usveceven = (ushort2)(1, 3); */ o A suffix of ".hi" or ".lo" can be used to access the elements in the upper half of a vector (for ".hi") or the elements in the lower half of a vector (for ".lo"). ushort8 usvec8 = (ushort8)(1, 2, 3, 4, 5, 6, 7, 8); ushort4 usvechi = usvec8.hi; /* usvechi = (ushort4)(5, 6, 7, 8); */ ushort4 usveclo = usvec8.lo; /* usveclo = (ushort4)(1, 2, 3, 4); */ The C6x programming model also supports an extension to the OpenCL C programming language for accessing elements of a complex type vector: o A suffix of ".r" can be used to access the real parts of each of the elements in a complex type vector. cfloat2 cfa = (cfloat2)(1.0, -2.0, 3.0, -4.0); float2 rfa = cfa.r; /* ".r" accesses real parts of cfa elements * rfa = (float2)(1.0, 3.0); */ o A suffix of ".i" can be used to access the imaginary parts of each of the elements in a complex type vector. cfloat2 cfa = (cfloat2)(1.0, -2.0, 3.0, -4.0); float2 ifa = cfa.i; /* ".i" accesses imaginary parts of cfa elements * ifa = (float2)(-2.0, -4.0); */ Swizzle operators can also be combined if the result of the combination is well-defined: ushort4 usvec4 = (ushort4)(1, 2, 3, 4); ... usvec4.hi.even = 5; /* After this assignment, * usvec4 contains (1, 2, 5, 4) */ Vector Operations: concatenation -------------------------------- Scalar entities or shorter vectors can be concatenated together to form longer vectors. When all of the components involved are constants, the result is a vector literal. Otherwise, the vector's value is determined at run-time. o Vector literals (short4)(1, 2, 3, 4); (float2)(3.2, -2.3); o Vector concatenation void foo(int a, int b) { int2 myvec = (int2)(a, b); ... } Vector Operations: conversion and re-interpretation --------------------------------------------------- The C6x programming model includes functions that can convert or re-interpret the elements of one vector type as another vector type. o convert_() can be used to perform an element by element conversion of one vector type object into another vector type object. The source vector type and the destination vector type must be the same length. void foo(int a, int b) { /* initialize a short2 vector from a converted int2 vector */ short2 svec2 = convert_short2((int2)(a, b)); ... } o as_() can be used to re-interpret the original vector type of an object as another vector type. The source type and destination type must be the same size. extern longlong lla; float2 fltvec2 = as_float2(lla); Neither the convert_() nor the as_() is available for use with complex types. Vector Operations: infix operators ---------------------------------- When infix operators are applied to vector type objects, the operator is applied element by element. That is, each element in the result vector is the result of applying the infix operator to the corresponding elements in the source vector(s). o Unary: Negate: - Bitwise complement: ~ Logical not (integer vectors only): ! int4 pos_i4 = (int4)(1, 2, 3, 4); int4 neg_i4 = -pos_i4; /* Use of negate operator initializes * neg_i4 to (-1, -2, -3, -4) */ o Binary Assignment operators: =, op= (+=, for example) Arithmetic operators: +, - , *, / Modulo operator (integer vectors only): % Bitwise operators: &, |, ^, <<, >> Relational operators: >, >=, ==, !=, <=, < Increment / decrement (integer vectors only): ++(), ()++, --(), ()-- Logical operators (integer vectors only): &&, || /* Assume iv4 argument contains (1, 2, 3, 4) coming in */ void foo(int4 iv4) { int4 local_iva = iv4++; /* local_iva = (1, 2, 3, 4) */ int4 local_ivb = iv4++; /* local_ivb = (2, 3, 4, 5) */ /* local_ivc = (1, 2, 3, 4) + (2, 3, 4, 5) = (3, 5, 7, 9) */ int4 local_ivc = local_iva + local_ivb; } /* iv4 contains (3, 4, 5, 6) on exit from foo() */ o Operators available with complex vector types Arithmetic operators: +, - , *, / Increment / decrement (by 1+0i): ++(), ()++, --(), ()-- /* On C6400+, the following code will call a built-in function to */ /* perform the copmlex multiply and divide operations. However, */ /* on C6600, the compiler will generate a CMPYSP instruction to */ /* carry out the complex multiply or divide operation. */ void foo() { cfloat2 va = (cfloat2) (1.0, -2.0, 3.0, -4.0); cfloat2 vb = (cfloat2) (4.0, -2.0, -4.0, 2.0); /* For details about the rules for complex multiplication and */ /* division, please see Annex G of the C99 C language */ /* specification. */ /* vc = < (0.0, -10.0), (-4.0, 22.0)> */ cfloat2 vc = va * vb; /* vd = < (0.4, -0.3), (-1.0, 0.5)> */ cfloat2 vd = va / vb; ... } Vector Operations: built-in functions ------------------------------------- Prototypes for all of the vector built-in functions supported in the C6x programming model are listed in the "c6x_vec.h" header file that you can find in the "include" sub-directory where your C6000 CGT package was installed. Please refer to the contents of "c6x_vec.h" for a complete list of the vector built-in functions. Here is an example which uses vector built-in functions: [vbif_ex.c] #include #include void print_short4(char *s, short4 v) { printf("%s", s); printf(" <%d, %d, %d, %d>\n", v.x, v.y, v.z, v.w); } int main() { short4 va = (short4) (1, 2, 3, -32766); short4 vb = (short4) (5, 32767, -13, 17); short4 vc = va + vb; short4 vd = va - vb; short4 ve = __add_sat(va, vb); short4 vf = __sub_sat(va, vb); print_short4("va=", va); print_short4("vb=", vb); print_short4("vc=(va+vb)=", vc); print_short4("vd=(va-vb)=", vd); print_short4("ve=__add_sat(va,vb)=", ve); print_short4("vf=__sub_sat(va,vb)=", vf); return 0; } Compile: %> cl6x -mv6400+ --vectypes -o1 -k vbif_ex.c -z -o vbif_ex.out -llnk.cmd Note: - lnk.cmd contains a reference to rts64plus_elf.lib - rts64plus_elf.lib contains c6x_veclib.obj which defines the built-in functions, __add_sat() and __sub_sat() Run: Load and run vbif_ex.out from your favorite C6400+ loader to get the following result: va= <1, 2, 3, -32766> vb= <5, 32767, -13, 17> vc=(va+vb)= <6, -32767, -10, -32749> vd=(va-vb)= <-4, -32765, 16, 32753> ve=__add_sat(va,vb)= <6, 32767, -10, -32749> vf=__sub_sat(va,vb)= <-4, -32765, 16, -32768> -- End Of File --