C6000 C/C++ Code Generation Tools v8.3.8 Release Notes
Table of Contents
- 1 Support Information
- 2 C++ 2014 support
- 3 Printf Support for Vector Data Types
- 4 Use of Vector Data Types no longer requires optimizer
- 5 Compiler Option –legacy
- 6 New Linker Feature: Using memory for multiple purposes
- 7 New Linker Option –ecc
- 8 New Function Inlining Control Pragmas
- 9 Bug related to restrict pointers fixed
1 Support Information
1.1 List of Resolved and Known Defects
Resolved defects
| ID | Summary |
|---|---|
| CODEGEN-7948 | TDEH EXIDX binary search helper reads past the end of EXIDX |
| CODEGEN-7681 | Compiler incorrectly rejects constexpr for array where length is not specified |
| CODEGEN-7600 | attribute((unpacked)) fails to override –enum_type=packed |
Open defects
| ID | Summary |
|---|---|
| CODEGEN-7956 | Compiler incorrectly changes if expression with && to an if expression that uses & |
| CODEGEN-7536 | C6000: Compiler manual incorrectly states the arguments to _ssub2 intrinsic are unsigned |
| CODEGEN-7337 | Compiler incorrectly issues remark: value copied to temporary, reference to temporary used |
| CODEGEN-6929 | Compiler generates many more single cycle NOP instructions |
| CODEGEN-6662 | C6000: callstack replicates caller function indefinitely when Step Into/Over |
| CODEGEN-6509 | Compiler error: no instance of function template matches the argument list |
| CODEGEN-6296 | Unexpectedly large loop-carried dependence bound in loop that touches struct containing array |
| CODEGEN-4942 | Conditional clause function call with GCC statement argument causes compiler crash |
| CODEGEN-1489 | lnk6x emits warnings about .tdata and .tbss when .TI.tls specification is present in a linker command file |
| CODEGEN-1013 | Array with many dimensions hangs parser |
| CODEGEN-793 | Ill advised enum scalar usage gets MISRA diagnostic, but similar usage of enum array does not |
| CODEGEN-792 | Array that is correctly initialized erroneously gets a MISRA diagnostic about size not being specified |
| CODEGEN-766 | Use of short form of options in C_OPTION may cause spurious warning |
| CODEGEN-750 | %#x should not prefix 0x to a zero value |
| CODEGEN-747 | Should reject certain unitless instructions in parallel with certain other instructions |
| CODEGEN-696 | Disassembler fails to disassemble DPINT DPTRUNC DPSP |
| CODEGEN-676 | C99 math.h macros not supported |
| CODEGEN-675 | C99 header file fenv.h not supported |
| CODEGEN-674 | isunordered not supported |
| CODEGEN-651 | Hex converter map file does not list all sections for RAM model program with initialized sections with .cinit records |
| CODEGEN-650 | Hex converter fails to process RAM model .cinit records for initialized sections |
| CODEGEN-633 | Floating point addition rounding error |
| CODEGEN-631 | pow(min, max) and pow(max, max) incorrect |
| CODEGEN-630 | global labels defined in .cproc region are discarded |
| CODEGEN-606 | When failing to place a section, include size of trampolines in error message |
| CODEGEN-581 | RTS float arithmetic functions rounding error |
| CODEGEN-367 | modf(-Inf, 1.0) with -mv6740 enters infinite loop |
| CODEGEN-322 | Structure is not initialized correctly when using -o2 or -o3 optimization |
| CODEGEN-292 | When building with -o2, compiler sometimes fails to complete compilation |
| CODEGEN-115 | compiler is scheduling use of A8 too early causing an incorrect branch |
| CODEGEN-104 | Linker gives misleading warning when dot expressions used in SECTION directive for .stack section |
| CODEGEN-63 | DWARF does not correctly represent variables stored in register pairs |
| CODEGEN-56 | Forward reference in .space generates an internal error |
| CODEGEN-30 | Compilers on PC will not work without TMP set |
1.2 Compiler Wiki
A Wiki has been established to assist developers in using TI Embedded Processor Software and Tools. Developers are encouraged to read and contribute to the articles. Registered users can update missing or incorrect information. There is a large section of compiler-related material. Please visit:
https://processors.wiki.ti.com/index.php?title=Category:Compiler
1.3 Compiler Documentation
The “TMS320C6000 Optimizing Compiler User’s Guide” can be downloaded from:
https://www.ti.com/tools-software/compilers/download.html
Navigate to the C6000 Code Generation Tools section to view the user guide in HTML or PDF format.
1.4 TI E2E Community
Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The Code Composer Studio support forum can be found at:
http://e2e.ti.com/support/tools/ccs/f/81
1.5 Defect Tracking Database
Issues filed against the TI compilers can be searched in the Code Generation Tools Defect Database.
2 C++ 2014 support
As of v8.3, the compiler supports the C++14 version of the C++ standard. C++03 is no longer supported. See the C++14 Standard ISO/IEC 14882:2014. For a description of unsupported C++ features, see Section 7.2 of the “TMS320C6000 Optimizing Compiler User’s Guide”.
The move to C++14 will break ABI compatibility with previous C++ RTS releases. Attempting to link old C++ object code with the new RTS will result in a link-time error. Suppressing this error will likely result in undefined symbols or undefined behavior during execution.
C ABI compatibility will not be affected by this change.
In most cases, recompiling old source code with the new RTS should be safe. However, due to the changes made in the language, some constructs will result in syntax errors. Some common issues include:
- Macro expansion immediately adjacent to string literals may fail due to the inclusion of new string literals and literal suffixes. Ex: u8“def” will fail to compile if ‘u8’ is a macro “def”_x will fail to compile if ’_x’ is a macro
- New keywords: alignas, alignof, char16_t, char32_t, constexpr, decltype, noexcept, nullptr, static_assert, and thread_local
- The auto keyword has been repurposed and is no longer a valid storage class specifier. Similarly, the register keyword has been deprecated and will be removed in the future.
A full list can be found in Appendix C, section 2 of the C++14 standard.
3 Printf Support for Vector Data Types
As of v8.3, the printf() function included it the RTS supports vector data types. The convention set by OpenCL 1.2 as documented in Section 6.12.13 of the OpenCL 1.2 standard is followed with one exception. This exception is to do with use of ll instead of l in the format string for longlong vector conversions.
Example:
float4 f = (float4)(1.0f, 2.0f, 3.0f, 4.0f); uchar4 uc = (uchar4)(0xFA, 0xFB, 0xFC, 0xFD);
printf(“f4 = %2.2v4hlf\n”, f); printf(“uc = %#v4hhx\n”, uc);
/* Output: */ f4 = 1.00,2.00,3.00,4.00 uc = 0xfa,0xfb,0xfc,0xfd
4 Use of Vector Data Types no longer requires optimizer
Usage of vector data types previously required the optimizer. As of v8.3, use of the optimizer is no longer required i.e. the –vectypes option can be used without specifying a -o[0-3] option.
5 Compiler Option –legacy
As of the 8.2.2 release, a compiler option, –legacy, has been added. When legacy code bases tuned for C6000 CGT v7.4.x or older exhibit performance degradations (cycles or code size) with later compiler versions, this option may help. Do not use this option in new applications. Any new features added to newer tool chains will not be available when the –legacy option is used.
6 New Linker Feature: Using memory for multiple purposes
As of v8.3, this feature enables overlaying an initialized section with the same load and run address with other sections that have separate load and run addresses.
One way to reduce memory required is to use the same range of memory for multiple purposes. It is possible to use a range of memory at first for system initialization and startup. Once that phase is complete, the same memory can then be repurposed as a collection of uninitialized data variables, or a heap. To implement this scheme, use the variation of UNION which allows one section to be initialized, and the remaining sections to be uninitialized.
Generally, an initialized section (one with raw data, such as .text) in a union must have its load allocation separately specified. However, one and only one initialized section in a union can be allocated at the union’s run address. By listing it in the union with no load allocation at all, it will use the union’s run address as its own load address.
For example:
UNION run = FAST_MEM
{ .cinit .bss }
.cinit is an initialized section. It will be loaded into FAST_MEM at the run address of the union. .bss is an uninitialized section. Its run address will also be that of the union.
7 New Linker Option –ecc
In previous versions, linker generated ECC has been enabled via an ECC specifier on memory ranges in the linker command file. This makes it difficult for TI to provide linker command files with ECC specified because users need the ability to enable/disable the support.
Starting with v8.3, users can enable/disable ecc support via the –ecc=[on|off] linker option. Existing users of ECC will need to specify –ecc=on
8 New Function Inlining Control Pragmas
Three new pragmas to control function inlining were added in this version:
a) The FORCEINLINE pragma will force functions to be inlined in the annotated statement i.e., it has no effect on those functions in general, only on function calls in a single statement.
b) The FORCEINLINE_RECURSIVE pragma will force inlining not only of calls visible in the statement, but also in the inlined bodies of calls from that statement.
c) The NOINLINE pragma prevents calls within a single statement from being inlined. (NOINLINE is the inverse of the FORCEINLINE pragma.)
9 Bug related to restrict pointers fixed
A bug that could propagate a restrict pointer into a disjoint scope (e.g., an inlined function) and make a wrong decision about memory disambiguation was fixed.
The fix may cause performance degradations when a restrict pointer is passed into an inlined function.
Based on the definition of ‘restrict’, ‘restrict’ means within the scope of the declaration of a pointer P. Only P or expressions based on P will be used to access the object or sub-object pointed to by P. A pointer copy of another restrict pointer can inherit the restrictness only when they are in the same scope or nested scopes.
For example:
int x[100]; void test() { int restrict p1; int restrict p2;
p1 = x; p2 = x+1;
foo(p1); bar(p2); }
void foo(int* r1) { *(r1+1) = 0; return; }
void bar(int* r2) { *r2 = 1; return; }
After inlining foo() and bar(), we have:
void test() { int restrict p1; int restrict p2;
p1 = x; p2 = x+1;
{// inlined function f00() int r1 = p1; (r1+1) = 0; }
{// inlined function bar() int r2=p2; r2 = 1; } }
Previous versions of the compiler might propagate p1 and p2 for r1 and r2, and incorrectly determine that (r1+1) and r2 do not alias.
This fix may cause performance degradations when pointers in disjoint scopes actually do not access the same memory locations, because the compiler has to assume that alias exists.