Readme for C2000 Code Generation Tools v20.2.7.LTS

Table of Contents


Long-term Support Release


The C2000 CGT v20.2.0.LTS release is a long term support (LTS) release. This release will be supported for roughly 2 years with periodic bug fix updates.


Compiler Downloads and Documentation


Documentation for the “TI C2000 Optimizing Compiler User’s Guide” and the “TI C2000 Assembly Language User’s Guide” is available online at:

https://www.ti.com/tool/C2000-CGT


TI E2E Community


Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The “Development Tools” forum can be found at:

http://e2e.ti.com/support/tools


Defect Tracking Database


Compiler defect reports can be tracked at the Development Tools bug database at:

https://sir.ext.ti.com/


New Features:



Integer Division Unit (HWINTDIV) updates


The Integer Division Unit feature support has below updates. Feature enabled with --idiv_support=idiv0 and requires --abi=eabi and --float_support=fpu32/fpu64.


Support inline memcpy operations larger than 255 words


Inlining of memcpy for operations less than or equal 255 words is already supported with use of the instruction: RPT #imm

Support has been added for inlining memcpy of operations larger than 255 words by using the RPT instruction with register operand.

Both memcpy inlining uses of RPT can be disabled with --rpt_threshold


FPU64 Run Time Support (RTS) library routine updates



New diagnostic checks



Hex utility --cmac option, supported added for --boot tables


The hex conversion utility’s Cipher-based Message Authentication Protocol (CMAC) feature now supports boot tables with CMAC tags.

To enable, use --cmac=key_file with --boot along with other required boot table options. The CMAC algorithm assumes a fill value of 1’s for gaps between boot table regions which requires setting --fill.


Hex utility --cmac option (cipher-based message authentication protocol)


The hex conversion utility supports the secure flash boot capability provided by TMS320F2838x devices, which have both C28 and ARM cores. The secure flash boot applies the Cipher-based Message Authentication Protocol (CMAC) algorithm to verify CMAC tags for regions of allocated memory.

In order to apply the CMAC algorithm to the appropriate regions in allocated memory, use the hex conversion utility as follows: --cmac=file where file contains a 128-bit hex CMAC key

NOTE: above additionally requires --image or --load_image options.

CMAC tag locations need to be defined in the user’s C code using below symbols along with LOCATION and RETAIN pragmas: secure boot regions: cmac_sb_1 cmac_sb_2 cmac_sb_3 or cmac_sb_4 user-specified region: cmac_all

The hex utility will then apply the CMAC algorithm to all the CMAC tags defined in the user’s C code.

See TMS320C28x Assembly Language Tools User Guide for details.


VCU register save/restore support for interrupt service routines


In prior releases, interrupt service routines (ISR) did not save/restore VCU registers.

Below new option generates VCU register save/restore to stack for ISR’s so vcu code can be re-entrant. If an ISR interrupts a VCU computation then it will not impact results.

 --isr_save_vcu_regs=on,off 

NOTE: VCU save/restore are only emitted for ISR’s that call other functions since leaf ISR routines will not have any VCU register usage as there is no current VCU code generation aside from below save/restore.

For --vcu_support=vcu0/vcu2, below are added to ISR’s:

 VMOV32 SP++,VCRC 
VMOV32
SP++,VSTATUS

VMOV32 VSTATUS,–SP
VMOV32 VCRC,
–SP

For --vcu_support=vcrc, below are added to ISR’s:

 VMOV32 SP++,VCRC 
VMOV32
SP++,VSTATUS
VMOV32 SP++,VCRCPOLY
VMOV32
SP++,VCRCSIZE

VMOV32 VCRCSIZE,–SP
VMOV32 VCRCPOLY,
–SP
VMOV32 VSTATUS,–SP
VMOV32 VCRC,
–SP


Default file extension for compiler generated object files


The default file extensions for object files created by the compiler have changed in order to prevent conflicts when C and C++ files have the same names. Object files generated from C source files have the .c.obj extension. Object files generated from C++ source files have the .cpp.obj extension.


MISRA-C 2004 Support Deprecation


Starting with C2000 CGT v20.2.5.LTS, MISRA-C 2004 checking support has been deprecated. The existing MISRA checking functionality will remain in further patch versions of this compiler stream as is, but no further issues will be addressed.


Resolved defects


Resolved defects in v20.2.7.LTS:

ID Summary
CODEGEN-10116 C2000 long-long compares using MINL/MINCUL used invalid indirect-postinc addressing mode
CODEGEN-10058 Compiler fails to handle bare \r as a line separator
CODEGEN-9831 ARM hextool boot table max block size limitation (when used with C28 on-chip boot loader)
CODEGEN-9631 CLA: Loads of 16bit signed, negative integers to MRn registers will incorrectly zero-extend by 16 bits rather than sign-extend
CODEGEN-9599 Some compiler diagnostic ID numbers changed in releases after 2019
CODEGEN-8471 Hex utility, when splitting a section as required by the bootloader, ignores the section alignment for the second part of the split
CODEGEN-4942 Conditional expression containing GNU statement expression crashes compiler in C++ mode

Known defects (dynamic)


The following link will lead to an updated list of known defects in this release:

Known defects – dynamic