| ID |
Summary |
State |
Reported In Release |
Target Release |
Workaround |
Release Notes |
| CODEGEN-1703 |
Designated initializer plus struct hack hangs compiler |
Fixed |
C2000_16.6.0.STS, C2000_16.3.0.STS, C2000_16.9.0.LTS |
C2000_16.9.1.LTS |
Avoiding using string constants to initialize objects with flexible array members. Instead, use a brace-initialized array. For example:
struct { int a; char b[]; } mystruct = {0, {'h', 'e', 'l', 'l', 'o'} }; |
Fixed a compiler hang caused by initializing flexible array members with string constants.
struct {int a; char b[]; } mystruct = {0, "hello"} /* Would cause the compiler to hang and/or crash */ |
| CODEGEN-1687 |
Assembler issues confusing diagnostic: Size is > 64 words, allocation will span page boundary |
Fixed |
C2000_16.6.0.STS, C2000_16.9.0.LTS |
C2000_16.9.1.LTS |
Compile source files without the --issue_remarks option. |
Blocking related diagnostics are longer be issued by the assembler when compiling C/C++ source files. However, these diagnostics will continue to be issued when compiling hand-coded assembly files. The diagnostics may be disabled by excluding --issue_remarks in the compiler options. |
| CODEGEN-1671 |
Arrays of Byte Peripherals or types aligned larger than their size should generate error |
Planned |
C2000_16.3.0.STS |
C2000_16.9.1.LTS |
Do not attempt to create an array of byte peripheral objects. |
The C language guarantees that the size of an array is equal to the size of each element times the number of elements. Because we double the alignment of byte peripheral data types but do not change the size, this does not hold true. There would be padding in the array, which is not allowed by the standard.
Underneath the hood, we use the aligned GCC attribute to change the alignment for byte peripherals. On GCC, if you try to make an array of elements whose alignment is larger than its size (see example code below), you get the following error:
"9:1: error: alignment of array elements is greater than element size"
However, our parser doesn’t generate an error. Instead, it just reduces the alignment of the element size silently and makes an array.
We need to generate an error and document that this is not allowed, both for byte peripherals and the aligned GCC attribute. |
| CODEGEN-1667 |
Assignment to 32-bit byte peripheral from 64-bit cast to 32-bit value causes internal error |
Fixed |
C2000_16.6.0.STS |
C2000_16.9.0.LTS |
Saving the cast value to a 32-bit temp and then assigning to the 32-bit byte peripheral will work at optimization settings of 0 and off. |
If a 64-bit value is cast to a 32-bit value and then assigned to a 32-bit byte peripheral type, an internal error occurs. |
| CODEGEN-1662 |
Optimizer incorrectly detects __fmin and __fmax idioms |
Fixed |
C2000_16.6.0.STS, C2000_16.3.0.STS |
C2000_16.9.1.LTS |
If you want floating-point absolute value, use fabs. However, there are other ways this bug could be triggered that have no practical workaround other than to use -Ooff |
|
| CODEGEN-1640 |
MISRA 19.1 misreported: #include statements should only be preceded by other preprocessor directives |
Planned |
C2000_16.6.0.STS, C2000_16.3.0.STS, C2000_16.9.0.LTS |
C2000_16.9.1.LTS |
No practical workaround |
|
| CODEGEN-1634 |
MISRA 7.1 misreported: octal tokens in token paste |
Planned |
C2000_16.6.0.STS, C2000_16.3.0.STS, C2000_16.9.0.LTS |
C2000_16.9.1.LTS |
No practical workaround |
|
| CODEGEN-1632 |
MISRA 15.2 misreported: switch clause unconditional break |
Planned |
C2000_16.6.0.STS, C2000_16.3.0.STS, C2000_16.9.0.LTS |
C2000_16.9.1.LTS |
Put an explicit break at the end of the compound statement |
|
| CODEGEN-1517 |
#pragma FUNCTION_OPTIONS meaningless unless at least -o0 is used |
Planned |
|
C2000_16.9.0.LTS |
|
|
| CODEGEN-1510 |
Assembler incorrectly issues warning on large constant used with MOVI32 instruction |
Fixed |
C2000_16.9.0.LTS |
C2000_16.9.0.LTS |
|
|
| CODEGEN-1420 |
Compiler mistakenly overwrites upper 32-bits to 0 by using MOVZ instruction to compute var32 |= 0x20 |
Fixed |
C2000_16.9.0.LTS |
C2000_16.9.1.LTS |
|
Fixed an issue where the compiler would issue a MOVZ instruction that zeroes the upper bits of an XAR register when those upper bits are needed for a future instruction. |
| CODEGEN-1333 |
Structure assignment causes compiler to fail with INTERNAL ERROR: Decomposition error |
Fixed |
C2000_16.6.0.STS |
C2000_16.9.0.LTS |
Replace struct assignments involving packed structures with a memcpy() call to copy the contents of the RHS of the struct assign to the LHS. |
|
| SDSCM00040386 |
Remove -olength option from hex utility's help summary and Users Guides |
Fixed |
C2000_16.9.0.LTS |
C2000_16.9.0.LTS |
|
|
| SDSCM00052603 |
Linker runs auto RTS even when errors have occurred |
Fixed |
|
C2000_16.3.0.STS |
None. |
|