4. GNU-Syntax Arm Assembly Directives

All assembler directives have names that begin with a period (.). The rest of the name is made up of letters (and occasionally numbers), almost always in lower case. A description of the GNU-syntax for Arm assembly, including use of directives, is provide in the GNU-Syntax Arm Assembly Source Anatomy section.

This section provides a description of each of the directives available on Arm processor variants supported by the tiarmclang toolchain (this includes Cortex-M0, Cortex-M0+, Cortex-M3, Cortex-M4, Cortex-M33, Cortex-R4, and Cortex-R5).

A full, alphabetic list of the available directives is provided in List of GNU-Syntax Arm Assembly Directives. Detailed descriptions of each directive are provided in the sections that follow, which organize directives by functional category.

GNU-syntax directives that are available only for Arm targets are indicated as “Arm only”.