1. Using the C/C++ CompilerΒΆ

This section of the tiarmclang Compiler User Manual describes the tiarmclang compiler, the compiler options that can be specified on the tiarmclang command-line, and how the compiler works with the linker to produce static executables that can be loaded and run on an Arm processor.