15.6. tiarmsize - Print Size Information¶
The tiarmsize tool prints size information for binary files.
15.6.1. Usage¶
tiarmsize [options] [input …]
tiarmsize - is the command used to invoke the tool.
options - affect the behavior of the tiarmsize tool.
input - identify one or more input object files, for which tiarmsize prints the size information for each input file specified. If no input is specified, tiarmsize attempts to print size information for a.out. If - is specified as an input file, tiarmsize reads a file from the standard input stream. If an input is an archive, size information is displayed for all its members.
The tiarmsize output is written to stdout.
15.6.2. Options¶
- -A¶
Equivalent to the --format=sysv option.
- -B¶
Equivalent to the --format=berkeley option.
- --common¶
Include ELF common symbol sizes in .bss section size for berkeley output format, or as a separate section entry for sysv output. If the --common option is not specified, these symbols are ignored.
- -d¶
Equivalent to the --radix=10 option.
- --format=<format>¶
Set the output format to the specified <format>. Available <format> argument values are:
berkeley (the default)
sysv
Berkeley output summarizes text, data and bss sizes in each file, as shown below for a typical pair of ELF files:
$ tiarmsize --format=berkeley test.out ref_global.o def_global.o text data bss dec hex filename 4968 4096 41885 50949 c705 test.out 62 0 0 62 3e ref_global.o 0 4 0 4 4 def_global.o
Sysv output displays size and address information for most sections, with each file being listed separately:
$ tiarmsize --format=sysv test.out ref_global.o def_global.o test.out : section size addr .intvecs 0 0 .bss 460 536912372 .data 465 536911904 .sysmem 8192 536903712 .stack 32768 536870944 .text 4788 32 .cinit 128 8968 .const 0 0 .rodata 52 4820 .ARM.exidx 0 0 .init_array 0 0 .TI.ramfunc 0 0 .TI.noinit 0 0 .TI.persistent 0 0 __llvm_prf_cnts 0 536870944 .binit 0 32 Veneer$$CMSE 0 0 .args 4096 4872 .ARM.attributes 83 0 .TI.section.flags 26 0 .symtab_meta 173 0 Total 51231 ref_global.o : section size addr .text 0 0 .text.main 36 0 .ARM.exidx.text.main 8 0 .rodata.str1.1 18 0 .comment 121 0 .note.GNU-stack 0 0 .ARM.attributes 65 0 .symtab_meta 5 0 .llvm_addrsig 2 0 Total 255 def_global.o : section size addr .text 0 0 .data 4 0 Total 4
- --help, -h¶
Display a summary of command line options.
- --help-list¶
Display an uncategorized summary of command line options.
- -o¶
Equivalent to the --radix=8 option.
- --radix=<value>¶
Display size information in the specified radix indicated by the <value> argument. Permitted values are 8, 10 (the default) and 16 for octal, decimal and hexadecimal output, respectively.
Example:
$ tiarmsize --radix=8 ref_global.o text data bss oct hex filename 076 0 0 76 3e ref_global.o $ tiarmsize --radix=10 ref_global.o text data bss dec hex filename 62 0 0 62 3e ref_global.o $ tiarmsize --radix=16 ref_global.o text data bss dec hex filename 0x3e 0 0 62 3e ref_global.o
- --totals, -t¶
Applies only to berkeley output format. Display the totals for all listed fields, in addition to the individual file listings.
Example:
$ llvm-size --totals ref_global.o def_global.o text data bss dec hex filename 62 0 0 62 3e ref_global.o 0 4 0 4 4 def_global.o 62 4 0 66 42 (TOTALS)
- --version¶
Display the version of the tiarmsize executable.
- -x¶
Equivalent to the --radix=16 option.
- @<file>¶
Read command-line options from specified <file>.
15.6.3. Exit Status¶
The tiarmsize utility exits with a non-zero exit code if there is an error. Otherwise, it exits with code 0.