13.1. Control Flow Integrity¶
13.1.1. Introduction¶
The TI Arm Clang Compiler Tools (tiarmclang) includes an implementation of a number of control flow integrity (CFI) schemes, which are designed to abort the program upon detecting certain forms of undefined behavior that can potentially allow attackers to subvert the program’s control flow. These schemes have been optimized for performance, allowing developers to enable them in release builds.
To enable the available CFI schemes, use the flag -fsanitize=cfi.
You can also enable a subset of available schemes.
As currently implemented, all schemes rely on link-time optimization (LTO);
so it is required to specify -flto.
The -fsanitize=cfi-{vcall,nvcall,derived-cast,unrelated-cast} flags
require that a -fvisibility= flag also be specified. This is because the
default visibility setting is -fvisibility=default, which would disable
CFI checks for classes without visibility attributes. Most users will want
to specify -fvisibility=hidden, which enables CFI checks for such classes.
13.1.2. Available Schemes¶
Available schemes are:
-fsanitize=cfi-cast-strict: Enables strict cast checks.
-fsanitize=cfi-derived-cast: Base-to-derived cast to the wrong dynamic type.
-fsanitize=cfi-unrelated-cast: Cast fromvoid*or another unrelated type to the wrong dynamic type.
-fsanitize=cfi-nvcall: Non-virtual call via an object whose vptr is of the wrong dynamic type.
-fsanitize=cfi-vcall: Virtual call via an object whose vptr is of the wrong dynamic type.
-fsanitize=cfi-icall: Indirect call of a function with wrong dynamic type.
-fsanitize=cfi-mfcall: Indirect call via a member function pointer with wrong dynamic type.
You can use -fsanitize=cfi to enable all the schemes and use
-fno-sanitize flag to narrow down the set of schemes as desired.
For example, you can build your program with
-fsanitize=cfi -fno-sanitize=cfi-nvcall,cfi-icall
to use all schemes except for non-virtual member function call and indirect call
checking.
Remember that you have to provide -flto if at least one CFI scheme is
enabled.
13.1.3. Forward-Edge CFI for Virtual Calls¶
This scheme checks that virtual calls take place using a vptr of the correct
dynamic type; that is, the dynamic type of the called object must be a
derived class of the static type of the object used to make the call.
This CFI scheme can be enabled on its own using -fsanitize=cfi-vcall.
For this scheme to work, all translation units containing the definition
of a virtual member function (whether inline or not), other than members
of ignored types or types with public visibility, must
be compiled with -flto enabled and be statically linked into the program.
13.1.4. Bad Cast Checking¶
This scheme checks that pointer casts are made to an object of the correct dynamic type; that is, the dynamic type of the object must be a derived class of the pointee type of the cast. The checks are currently only introduced where the class being casted to is a polymorphic class.
Bad casts are not in themselves control flow integrity violations, but they can also create security vulnerabilities, and the implementation uses many of the same mechanisms.
There are two types of bad cast that may be forbidden: bad casts
from a base class to a derived class (which can be checked with
-fsanitize=cfi-derived-cast), and bad casts from a pointer of
type void* or another unrelated type (which can be checked with
-fsanitize=cfi-unrelated-cast).
The difference between these two types of casts is that the first is defined
by the C++ standard to produce an undefined value, while the second is not
in itself undefined behavior (it is well defined to cast the pointer back
to its original type) unless the object is uninitialized and the cast is a
static_cast (see C++14 [basic.life]p5).
If a program as a matter of policy forbids the second type of cast, that
restriction can normally be enforced. However it may in some cases be necessary
for a function to perform a forbidden cast to conform with an external API
(e.g. the allocate member function of a standard library allocator). Such
functions may be ignored.
For this scheme to work, all translation units containing the definition
of a virtual member function (whether inline or not), other than members
of ignored types or types with public visibility, must
be compiled with -flto enabled and be statically linked into the program.
13.1.5. Non-Virtual Member Function Call Checking¶
This scheme checks that non-virtual calls take place using an object of
the correct dynamic type; that is, the dynamic type of the called object
must be a derived class of the static type of the object used to make the
call. The checks are currently only introduced where the object is of a
polymorphic class type. This CFI scheme can be enabled on its own using
-fsanitize=cfi-nvcall.
For this scheme to work, all translation units containing the definition
of a virtual member function (whether inline or not), other than members
of ignored types or types with public visibility, must
be compiled with -flto enabled and be statically linked into the program.
13.1.5.1. Strictness¶
If a class has a single non-virtual base and does not introduce or override virtual member functions or fields other than an implicitly defined virtual destructor, it will have the same layout and virtual function semantics as its base. By default, casts to such classes are checked as if they were made to the least derived such class.
Casting an instance of a base class to such a derived class is technically
undefined behavior, but it is a relatively common hack for introducing
member functions on class instances with specific properties that works under
most compilers and should not have security implications, so we allow it by
default. It can be disabled with -fsanitize=cfi-cast-strict.
13.1.6. Indirect Function Call Checking¶
This scheme checks that function calls take place using a function of the
correct dynamic type; that is, the dynamic type of the function must match
the static type used at the call. This CFI scheme can be enabled on its own
using -fsanitize=cfi-icall.
For this scheme to work, each indirect function call in the program, other
than calls in ignored functions, must call a
function which was either compiled with -fsanitize=cfi-icall enabled,
or whose address was taken by a function in a translation unit compiled with
-fsanitize=cfi-icall.
If a function in a translation unit compiled with -fsanitize=cfi-icall
takes the address of a function not compiled with -fsanitize=cfi-icall,
that address may differ from the address taken by a function in a translation
unit not compiled with -fsanitize=cfi-icall. This is technically a
violation of the C and C++ standards, but it should not affect most programs.
Each translation unit compiled with -fsanitize=cfi-icall must be
statically linked into the program or shared library, and calls across
shared library boundaries are handled as if the callee was not compiled with
-fsanitize=cfi-icall.
13.1.6.1. -fsanitize-cfi-icall-generalize-pointers¶
Mismatched pointer types are a common cause of cfi-icall check failures.
Translation units compiled with the -fsanitize-cfi-icall-generalize-pointers
flag relax pointer type checking for call sites in that translation unit,
applied across all functions compiled with -fsanitize=cfi-icall.
Specifically, pointers in return and argument types are treated as equivalent as
long as the qualifiers for the type they point to match. For example, char*,
char**, and int* are considered equivalent types. However, char* and
const char* are considered separate types.
13.1.6.2. -fsanitize-cfi-canonical-jump-tables¶
The default behavior of the compiler’s indirect function call checker will
replace the address of each CFI-checked function in the output file’s symbol
table with the address of a jump table entry which will pass CFI checks. We
refer to this as making the jump table canonical. This property allows code
that was not compiled with -fsanitize=cfi-icall to take a CFI-valid address
of a function, but it comes with a couple of caveats:
There is a performance and code size overhead associated with each exported function, because each such function must have an associated jump table entry, which must be emitted even in the common case where the function is never address-taken anywhere in the program, and must be used.
There is no good way to take a CFI-valid address of a function written in assembly or a language not supported by Clang. The reason is that the code generator would need to insert a jump table in order to form a CFI-valid address for assembly functions, but there is no way in general for the code generator to determine the language of the function.
For these reasons, we provide the option of making the jump table non-canonical
with the flag -fno-sanitize-cfi-canonical-jump-tables. When the jump
table is made non-canonical, symbol table entries point directly to the
function body. Any instances of a function’s address being taken in C will
be replaced with a jump table address.
This scheme does have its own caveats, however. It does end up breaking function address equality more aggressively than the default behavior.
Furthermore, it is occasionally necessary for code not compiled with
-fsanitize=cfi-icall to take a function address that is valid
for CFI. For example, this is necessary when a function’s address
is taken by assembly code and then called by CFI-checking C code. The
__attribute__((cfi_canonical_jump_table)) attribute may be used to make
the jump table entry of a specific function canonical so that the external
code will end up taking an address for the function that will pass CFI checks.
13.1.7. Member Function Pointer Call Checking¶
This scheme checks that indirect calls via a member function pointer
take place using an object of the correct dynamic type. Specifically, we
check that the dynamic type of the member function referenced by the member
function pointer matches the “function pointer” part of the member function
pointer, and that the member function’s class type is related to the base
type of the member function. This CFI scheme can be enabled on its own using
-fsanitize=cfi-mfcall.
The compiler will only emit a full CFI check if the member function pointer’s
base type is complete. This is because the complete definition of the base
type contains information that is necessary to correctly compile the CFI
check. To ensure that the compiler always emits a full CFI check, it is
recommended to also pass the flag -fcomplete-member-pointers, which
enables a non-conforming language extension that requires member pointer
base types to be complete if they may be used for a call.
For this scheme to work, all translation units containing the definition
of a virtual member function (whether inline or not), other than members
of ignored types or types with public visibility, must
be compiled with -flto enabled and be statically linked into the program.
13.1.8. Ignorelist¶
An IgnoreList can be used to relax CFI checks for certain
source files, functions and types using the src, fun and type
entity types. Specific CFI modes can be be specified using [section]
headers.
# Suppress all CFI checking for code in a file.
src:bad_file.cpp
src:bad_header.h
# Ignore all functions with names containing MyFooBar.
fun:*MyFooBar*
# Ignore all types in the standard library.
type:std::*
# Disable only unrelated cast checks for this function
[cfi-unrelated-cast]
fun:*UnrelatedCast*
# Disable CFI call checks for this function without affecting cast checks
[cfi-vcall|cfi-nvcall|cfi-icall]
fun:*BadCall*
13.1.9. Publications¶
Control-Flow Integrity: Principles, Implementations, and Applications. Martin Abadi, Mihai Budiu, Úlfar Erlingsson, Jay Ligatti.
Enforcing Forward-Edge Control-Flow Integrity in GCC & LLVM. Caroline Tice, Tom Roeder, Peter Collingbourne, Stephen Checkoway, Úlfar Erlingsson, Luis Lozano, Geoff Pike.