2.1. Data Types

2.1.1. Scalar Data Types

The table below lists the size and range of each scalar type as supported in the tiarmclang compiler. Many of the minimum and maximum values for each range are available as standard macros in the C standard header file limits.h.

The storage and alignment of data types is described in Object Representation.

Type

Size

Min Value

Max Value

signed char

8 bits

-128

127

char unsigned char bool

8 bits

0

255

short signed short

16 bits

-32768

32767

unsigned short

16 bits

0

65535

int signed int long signed long

32 bits

-2147483648

2147483647

enum

packed

-2147483648

2147483647

unsigned int unsigned long wchar_t

32 bits

0

4294967295

long long signed long long

64 bits

-9223372036854775808

9223372036854775807

unsigned long long

64 bits

0

18446744073709551615

float

32 bits

1.175494e-38

3.40282346e+38

double long double

64 bits

2.22507385e-308

1.79769313e+308

pointers references data member ptrs

32 bits

0

0xFFFFFFFF

Notes:

  • The “plain” char type has the same representation as either signed char or unsigned char. The -fsigned-char and -funsigned-char options control whether “plain” char is signed or unsigned. The default is unsigned.

  • The wchar_t type has the same representation as unsigned int. The tiarmclang runtime libraries do not support a 16-bit wchar_t type. Attempts to use the tiarmclang -fshort-wchar option may cause issues when linked with the tiarmclang runtime libraries.

  • 64-bit data types is aligned on a 64-bit (8-byte) boundary.

  • Further discussion about the size of enum types can be found below in the Enum Type Storage.

  • Specified minimum values for floating-point types in the table above indicate the smallest precision value > 0.

  • Negative values for signed types are represented using two’s complement.

2.1.2. Enum Type Storage

The type of the storage container for an enumerated type is the smallest integer type that contains all the enumerated values. The container types for enumerators are shown in the following table:

Lower Bound Range

Upper Bound Range

Enumerator Type

0 to 255

0 to 255

unsigned char

-128 to 1

-128 to 127

signed char

0 to 65535

256 to 65535

unsigned short

-128 to 1 -32768 to -129

128 to 32767 -32768 to 32767

signed short

0 to 4294967295

2147483648 to 4294967295

unsigned int

-32768 to -1 -2147483648 to -32769 0 to 2147483647

32767 to 2147483647 -2147483648 to 2147483647 65536 to 2147483647

signed int

The compiler determines the type based on the range of the lowest and highest elements of the enumerator.

For example, the following code results in an enumerator type of int:

enum COLORS {
  green  = -200,
  blue   = 1,
  yellow = 2,
  red    = 60000
};

The following code results in an enumerator type of short:

enum COLORS {
  green  = -200,
  blue   = 1,
  yellow = 2,
  red    = 60000
};