1.3.7. Optimization Options¶
To enable optimization passes in the tiarmclang compiler, select a level of optimization from among the following -O[0|1|2|3|fast|g|s|z] options. In general, the options below represent various levels of optimization with some options designed to favor smaller compiler generated code size over performance, while others favor performance at the cost of increased compiler generated code size.
For a more precise list of optimizations performed for each level, please see Optimizations Performed at Each Level.
1.3.7.1. Optimization Level Options¶
Among the options listed below, -Oz is recommended as the optimization option to use if small compiler generated code size is a priority for an application. Use of -Oz will still retain performance gains from many of the -O2 level optimizations that are performed.
-
-O0
¶
No optimization. This level of optimization does not inhibit compile time and generates debug-friendly code.
-
-O1
,
-O
¶
Enable restricted optimizations, providing a good trade-off between code size and debug-ability.
-
-O2
¶
Enable most optimizations, but some optimizations that require significantly additional compile time are disabled.
-
-O3
¶
Enable all optimizations available at -O2 plus others that require additional compile time to perform.
-
-Ofast
¶
Enable all optimizations available at -O3 plus additional aggressive optimizations with potential for additional performance gains, but also not guaranteed to be in strict compliance with language standards.
-
-Og
¶
Enable restricted optimizations while preserving debug-ability.
-
-Os
¶
Enable all optimizations available at -O2 plus additional optimizations that are designed to reduce code size while mitigating negative impacts on performance.
-
-Oz
¶
Enable all optimizations available at -O2 plus additional optimizations to further reduce code size with the risk of sacrificing performance.
Note
Optimization Option Recommendations
- The -Oz option is recommended for optimizing code size.
- The -O3 option is recommended for optimizing performance, but it is likely to increase compiler generated code size.
1.3.7.2. Optimizations Performed at Each Level¶
This table describes some examples of optimizations performed at each optimization level.
Optimization Level Optimizations Performed
-O0
¶
None
-O1
¶
- Control Flow Simplification
- Merge contiguous icmps into a memcmp
- memcpy/memset/memcmp inlining
- Constant Hoisting
- Partially inline calls to library functions
- Inline for always_inline functions
- Global Variable Merging
- Merge disjoint stack slots
- Loop Strength Reduction
- Loop Invariant Code Motion
- Common Subexpression Elimination
- Dead Argument Elimination
- Machine code sinking
- Peephole optimization
- Tail Predication
- Tail Duplication
- Load/store optimization
- Simple Register Coalescing
- Copy Propagation
- Conditional Constant Propagation
- Called Value Propagation
- Control Flow optimization
- If-conversion
- Thumb2 instruction size reduction
- Dead Code Elimination
- Loop Vectorization
- Printf function specialization
- Small memcpy/memset function specialization
- Conditionally eliminate dead library calls
- Loop Rotation
- Loop Unrolling
-O2
¶
- Performs all (-O1) optimizations, plus:
- Function Integration/Inlining
- Instruction speculation
- Value Propagation
- Jump Threading (non-DFA)
- Tail Call Elimination
- Merged Load/Store Motion
- Global Value Numbering
- Memory Dependence Analysis
- Dead Store Elimination
- Superword-Level Parallelism (SLP) vectorization
- Combine redundant instructions
- Dead Global Elimination
- Global Duplicate Constant Merging
- Fast memcpy/memset function specialization
- Align loop target boundaries to 16bytes (Cortex-R4/R5)
-O3
¶
- Performs all (-O2) optimizations tuned for speed, plus:
- Replace functions with supported intrinsics
- Additional alias analysis and loop optimization
- Aggressive Function Inlining
- Call-site splitting
- Promote ‘by reference’ arguments to scalars
- Combine pattern based expressions
-Ofast
¶
- Performs all (-O3) optimizations, plus:
- Allow optimizations to treat the sign of a zero argument or result as insignificant
- Assumes no Inf values
- Assumes no NaN values
- Enable optimizations that make unsafe assumptions about IEEE math
- Allow reassociation transformations for floating-point instructions
- Allow optimizations to use the reciprocal of an argument rather than perform division
- Allow more aggressive, lossy floating point math operations that enhance speed
-Og
¶
- Performs all (-O2) optimizations, but disables the following:
- No Loop Vectorization
- No function inlining except for always_inline functions
- No instruction speculation
- No Jump Threading
- No Value Propagation
- No Tail Call Elimination
- No Merged Load/Store Motion
- No Global Value Numbering
- No Memory Dependence Analysis
- No Superword-Level Parallelism (SLP) Vectorization
- No Dead Global Elimination
- No Global Duplicate Constant Merging
-Os
¶
- Performs all (-O2) optimizations tuned for code size, plus:
- Previously enabled optimizations tuned for code size
- Small memcpy/memset function specialization
- Minimal memcpy/memset/memcmp inlining
- Don’t conditionally eliminate dead library calls
- Don’t align loop target boundaries to 16bytes (Cortex-R4/R5)
-Oz
¶
- Performs all (-Os) optimizations, plus:
- Machine Outlining
- No Loop Vectorization
- Less aggressive optimizations that impact code size
- Don’t align loop target boundaries to 16bytes (Cortex-R4/R5)
1.3.7.3. More Specialized Optimization Options¶
1.3.7.3.1. Floating-Point Arithmetic¶
-
-fsigned-zeros
,
-fno-signed-zeros
¶
Assume the presence of signed floating-point zero values. Use of the -fno-signed-zeros option can improve code if the compiler can assume that it doesn’t need to account for the presence of signed floating-point zero values.
-
-fhonor-nans
,
-fno-honor-nans
¶
Instruct the compiler to check for and properly handle floating-point NaN values. Use of the -fno-honor-nans can improve code if the compiler can assume that it doesn’t need to check for and enforce the proper handling of floating-point NaN values.
1.3.7.3.2. Function Outlining¶
-
-moutline
,
-moutline-inter-function
,
-mno-outline
¶
Function outlining (aka “machine outlining”) is an optimization that saves code size by identifying recurring sequences of machine code and replacing each instance of the sequence with a call to a new function that the identified sequence of operations.
Function outlining is enabled when the -Oz option is specified on the tiarmclang command-line. There are 3 settings for the function outlining optimization when using the -Oz option:
-
-moutline
¶
The -moutline option is the default setting and will perform machine outlining within functions. This is less aggressive than -moutline-inter-function, but it is guaranteed to be applied only when doing so will reduce the net code size.
-
-moutline-inter-function
¶
The -moutline-inter-function option can be specified in combination with the -Oz option to enable inter-function outlining. While this is the more aggressive of the function outlining settings, it does not always guarantee an overall code size reduction if, for example, outlining occurs across multiple functions in a given compilation unit yet only one of those functions is included in the linked application, the application will include the outlined code as well as the additional instructions required to call that code. However, it is likely to be beneficial when all functions defined in a given compilation unit are included in the linked application.
-
-mno-outline
¶
The -mno-outline option can be used to disable function outlining for a given compilation unit when using the -Oz option.
1.3.7.3.3. Inlining¶
-
-finline-functions
,
-fno-inline-functions
¶
Inline suitable functions. The -fno-inline-functions will disable this optimization.
-
-finline-hint-functions
¶
Inline functions which are explicitly or implicitly marked inline.
-
-mllvm
-arm-memset-max-stores=<n>
¶ When optimization is turned on during a compilation, the tiarmclang compiler will inline calls to runtime support routines memset or memclr if the size of the data is below a certain threshold. For example, in the following source file:
#include <string.h> struct { int t1; int t2; int t3; int t4; short t5; long t6; } my_struct_inline; void func() { memset(&my_struct_inline, 0, sizeof(my_struct_inline)); }
When compiled with -O[1|2|3|fast], the call to memset will be inlined if the clearing of the my_struct_inline data object can be done with <= 8 store instructions:
%> tiarmclang -mcpu=cortex-m0 -O3 -S struct_inline.c %> cat struct_inline.s ... func: ldr r0, .LCPI0_0 movs r1, #0 str r1, [r0] str r1, [r0, #4] str r1, [r0, #8] str r1, [r0, #12] str r1, [r0, #16] str r1, [r0, #20] bx lr .p2align 2 .LCPI0_0: .long my_struct_inline ...
However, when compiled with -O[s|z}, where the compiler is attempting to generate smaller code, the call to memset will be inlined if the clearing of the my_struct_inline data object can be done with <= 4 store instructions. When compiled in combination with the -mcpu=cortex-m0 option, the call to memset will not be inlined, but it will be implemented with a call to __aeabi_memclr:
%> tiamclang -mcpu=cortex-m0 -Oz -S struct_inline.c %> cat struct_inline.s ... func: push {r7, lr} ldr r0, .LCPI0_0 movs r1, #24 bl __aeabi_memclr4 pop {r7, pc} .p2align 2 .LCPI0_0: .long my_struct_inline
The -mllvm -arm-memset-max-stores=<n> option allows you to control the criteria used by the compiler to decide whether or not to inline a call to the memset or memclr function. If the above example is re-compiled with -mcpu=cortex-m0 -Oz -mllvm -arm-memset-max_stores=6, then the call to memset will get inlined since the clearing of my_struct_inline can be acccomplished on Cortex-M0 with 6 store instructions:
%> tiarmclang -mcpu=cortex-m0 -Oz -mllvm -arm-memset-max-stores=6 -S struct_inline.c %> cat struct_inline.s ... func: ldr r0, .LCPI0_0 movs r1, #0 str r1, [r0] str r1, [r0, #4] str r1, [r0, #8] str r1, [r0, #12] str r1, [r0, #16] str r1, [r0, #20] bx lr .p2align 2 .LCPI0_0: .long my_struct_inline ...
The optimal value for the argument <n> to use with the -mllvm -arm-memset-max-stores=<n> option will vary depending on each particular use-case. Adjusting this value will only be beneficial if you are able to control the limit as needed.